Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:fpga:xilinx:interposer:ad5694r [28 Sep 2012 11:22] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costinaresources:fpga:xilinx:interposer:ad5694r [09 Jan 2021 00:48] (current) – user interwiki links Robin Getz
Line 12: Line 12:
 ====== Overview ====== ====== Overview ======
  
-This document presents the steps to setup an environment for using the **[[adi>AD5694R|EVAL-AD5694RSDZ]]** evaluation board together with the Xilinx KC705 FPGA boardthe Xilinx Embedded Development Kit (EDK) and the [[http://micrium.com/page/products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5694RSDZ Evaluation Board with the Xilinx KC705 board.+This document presents the steps to setup an environment for using the **[[adi>AD5694R|EVAL-AD5694RSDZ]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5694RSDZ Evaluation Board with the Xilinx KC705 board.
  
 {{ :resources:fpga:xilinx:interposer:img_ad5694r.jpg?400 }} {{ :resources:fpga:xilinx:interposer:img_ad5694r.jpg?400 }}
Line 29: Line 29:
   * [[adi>AD5694R|AD5694R Product Info]] - pricing, samples, datasheet   * [[adi>AD5694R|AD5694R Product Info]] - pricing, samples, datasheet
   * EVAL-AD5694RSDZ evaluation board user guide   * EVAL-AD5694RSDZ evaluation board user guide
-  * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] +  * [[xilinx>products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
-  * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]]+
  
 ====== Getting Started ====== ====== Getting Started ======
Line 38: Line 37:
 ===== Required Hardware ===== ===== Required Hardware =====
  
-  * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]+  * [[xilinx>products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]]
   * FMC-SDP adapter board   * FMC-SDP adapter board
   * **EVAL-AD5694R** evaluation board   * **EVAL-AD5694R** evaluation board
Line 44: Line 43:
 ===== Required Software ===== ===== Required Software =====
  
-  * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack)+  * Xilinx ISE 14.6
-  * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool+  * UART Terminal (Termite/Tera Term/Hyperterminal), baud rate 115200. 
 +  * The EVAL-AD5694R reference project for Xilinx KC705 FPGA.
  
 ===== Downloads ===== ===== Downloads =====
- +<WRAP round download 80%> 
-  * {{:resources:fpga:xilinx:interposer:ad5694r_evalboard.zip|Reference Design Files}} +\\ 
- +  * **AD5694R Driver:** https://github.com/analogdevicesinc/no-OS/tree/master/device_drivers/AD5686 
-The following table presents a short description the reference design archive contents. +  * **AD5694R Commands:** https://github.com/analogdevicesinc/no-OS/tree/master/device_commands/AD5686 
- +  * **Xilinx Boards Common Drivers:** https://github.com/analogdevicesinc/no-OS/tree/master/platform_drivers/Xilinx/SDP_Common 
-**Folder** **Description** +  * **EDK KC705 Reference project:** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_sdp_kc705 
-| Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation| +\\ 
-| Microblaze | Contains the EDK project for the Microblaze softcore that will be implemented in the KC705 FPGA. | +</WRAP>
-| Software | Contains the source files of the software project that will be run by the Microblaze processor.| +
-| uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | +
 ====== Run the Demonstration Project ====== ====== Run the Demonstration Project ======
  
-===== Hardware Setup =====+===== Hardware setup =====
  
-<note important>Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</note>+<WRAP round important 80%> 
 +\\ 
 +Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. 
 +</WRAP>
  
   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.   * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector.
   * Connect the JTAG and UART cables to the KC705 and power up the FPGA board.   * Connect the JTAG and UART cables to the KC705 and power up the FPGA board.
-  * Start IMPACT, and double click “//Boundary Scan//”. Right click and select //Initialize Chain//. The program should recognize the Kintex 7 device (see screenshot below). 
-{{ :resources:fpga:xilinx:interposer:impact_config.png?300 }}  
-  * Program the KC705 FPGA using the "//Bit/download.bit//" file provided in the reference design archive. 
-  * Power the ADI evaluation board. 
- 
-At this point everything is set up and it is possible to start the evaluation of the ADI hardware through the controls in the uC-Probe application provided in the reference design. 
- 
-===== Configure uC-Probe ===== 
- 
-Launch **uC-Probe** from the **//Start -> All Programs -> Micrium -> uC-Probe//**. 
- 
-Select **uC-Probe** options. 
-  * Click on the **uC-Probe** icon on the top left portion of the screen. 
-  * Click on the **//Options//** button to open the dialog box. 
- 
-{{ :resources:fpga:altera:bemicro:ucprobeoptionsbtn.png?300 }} 
- 
-Set target board communication protocol as **//RS-232//** 
-  * Click on the **//Communication//** tab icon on the top left portion of the dialog box 
-  * Select the **//RS-232//** option. 
- 
-{{ :resources:fpga:xilinx:interposer:ucprobe_comm.png?300 }} 
- 
-Setup **//RS-232//** communication settings 
-  * Select the **//RS-232//** option from the **//Communication//** tab. 
-  * Select the COM port to which the KC705 board is connected. 
-  * Set the Baud Rate to 115200 bps. 
- 
-{{ :resources:fpga:xilinx:interposer:ucprobe_rs232.png?300 }} 
- 
-  * Press **//Apply//** and **//OK//** to exit the options menu. 
- 
-===== Load and Run the Demonstration Project ===== 
- 
-  * Click the **//Open//** option from the **uC-Probe** menu and select the file **//ucProbeInterface/AD5694R_Interface.wsp//** provided within the reference design files. 
- 
-  * Before opening the interface **uC-Probe** will ask for a symbols file that must be associated with the interface. Select the file **//ucProbeInterface/ADIEvalBoard.elf//** to be loaded as a symbol file. 
- 
-  * Run the demonstration project by pressing the **//Play//** button. 
- 
-{{ :resources:fpga:altera:bemicro:image081.png?200 }} 
- 
-<note tip>In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **//Stop//** button and run it again by pressing the **//Play//** button.</note> 
- 
-===== Demonstration Project User Interface ===== 
- 
-The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5694RSDZ** evaluation board. 
- 
-{{ :resources:fpga:altera:bemicro:ad5694r_interface.png?700 }} 
- 
-**Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the //ON/OFF// switch. The //Activity// LED turns green when the communication is active. If the //ON/OFF// switch is set to //ON// and the //Activity// LED is //BLACK// it means that there is a communication problem with the board. See the **Troubleshooting** section for indications on how to fix the communication problems. 
- 
-**Section B** is used to select the //Command// to be sent to the DAC. The definition of each command is available in Table 7 of the part's datasheet. 
- 
-**Section C** is used to select the //Address// of the registers to be affected by the command, if the command is 1, 2 or 3. If the selected command is 5, the //Address// buttons will be used to program the //LDAK MASK REGISTER// for the corresponding DAC. For the other commands, they are ignored. 
- 
-**Section D** is used to program the value to be written to the DAC registers.  
- 
-**Section E** is used to send the selected command to the DAC. 
  
-**Section F** is used to configure the databits sent for the command 4. Each DAC's power operation can be configured independently.+<WRAP round important 80%> 
 +\\ 
 +To power on the EVAL-AD5694R evaluation board, you need to apply +6V supply voltage to J3 connector of the board. 
 +</WRAP>
  
-**Section G** is used to configure the databits sent for the command 7If the button is pressed, the Internal reference will be turned off.+===== Reference Project Overview ===== 
 +The following commands were implemented in this version of EVAL-AD5694R reference project for Xilinx KC705 FPGA board. 
 +^ Command ^ Description ^ 
 +**help?** | Displays all available commands. | 
 +| **reset!** | Activate a power-on reset. | 
 +| **load=** | Loads selected DAC input register with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | 
 +| **update=** | Update the selected DAC channel with the input register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels. | 
 +| **loadAndUpdate=** | Loads and updates the selected DAC with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | 
 +| **pwrMode=** | Set up the Power Mode of a selected channel. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ power mode:\\ 0 - normal operation.\\ 1 - 1KOhm to GND.\\ 2 - 100KOhms to GND.\\ 3 - three-state. | 
 +| **pwrMode?** | Displays the power mode for one selected DAC. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D. | 
 +| **ldacMask=** | Set up the LDAC mask registerAccepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ set/reset mask:\\ 0 - reset LDAC mask for the selected channel.\\ 1 - set LDAC mask for the selected channel. | 
 +| **ldacMask?** | Displays the LDAC register. | 
 +| **intRef=** | Turns ON or OFF the internal reference. Accepted values:\\ 0 - turns OFF the internal reference.(default)\\ 1 - turns ON the internal reference. | 
 +| **intRef?** | Displays the status of the internal reference. | 
 +| **ldacPin=** | Sets the output value of LDAC pin. Accepted values:\\ 0 - sets LDAC pin low.(default)\\ 1 - sets LDAC pin high. | 
 +| **ldacPin?** | Displays the value of LDAC pin. |
  
-**Section H** is used to control the Hardware pins of the AD7694R. 
  
-**Section I** is used to perform a readback of all four registers of AD7694R.+Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA.
  
-===== Troubleshooting =====+The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. 
 +{{ :resources:fpga:xilinx:interposer:Terminal_KC705.jpg? }}
  
-In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: +===== Software Project Setup ===== 
-  * Check that the evaluation board is powered as instructed in the board's user guide. +{{page>import_workspace}}
-  * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//**. +
-  * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again.+
  
 ====== More information ====== ====== More information ======
 {{page>ez_common}} {{page>ez_common}}
resources/fpga/xilinx/interposer/ad5694r.txt · Last modified: 09 Jan 2021 00:48 by Robin Getz