This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | Last revision Both sides next revision | ||
resources:fpga:xilinx:interposer:ad5694r [03 Jan 2013 20:42] external edit |
resources:fpga:xilinx:interposer:ad5694r [01 Oct 2013 11:35] Lucian Sin changed source code (without Micrium uC-Probe), added Software Setup, remove programming with Impact |
||
---|---|---|---|
Line 12: | Line 12: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi>AD5694R|EVAL-AD5694RSDZ]]** evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the [[http://micrium.com/page/products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5694RSDZ Evaluation Board with the Xilinx KC705 board. | + | This document presents the steps to setup an environment for using the **[[adi>AD5694R|EVAL-AD5694RSDZ]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5694RSDZ Evaluation Board with the Xilinx KC705 board. |
{{ :resources:fpga:xilinx:interposer:img_ad5694r.jpg?400 }} | {{ :resources:fpga:xilinx:interposer:img_ad5694r.jpg?400 }} | ||
Line 30: | Line 30: | ||
* EVAL-AD5694RSDZ evaluation board user guide | * EVAL-AD5694RSDZ evaluation board user guide | ||
* [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] | * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] | ||
- | * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]] | ||
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 44: | Line 43: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool | + | * UART Terminal (Termite/Tera Term/Hyperterminal), baud rate 115200. |
+ | * The EVAL-AD5694R reference project for Xilinx KC705 FPGA. | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | + | <WRAP round download 80%> | |
- | * {{:resources:fpga:xilinx:interposer:ad5694r_evalboard.zip|Reference Design Files}} | + | \\ |
- | + | * **AD5694R Driver:** https://github.com/analogdevicesinc/no-OS/tree/master/device_drivers/AD5686 | |
- | The following table presents a short description the reference design archive contents. | + | * **AD5694R Commands:** https://github.com/analogdevicesinc/no-OS/tree/master/device_commands/AD5686 |
- | + | * **Xilinx Boards Common Drivers:** https://github.com/analogdevicesinc/no-OS/tree/master/platform_drivers/Xilinx/SDP_Common | |
- | ^ **Folder** ^ **Description** ^ | + | * **EDK KC705 Reference project:** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_sdp_kc705 |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | \\ |
- | | Microblaze | Contains the EDK project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | </WRAP> |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
====== Run the Demonstration Project ====== | ====== Run the Demonstration Project ====== | ||
- | ===== Hardware Setup ===== | + | ===== Hardware setup ===== |
- | <WRAP important>Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page.</WRAP> | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </WRAP> | ||
* Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. | ||
* Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. | ||
- | * Start IMPACT, and double click “//Boundary Scan//”. Right click and select //Initialize Chain//. The program should recognize the Kintex 7 device (see screenshot below). | ||
- | {{ :resources:fpga:xilinx:interposer:impact_config.png?300 }} | ||
- | * Program the KC705 FPGA using the "//Bit/download.bit//" file provided in the reference design archive. | ||
- | * Power the ADI evaluation board. | ||
- | |||
- | At this point everything is set up and it is possible to start the evaluation of the ADI hardware through the controls in the uC-Probe application provided in the reference design. | ||
- | |||
- | ===== Configure uC-Probe ===== | ||
- | |||
- | Launch **uC-Probe** from the **//Start -> All Programs -> Micrium -> uC-Probe//**. | ||
- | |||
- | Select **uC-Probe** options. | ||
- | * Click on the **uC-Probe** icon on the top left portion of the screen. | ||
- | * Click on the **//Options//** button to open the dialog box. | ||
- | |||
- | {{ :resources:fpga:altera:bemicro:ucprobeoptionsbtn.png?300 }} | ||
- | |||
- | Set target board communication protocol as **//RS-232//** | ||
- | * Click on the **//Communication//** tab icon on the top left portion of the dialog box | ||
- | * Select the **//RS-232//** option. | ||
- | |||
- | {{ :resources:fpga:xilinx:interposer:ucprobe_comm.png?300 }} | ||
- | |||
- | Setup **//RS-232//** communication settings | ||
- | * Select the **//RS-232//** option from the **//Communication//** tab. | ||
- | * Select the COM port to which the KC705 board is connected. | ||
- | * Set the Baud Rate to 115200 bps. | ||
- | |||
- | {{ :resources:fpga:xilinx:interposer:ucprobe_rs232.png?300 }} | ||
- | |||
- | * Press **//Apply//** and **//OK//** to exit the options menu. | ||
- | |||
- | ===== Load and Run the Demonstration Project ===== | ||
- | |||
- | * Click the **//Open//** option from the **uC-Probe** menu and select the file **//ucProbeInterface/AD5694R_Interface.wsp//** provided within the reference design files. | ||
- | |||
- | * Before opening the interface **uC-Probe** will ask for a symbols file that must be associated with the interface. Select the file **//ucProbeInterface/ADIEvalBoard.elf//** to be loaded as a symbol file. | ||
- | |||
- | * Run the demonstration project by pressing the **//Play//** button. | ||
- | |||
- | {{ :resources:fpga:altera:bemicro:image081.png?200 }} | ||
- | |||
- | <WRAP tip>In some cases it is possible that the uC-Probe interface will not respond to the commands the first time it is ran. In this situation just stop the interface by pressing the **//Stop//** button and run it again by pressing the **//Play//** button.</WRAP> | ||
- | |||
- | ===== Demonstration Project User Interface ===== | ||
- | |||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5694RSDZ** evaluation board. | ||
- | |||
- | {{ :resources:fpga:altera:bemicro:ad5694r_interface.png?700 }} | ||
- | |||
- | **Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the //ON/OFF// switch. The //Activity// LED turns green when the communication is active. If the //ON/OFF// switch is set to //ON// and the //Activity// LED is //BLACK// it means that there is a communication problem with the board. See the **Troubleshooting** section for indications on how to fix the communication problems. | ||
- | |||
- | **Section B** is used to select the //Command// to be sent to the DAC. The definition of each command is available in Table 7 of the part's datasheet. | ||
- | |||
- | **Section C** is used to select the //Address// of the registers to be affected by the command, if the command is 1, 2 or 3. If the selected command is 5, the //Address// buttons will be used to program the //LDAK MASK REGISTER// for the corresponding DAC. For the other commands, they are ignored. | ||
- | |||
- | **Section D** is used to program the value to be written to the DAC registers. | ||
- | |||
- | **Section E** is used to send the selected command to the DAC. | ||
- | **Section F** is used to configure the databits sent for the command 4. Each DAC's power operation can be configured independently. | + | <WRAP round important 80%> |
+ | \\ | ||
+ | To power on the EVAL-AD5694R evaluation board, you need to apply +6V supply voltage to J3 connector of the board. | ||
+ | </WRAP> | ||
- | **Section G** is used to configure the databits sent for the command 7. If the button is pressed, the Internal reference will be turned off. | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-AD5694R reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **reset!** | Activate a power-on reset. | | ||
+ | | **load=** | Loads selected DAC input register with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | | ||
+ | | **update=** | Update the selected DAC channel with the input register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels. | | ||
+ | | **loadAndUpdate=** | Loads and updates the selected DAC with a given value. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ value:\\ 0 .. 4095 - value to be written in register. | | ||
+ | | **pwrMode=** | Set up the Power Mode of a selected channel. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ power mode:\\ 0 - normal operation.\\ 1 - 1KOhm to GND.\\ 2 - 100KOhms to GND.\\ 3 - three-state. | | ||
+ | | **pwrMode?** | Displays the power mode for one selected DAC. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D. | | ||
+ | | **ldacMask=** | Set up the LDAC mask register. Accepted values:\\ channel:\\ 0 - select channel A.\\ 1 - select channel B.\\ 2 - select channel C.\\ 3 - select channel D.\\ 4 - select all channels.\\ set/reset mask:\\ 0 - reset LDAC mask for the selected channel.\\ 1 - set LDAC mask for the selected channel. | | ||
+ | | **ldacMask?** | Displays the LDAC register. | | ||
+ | | **intRef=** | Turns ON or OFF the internal reference. Accepted values:\\ 0 - turns OFF the internal reference.(default)\\ 1 - turns ON the internal reference. | | ||
+ | | **intRef?** | Displays the status of the internal reference. | | ||
+ | | **ldacPin=** | Sets the output value of LDAC pin. Accepted values:\\ 0 - sets LDAC pin low.(default)\\ 1 - sets LDAC pin high. | | ||
+ | | **ldacPin?** | Displays the value of LDAC pin. | | ||
- | **Section H** is used to control the Hardware pins of the AD7694R. | ||
- | **Section I** is used to perform a readback of all four registers of AD7694R. | + | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |
- | ===== Troubleshooting ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ :resources:fpga:xilinx:interposer:Terminal_KC705.jpg? }} | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | ===== Software Project Setup ===== |
- | * Check that the evaluation board is powered as instructed in the board's user guide. | + | {{page>import_workspace}} |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//**. | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
{{page>ez_common}} | {{page>ez_common}} |