This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5629 [30 Sep 2013 17:26] – changed source code (without Micrium uC-Probe), added Software Setup, remove programming with Impact Lucian Sin | resources:fpga:xilinx:interposer:ad5629 [22 Jul 2019 13:40] – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 51: | Line 51: | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
\\ | \\ | ||
- | * **AD5629R Driver:** https:// | + | * **AD5629R Driver:** https:// |
* **AD5629R Commands:** https:// | * **AD5629R Commands:** https:// | ||
* **Xilinx Boards Common Drivers:** https:// | * **Xilinx Boards Common Drivers:** https:// | ||
Line 80: | Line 80: | ||
| **reset!** | Makes a power-on reset. | | | **reset!** | Makes a power-on reset. | | ||
| **powerMode=** | Selects a given power mode for selected DAC. Accepted values:\\ channel:\\ 0 .. 7 - selected DAC A .. H.\\ power mode:\\ 0 - normal operation.\\ 1 - 1KOhm to GND.\\ 2 - 100KOhms to GND.\\ 3 - three-state. | | | **powerMode=** | Selects a given power mode for selected DAC. Accepted values:\\ channel:\\ 0 .. 7 - selected DAC A .. H.\\ power mode:\\ 0 - normal operation.\\ 1 - 1KOhm to GND.\\ 2 - 100KOhms to GND.\\ 3 - three-state. | | ||
- | | **powerMode? | + | | **powerMode? |
- | | **intRef=** | Writes to the DAC register. Accepted values:\\ 0 - turns off the internal reference.\\ 1 - turns on the internal reference. | | + | | **intRef=** | Turns on/ |
| **intRef?** | Displays the status of the internal reference. | | | **intRef?** | Displays the status of the internal reference. | | ||
| **loadN=** | Loads selected DAC register with a given value. Accepted values:\\ channel:\\ 0 .. 7 - selected DAC A .. H.\\ 15 - all DACs.\\ value:\\ 0 .. 4095 - value to be written in register. | | | **loadN=** | Loads selected DAC register with a given value. Accepted values:\\ channel:\\ 0 .. 7 - selected DAC A .. H.\\ 15 - all DACs.\\ value:\\ 0 .. 4095 - value to be written in register. | | ||
Line 105: | Line 105: | ||
The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. | ||
{{ : | {{ : | ||
- | |||
===== Software Project Setup ===== | ===== Software Project Setup ===== | ||
{{page> | {{page> |