This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:xilinx:interposer:ad5421 [06 Sep 2013 15:48] – added link to EDK KC705 reference project on Github Lucian Sin | resources:fpga:xilinx:interposer:ad5421 [02 Oct 2013 14:22] – remove reference_design_files.zip, changed commands, remove quick start evaluation Lucian Sin | ||
---|---|---|---|
Line 50: | Line 50: | ||
<WRAP round download 80%> | <WRAP round download 80%> | ||
\\ | \\ | ||
- | * {{: | ||
* **AD5421 Driver:** https:// | * **AD5421 Driver:** https:// | ||
* **AD5421 Commands:** https:// | * **AD5421 Commands:** https:// | ||
Line 73: | Line 72: | ||
To power on the EVAL-AD5421 evaluation board, you need to provide external differential supply voltage from LOOP- to LOOP+ (for more information see: [[adi>/ | To power on the EVAL-AD5421 evaluation board, you need to provide external differential supply voltage from LOOP- to LOOP+ (for more information see: [[adi>/ | ||
</ | </ | ||
- | |||
- | ===== Quick start evaluation ===== | ||
- | For a quick start evaluation, run the **download.bat** script located in the **SDK/ | ||
- | |||
- | <WRAP round info 80%> | ||
- | \\ | ||
- | The **download.bat** script assumes that the Xilinx ISE Design Suite 14.6 is installed at this path: **C:/ | ||
- | </ | ||
- | |||
- | If programming was successful, you should be seeing the command messages appear on the terminal. | ||
===== Reference Project Overview ===== | ===== Reference Project Overview ===== |