This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision | ||
resources:fpga:xilinx:interposer:ad5172 [17 Feb 2012 15:58] Andrei Cozma Approved |
resources:fpga:xilinx:interposer:ad5172 [09 Jan 2021 00:48] (current) Robin Getz user interwiki links |
||
---|---|---|---|
Line 11: | Line 11: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This document presents the steps to setup an environment for using the **[[adi>AD5172|EVAL-AD5172SDZ]]** evaluation board together with the Xilinx KC705 FPGA board, the Xilinx Embedded Development Kit (EDK) and the [[http://micrium.com/page/products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5172SDZ Evaluation Board with the Xilinx KC705 board. | + | This document presents the steps to setup an environment for using the **[[adi>AD5172|EVAL-AD5172SDZ]]** evaluation board together with the Xilinx KC705 FPGA board and the Xilinx Embedded Development Kit (EDK). Below is presented a picture of the EVAL-AD5172SDZ Evaluation Board with the Xilinx KC705 board. |
{{ :resources:fpga:xilinx:interposer:ad5172.jpg?400 }} | {{ :resources:fpga:xilinx:interposer:ad5172.jpg?400 }} | ||
- | For component evaluation and performance purposes, as opposed to quick prototyping, the user is directed to Analog Devices [[/resources/eval/sdp|System Demonstration Platform]] (**SDP**). The **SDP** consists of a: | + | {{page>common_sdp}} |
- | * a controller board, like the **[[resources/eval/sdp/sdp-b|EVAL-SDP-CB1Z]] (SDP-B)** | + | |
- | * a compatible Analog Devices SDP [[adi>sdp#exallist|product evaluation board]] | + | |
- | * corresponding PC software | + | |
- | The EVAL-SDP-CB1Z controller board is part of Analog Devices SDP providing USB 2.0 high-speed connectivity to a PC computer running specific component evaluation software. Each SDP evaluation daughter board includes the necessary installation files needed for this performance testing. It's expected that the analog performance on the two platforms may differ. | + | |
Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5172SDZ** Evaluation Board. | Below is presented a picture of **SDP-B** Controller Board with the **EVAL-AD5172SDZ** Evaluation Board. | ||
Line 32: | Line 28: | ||
* [[adi>AD5172|AD5172 Product Info]] - pricing, samples, datasheet | * [[adi>AD5172|AD5172 Product Info]] - pricing, samples, datasheet | ||
* [[adi>/static/imported-files/user_guides/UG-243.pdf|EVAL-AD5172SDZ evaluation board user guide]] | * [[adi>/static/imported-files/user_guides/UG-243.pdf|EVAL-AD5172SDZ evaluation board user guide]] | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] | + | * [[xilinx>products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] |
- | * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]] | + | |
====== Getting Started ====== | ====== Getting Started ====== | ||
Line 41: | Line 36: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * [[http://www.xilinx.com/products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] | + | * [[xilinx>products/boards-and-kits/EK-K7-KC705-G.htm | Xilinx KC705 FPGA board]] |
* FMC-SDP adapter board | * FMC-SDP adapter board | ||
* **EVAL-AD5172** evaluation board | * **EVAL-AD5172** evaluation board | ||
Line 47: | Line 42: | ||
===== Required Software ===== | ===== Required Software ===== | ||
- | * Xilinx ISE 13.4 (Programmer (IMPACT) is sufficient for the demo and is available on Webpack). | + | * Xilinx ISE 14.6. |
- | * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool | + | * UART Terminal (Termite/Tera Term/Hyperterminal), baud rate 115200. |
===== Downloads ===== | ===== Downloads ===== | ||
+ | <WRAP round download 80%> | ||
+ | \\ | ||
+ | * **AD5172 Driver:** https://github.com/analogdevicesinc/no-OS/tree/master/device_drivers/AD5172 | ||
+ | * **AD5172 Commands:** https://github.com/analogdevicesinc/no-OS/tree/master/device_commands/AD5172 | ||
+ | * **Xilinx Boards Common Drivers:** https://github.com/analogdevicesinc/no-OS/tree/master/platform_drivers/Xilinx/SDP_Common | ||
+ | * **EDK KC705 Reference project:** https://github.com/analogdevicesinc/fpgahdl_xilinx/tree/master/cf_sdp_kc705 | ||
+ | \\ | ||
+ | </WRAP> | ||
- | * {{:resources:fpga:xilinx:interposer:ad5172_evalboard.zip|Reference Design Files}} | + | ===== Hardware setup ===== |
- | The following table presents a short description the reference design archive contents. | + | <WRAP round important 80%> |
+ | \\ | ||
+ | Before connecting the ADI evaluation board to the Xilinx KC705 make sure that the VADJ_FPGA voltage of the KC705 is set to 3.3V. For more details on how to change the setting for VADJ_FPGA visit the Xilinx KC705 product page. | ||
+ | </WRAP> | ||
- | ^ **Folder** ^ **Description** ^ | + | * Use the FMC-SDP interposer to connect the ADI evaluation board to the Xilinx KC705 board on the FMC LPC connector. |
- | | Bit | Contains the KC705 configuration file that can be used to program the system for quick evaluation. | | + | * Connect the JTAG and UART cables to the KC705 and power up the FPGA board. |
- | | Microblaze | Contains the EDK 13.4 project for the Microblaze softcore that will be implemented in the KC705 FPGA. | | + | |
- | | Software | Contains the source files of the software project that will be run by the Microblaze processor.| | + | |
- | | uCProbeInterface | Contains the uCProbe interface and the .elf symbols file used by uC-Probe to access data from the Microbalze memory. | | + | |
- | ====== Run the Demonstration Project ====== | + | ===== Reference Project Overview ===== |
+ | The following commands were implemented in this version of EVAL-AD5172 reference project for Xilinx KC705 FPGA board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | **help?** | Displays all available commands. | | ||
+ | | **rdac=** | Load the wiper register with a give value. Accepted values:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register.\\ value:\\ 0 .. 255 - value to be written in register. | | ||
+ | | **rdac?** | Read back the value of the wiper register. Accepted values:\\ channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **wbuf1?** | Read back the value of the Wiper Buffer in voltage. (VDD=3.2V) | | ||
+ | | **shutdown=** | Shutdown connects wiper to B terminal and open circuits the A terminal. channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
+ | | **shutdown?** | Notify about the state of the selected RDAC. channel:\\ 0 - select RDAC 1 wiper register.\\ 1 - select RDAC 2 wiper register. | | ||
- | {{page>ucprobe_common}} | + | Commands can be executed using a serial terminal connected to the UART peripheral of Xilinx KC705 FPGA. |
- | ===== Demonstration Project User Interface ===== | + | The following image shows a generic list of commands in a serial terminal connected to Xilinx KC705 FPGA's UART peripheral. |
+ | {{ :resources:fpga:xilinx:interposer:Terminal_KC705.jpg? }} | ||
- | The following figure presents the **uC-Probe** interface that can be used for monitoring and controlling the operation of the **EVAL-AD5172SDZ** evaluation board. | + | ===== Software Project Setup ===== |
- | + | {{page>import_workspace}} | |
- | {{ :resources:fpga:altera:bemicro:ad5172interface.png?700 }} | + | |
- | + | ||
- | **Section A** is used to activate the board and monitor activity. The communication with the board is activated / deactivated by toggling the **//ON/OFF//** switch. The **//Activity//** LED turns green when the communication is active. If the **//ON/OFF//** switch is set to **//ON//** and the **//Activity//** LED is **//BLACK//** it means that there is a communication problem with the board. See the **Troubleshooting** section for indications on how to fix the communication problems. | + | |
- | + | ||
- | **Section B** is used to update the RDAC registers, to switch the device to shutdown mode and to program the wiper permanently.The RDAC registers can be updated by selecting a desirable value on the slider and clicking **//Load RDACx//**. | + | |
- | * **//Shutdown//**: When it is pressed, connects wiper to B terminal and open circuits the A terminal. It does not change the contents of the wiper register. When it is released, the previous latch settings put the wiper in the same resistance setting prior to shutdown. | + | |
- | * **//Program//**: When it is pressed, programs the wiper permanently. The **//Fuse Status//** numeric box shows the status of the device's fuse and can have the followin values: 0 - ready, 2 - error, 3 - success. | + | |
- | + | ||
- | **Section C** is used to send one or two bytes to the AD5172 circuit. A customized I2C data-word can be sent by manually switching the buttons from 0 to 1 or from 1 to 0 as desired and then toggling the **//Send Data//** switch. The number of bytes to send can be selected by switching the **//Bytes to Send//** switch to 1 or 2. | + | |
- | + | ||
- | ===== Troubleshooting ===== | + | |
- | + | ||
- | In case there is a communication problem with the board the follwing actions can be perfomed in order to try to fix the issues: | + | |
- | * Check that the evaluation board is powered as instructed in the board's user guide. | + | |
- | * In uC-Probe refresh the symbols file by right-clicking on the **//System Browser//** window and selecting **//Refresh Symbols//**. | + | |
- | * If the communication problem persists even after performing the previous steps, restart the uC-Probe application and try to run the interface again. | + | |
====== More information ====== | ====== More information ====== | ||
- | * [[ez>community/fpga|ask questions about the FPGA reference design]] | + | * [[resources:tools-software:linux-drivers:misc:dpot|AD5172 Digital Potentiometer Linux Driver]] |
+ | {{page>ez_common}} |