There are many times creating a graphics image, and including it into an FPGA project is necessary. The goal of this tutorial is to show you the various methods of doing this. The various methods will differ, depending on the size or depth of the image.
The Linux kernel uses a “compressed” image format, which creates a header file from a Colour_look-up_table scheme. Since it uses the same format used in the Linux kernel, there are some Linux utiltites needed:
rgetz@curly:~/logos$ wget http://upload.wikimedia.org/wikipedia/commons/8/86/Analog_Devices_Logo.svg --2011-12-20 13:41:47-- http://upload.wikimedia.org/wikipedia/commons/8/86/Analog_Devices_Logo.svg Resolving upload.wikimedia.org... 208.80.152.211 Connecting to upload.wikimedia.org|208.80.152.211|:80... connected. HTTP request sent, awaiting response... 200 OK Length: 4525 (4.4K) [image/svg+xml] Saving to: `Analog_Devices_Logo.svg' 100%[=============================================================>] 4,525 21.4K/s in 0.2s 2011-12-20 13:41:48 (21.4 KB/s) - `Analog_Devices_Logo.svg' saved [4525/4525]
rgetz@curly:~/logos$ gimp Analog_Devices_Logo.svgHere I “save as” a
.ppm
file.pnmquant
application quantizes the colors in a Netpbm image to a smaller set, and the pnmnoraw application, converts this into a file which can be processed by the script to create a header file. rgetz@curly:~/fooo$ pnmquant 224 Analog_Devices_Logo.ppm | pnmnoraw > Analog_Devices_Logo_clut224.ppm
rgetz@curly:~/logos$ ~/linux/scripts/pnmtologo -t clut224 Analog_Devices_Logo_clut224.ppm -o Analog_Devices_Logo_clut224.h -n Analog_Devices_logo
rgetz@curly:~/logos$ sed -i -e 's:__initdata::' -e 's:__initconst::' Analog_Devices_Logo_clut224.h rgetz@curly:~/logos$ sed -i '/^#include/d' Analog_Devices_Logo_clut224.h rgetz@curly:~/logos$ sed -i '/^space*\.data/d' Analog_Devices_Logo_clut224.h rgetz@curly:~/logos$ sed -i '/^space*\.clut/d' Analog_Devices_Logo_clut224.h rgetz@curly:~/logos$ sed -i '/^space*\.type/d' Analog_Devices_Logo_clut224.h rgetz@curly:~/logos$ sed -i 's:linux_logo:logo:' Analog_Devices_Logo_clut224.h
And that's it - it's just a matter of including the image data into your application.
#include "Analog_Devices_Logo_clut224.h" int main(void) { for (h = 0; h < height; h++) { for (w = 0; w < width; w++) { pixel_data = Analog_Devices_data[pixel_cnt]; if ((pixel_data < 32) || (pixel_data > 252)) { printf("Error: pixel data at(%d): 0x%02x\n", pixel_cnt, pixel_data); return(-1); } pixel_data = pixel_data - 32; pixel_r = Analog_Devices_clut[(pixel_data * 3) + 0]; pixel_g = Analog_Devices_clut[(pixel_data * 3) + 1]; pixel_b = Analog_Devices_clut[(pixel_data * 3) + 2]; waddr = baseaddr + (h*2048) + (w*4); wdata = (pixel_r << 16) | (pixel_b << 8) | pixel_g; printf("mwr 0x%08x 0x%08x\n", waddr, wdata); pixel_cnt = pixel_cnt + 1; } waddr = baseaddr + (h*2048); printf("set logfile [open \"demo_img.log\" \"a\"]\n"); printf("puts $logfile [mrd 0x%08x]\n", waddr); printf("close $logfile\n"); } }
Once this is done, you can have a quick look, to see how big things are.
rgetz@curly:~/logos$ readelf -s Analog_Devices_Logo | grep Analog_Devices 42: 0000000000601040 34900 OBJECT LOCAL DEFAULT 24 Analog_Devices_logo_data 43: 00000000006098a0 672 OBJECT LOCAL DEFAULT 24 Analog_Devices_logo_clut
The data and colour lookup table are 35,572 bytes (~35k) to represent a 349 pixel x 100 pixel (RGB) image (uncompressed, this would be 104,700 bytes) - the clut data is 1/3 of the size, and minimal overhead.
U-Boot or Das_U-Boot also includes tools for including graphics as splash screens. All that is needed to do, is download a recent version of U-Boot, and do a:
rgetz@curly:~/u-boot$ make tools-all HOST_TOOLS_ALL=y
This will provide you with multple tools which you can used to create the header files.
bmp_logo
takes a 256-colour bitmap file, and creates a header file. This is similar to the Linux tools in size.
rgetz@curly:~/u-boot$ ~/u-boot/tools/bmp_logo Analog_Devices_Logo.bmp > Analog_Devices_Logo_bmp.h
easylogo
takes a 24-bit TGA image, and can output YUYV, RGB888, RGB565, and optionally Compress with gzip.
rgetz@curly:~/fooo$ ppmtotga -rgb -norle Analog_Devices_Logo.ppm > Analog_Devices_Logo.tga rgetz@curly:~/fooo$ ~/u-boot/tools/easylogo/easylogo Analog_Devices_Logo.tga -r Analog_Logo Analog_Devices_Logo_tga.h Using 24-bit RGB888 Output Fromat Doing 'Analog_Devices_Logo_tga.h' (Analog_Logo) from 'Analog_Devices_Logo.tga'...LSS rgetz@curly:~/fooo$ ~/u-boot/tools/easylogo/easylogo Analog_Devices_Logo.tga -r -g Analog_Logo Analog_Devices_Logo_tga_zip.h Using 24-bit RGB888 Output Fromat Compressing with gzip Doing 'Analog_Devices_Logo_tga_zip.h' (Analog_Logo) from 'Analog_Devices_Logo.tga'...LSS
Using the gzip version, does require a little more processing on the target (to decompress things), but offers substational saving in space.
rgetz@curly:~/fooo$ readelf -s Analog_Devices_Logo | grep Analog -i 41: 0000000000000000 0 FILE LOCAL DEFAULT ABS Analog_Devices_Logo.c 59: 00000000006032c0 32 OBJECT GLOBAL DEFAULT 24 Analog_Logo 64: 0000000000601040 8805 OBJECT GLOBAL DEFAULT 24 DEF_ANALOG_LOGO_DATA
This is 8805 bytes, to store the same 349 pixel x 100 pixel (RGB) image (uncompressed, this would be 104,700 bytes) - the gzip data is 1/12 of the size, making up for the extra processing required. For decompression, check out the ./contrib/puff
lib/application in zlib compression library.