Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Next revision Both sides next revision
resources:fpga:xilinx:fmc:ad9739a [11 Nov 2016 11:08]
LucianS [Supported Devices] increase size for board picture
resources:fpga:xilinx:fmc:ad9739a [29 Sep 2017 09:28]
AdrianC [Quick Start Guide] Added ZC706 to the tested boards.
Line 19: Line 19:
 ===== Supported Carriers ===== ===== Supported Carriers =====
  
-  * [[xilinx>​ML605]] +  * [[xilinx>​ML605]] ​Legacy (limited support) 
-  * [[xilinx>​KC705]]  +  * [[xilinx>​KC705]] ​Legacy (limited support) 
-  * [[xilinx>​VC707]]  +  * [[xilinx>​VC707]] ​Legacy (limited support) 
-  * [[xilinx>​AC701]]+  * [[xilinx>​AC701]] ​Legacy (limited support) 
 +  * [[xilinx>​ZC706]] LPC Slot
 ===== Quick Start Guide ===== ===== Quick Start Guide =====
  
-The reference design has been tested on ML605(Virtex-6),​ KC705(Kintex-7) ​and VC707(Virtex-7) boards. The notes below refer to ML605, however the procedure is same for the other boards. Please make sure that you have downloaded and are using the correct design files for your board. All you need is the hardware and a PC running a UART terminal. ​+The reference design has been tested on ML605(Virtex-6),​ KC705(Kintex-7)VC707(Virtex-7) and ZC706 (Zynq) boards. The notes below refer to ML605, however the procedure is same for the other boards. Currently, we fully support only the ZC706 Vivado based design. Please make sure that you have downloaded and are using the correct design files for your board. All you need is the hardware and a PC running a UART terminal. ​
  
 {{analogTV>​1423927819001}} {{analogTV>​1423927819001}}
resources/fpga/xilinx/fmc/ad9739a.txt · Last modified: 22 Jul 2019 13:59 by AndreiD1994