Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:fpga:xilinx:fmc:ad9739a [09 Jan 2021 00:39] – user interwiki links Robin Getz | resources:fpga:xilinx:fmc:ad9739a [12 Feb 2021 11:55] (current) – [Quick Start Guide] -update video tutorial link Dan Nechita |
---|
The reference design has been tested on ML605(Virtex-6), KC705(Kintex-7), VC707(Virtex-7) and ZC706 (Zynq) boards. The notes below refer to ML605, however the procedure is same for the other boards. Currently, we fully support only the ZC706 Vivado based design. Please make sure that you have downloaded and are using the correct design files for your board. All you need is the hardware and a PC running a UART terminal. | The reference design has been tested on ML605(Virtex-6), KC705(Kintex-7), VC707(Virtex-7) and ZC706 (Zynq) boards. The notes below refer to ML605, however the procedure is same for the other boards. Currently, we fully support only the ZC706 Vivado based design. Please make sure that you have downloaded and are using the correct design files for your board. All you need is the hardware and a PC running a UART terminal. |
| |
A video tutorial is available [[adi>en/education/education-library/videos/1423927819001.html|here]] | A video tutorial is available: {{analogTV>1423927819001}} |
==== Required Hardware ==== | ==== Required Hardware ==== |
* ML605/KC705/VC707/AC701 board (use the corresponding design file). | * ML605/KC705/VC707/AC701 board (use the corresponding design file). |