Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
resources:fpga:xilinx:fmc:ad9467 [03 Jan 2021 22:12] – fix links Robin Getzresources:fpga:xilinx:fmc:ad9467 [09 Jan 2021 00:39] – user interwiki links Robin Getz
Line 23: Line 23:
 <WRAP round important 100%> <WRAP round important 100%>
 \\ \\
-Please make sure you have removed or inserted the corresponding components on the board to select the desired clock path. The schematic of the board can be found at the [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section.+Please make sure you have removed or inserted the corresponding components on the board to select the desired clock path. The schematic of the board can be found at the [[/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section.
 </WRAP> </WRAP>
  
Line 37: Line 37:
 ==== Required Software ==== ==== Required Software ====
  
-  * We're upgrade the Xilinx tools on every release. The supported version number can be found in our HDL [[https://wiki.analog.com/resources/fpga/docs/releases | release page]].  +  * We're upgrade the Xilinx tools on every release. The supported version number can be found in our HDL [[/resources/fpga/docs/releases | release page]].  
   * A UART terminal (Tera Term/Hyperterminal), baud rate 115200.   * A UART terminal (Tera Term/Hyperterminal), baud rate 115200.
  
Line 43: Line 43:
  
 <WRAP round info 100%> <WRAP round info 100%>
-Instruction about how to build the HDL design and generate a bit stream can be found [[https://wiki.analog.com/resources/fpga/docs/build | here]]. +Instruction about how to build the HDL design and generate a bit stream can be found [[/resources/fpga/docs/build | here]]. 
 </WRAP> </WRAP>
  
Line 75: Line 75:
   * Capture data from the AD9467 using DMA transfers   * Capture data from the AD9467 using DMA transfers
  
-The software project contains 3 components: the AD9467-FMC-EBZ reference design files, the AD9467 driver and the AD9517 driver. All the components have to be downloaded from the links provided in the [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads|Downloads]] section.+The software project contains 3 components: the AD9467-FMC-EBZ reference design files, the AD9467 driver and the AD9517 driver. All the components have to be downloaded from the links provided in the [[/resources/fpga/xilinx/fmc/ad9467#downloads|Downloads]] section.
  
 ==== AD9467 Software Driver ==== ==== AD9467 Software Driver ====
Line 109: Line 109:
  
 <WRAP round info 100%> <WRAP round info 100%>
-Instruction about how to create a software application can be found [[http://wiki.analog.com/resources/fpga/xilinx/software_setup|here]]. +Instruction about how to create a software application can be found [[/resources/fpga/xilinx/software_setup|here]]. 
 </WRAP> </WRAP>
  
-The exact location of the no-OS source files can be found in the [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section. +The exact location of the no-OS source files can be found in the [[/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section. 
      
 ===== Downloads ===== ===== Downloads =====
resources/fpga/xilinx/fmc/ad9467.txt · Last modified: 06 Nov 2023 14:23 by iulia Moldovan