Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:fpga:xilinx:fmc:ad9467 [04 Jun 2018 14:45] – Updated build and release instructions. Pointing to 2018_r1 release as the latest release Adrian Costina | resources:fpga:xilinx:fmc:ad9467 [09 Jan 2021 00:39] – user interwiki links Robin Getz |
---|
===== Evaluation Board Hardware ===== | ===== Evaluation Board Hardware ===== |
| |
To find out more information about the [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-documentation|evaluation board]] hardware, default operation and jumper selection settings please read the Evaluation User Guide of the board. ([[http://www.analog.com/media/en/technical-documentation/user-guides/UG-200.pdf|UG200]]) | To find out more information about the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-documentation|evaluation board]] hardware, default operation and jumper selection settings please read the Evaluation User Guide of the board. ([[adi>media/en/technical-documentation/user-guides/UG-200.pdf|UG200]]) |
| |
{{:resources:fpga:xilinx:fmc:ad9467_fmc.jpg?300|}} | {{:resources:fpga:xilinx:fmc:ad9467_fmc.jpg?300|}} |
The evaluation board can be set up to be clocked from the **crystal oscillator**, Y200. This oscillator is a low phase noise oscillator from Vectron (VCC6-QCD-250M000). If this clock source is desired, install C205 and C206 and remove C202. Jumper P200 is used to disable the oscillator from running. | The evaluation board can be set up to be clocked from the **crystal oscillator**, Y200. This oscillator is a low phase noise oscillator from Vectron (VCC6-QCD-250M000). If this clock source is desired, install C205 and C206 and remove C202. Jumper P200 is used to disable the oscillator from running. |
| |
A **differential LVPECL or LVDS clock driver** can also be used to clock the ADC input using the [[http://www.analog.com/media/en/technical-documentation/data-sheets/AD9517-4.pdf|AD9517]]. Populate C304, C305, C306, and C307 with 0.1 µF capacitors for one drive option or the other and remove C209 and C210 to disconnect the default clock path inputs. The AD9517 has many SPI-selectable options that are set to a default mode of operation. Consult the AD9517 data sheet for more information about these and other options. | A **differential LVPECL or LVDS clock driver** can also be used to clock the ADC input using the [[adi>media/en/technical-documentation/data-sheets/AD9517-4.pdf|AD9517]]. Populate C304, C305, C306, and C307 with 0.1 µF capacitors for one drive option or the other and remove C209 and C210 to disconnect the default clock path inputs. The AD9517 has many SPI-selectable options that are set to a default mode of operation. Consult the AD9517 data sheet for more information about these and other options. |
| |
<WRAP round important 100%> | <WRAP round important 100%> |
\\ | \\ |
Please make sure you have removed or inserted the corresponding components on the board to select the desired clock path. The schematic of the board can be found at the [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section. | Please make sure you have removed or inserted the corresponding components on the board to select the desired clock path. The schematic of the board can be found at the [[/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section. |
</WRAP> | </WRAP> |
| |
==== Required Software ==== | ==== Required Software ==== |
| |
* We're upgrade the Xilinx tools on every release. The supported version number can be found in our HDL [[https://wiki.analog.com/resources/fpga/docs/releases | release page]]. | * We're upgrade the Xilinx tools on every release. The supported version number can be found in our HDL [[/resources/fpga/docs/releases | release page]]. |
* A UART terminal (Tera Term/Hyperterminal), baud rate 115200. | * A UART terminal (Tera Term/Hyperterminal), baud rate 115200. |
| |
| |
<WRAP round info 100%> | <WRAP round info 100%> |
Instruction about how to build the HDL design and generate a bit stream can be found [[https://wiki.analog.com/resources/fpga/docs/build | here]]. | Instruction about how to build the HDL design and generate a bit stream can be found [[/resources/fpga/docs/build | here]]. |
</WRAP> | </WRAP> |
| |
The reference design is built on a ARM/Microblaze based system tailored for Linux. A functional block diagram of the design is given below. | The reference design is built on a ARM/Microblaze based system tailored for Linux. A functional block diagram of the design is given below. |
| |
{{:resources:fpga:xilinx:fmc:cf_ad9467_bd.jpg?400|block diagram}} | === Xilinx block diagram === |
| {{:resources:fpga:xilinx:fmc:ad9467_ebz:ad9467_fmc.svg?500|Xilinx HDL Block Diagram}} |
| |
| === AD9467 FMC Card block diagram === |
| {{:resources:fpga:xilinx:fmc:ad9467_ebz:ad9467_fmc_card.svg?400|Xilinx HDL Block Diagram}} |
| |
Through an SPI interface, the software can access the AD9467/AD9517-4 registers, given the possibility to initialize and configure the ADC and/or clock chip. | Through an SPI interface, the software can access the AD9467/AD9517-4 registers, given the possibility to initialize and configure the ADC and/or clock chip. |
* Capture data from the AD9467 using DMA transfers | * Capture data from the AD9467 using DMA transfers |
| |
The software project contains 3 components: the AD9467-FMC-EBZ reference design files, the AD9467 driver and the AD9517 driver. All the components have to be downloaded from the links provided in the [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads|Downloads]] section. | The software project contains 3 components: the AD9467-FMC-EBZ reference design files, the AD9467 driver and the AD9517 driver. All the components have to be downloaded from the links provided in the [[/resources/fpga/xilinx/fmc/ad9467#downloads|Downloads]] section. |
| |
==== AD9467 Software Driver ==== | ==== AD9467 Software Driver ==== |
| |
<WRAP round info 100%> | <WRAP round info 100%> |
Instruction about how to create a software application can be found [[http://wiki.analog.com/resources/fpga/xilinx/software_setup|here]]. | Instruction about how to create a software application can be found [[/resources/fpga/xilinx/software_setup|here]]. |
</WRAP> | </WRAP> |
| |
The exact location of the no-OS source files can be found in the [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section. | The exact location of the no-OS source files can be found in the [[/resources/fpga/xilinx/fmc/ad9467#downloads|Download]] section. |
| |
===== Downloads ===== | ===== Downloads ===== |
* **AD9467 Driver: ** https://github.com/analogdevicesinc/no-OS/tree/2018_R1/drivers/ad9467 | * **AD9467 Driver: ** https://github.com/analogdevicesinc/no-OS/tree/2018_R1/drivers/ad9467 |
* **AD9517 Driver: ** https://github.com/analogdevicesinc/no-OS/tree/2018_R1/drivers/ad9517 | * **AD9517 Driver: ** https://github.com/analogdevicesinc/no-OS/tree/2018_R1/drivers/ad9517 |
* **AD9467-FMC-EBZ Reference Design: ** https://github.com/analogdevicesinc/no-OS/tree/2018_R1/AD9467-FMC-EBZ | * **AD9467-FMC-EBZ Reference Design: ** https://github.com/analogdevicesinc/no-OS/tree/2018_R1/ad9467-fmc-ebz |
</WRAP> | </WRAP> |
| |
* {{:resources:fpga:xilinx:fmc:9467fmc01c_sch.pdf|Rev C Schematics for the card}} | * {{:resources:fpga:xilinx:fmc:9467fmc01c_sch.pdf|Rev C Schematics for the card}} |
* {{:resources:fpga:xilinx:fmc:9467fmc01c_bom.xls|Bill of Materials for Rev C}} | * {{:resources:fpga:xilinx:fmc:9467fmc01c_bom.xls|Bill of Materials for Rev C}} |
* {{:resources:fpga:xilinx:fmc:9467fmc01c.zip|AD9467FMC-250EBZ Gerber/Layout Fabrication Files}} | * {{ :resources:fpga:xilinx:fmc:9467fmc01c.zip|AD9467FMC-250EBZ Gerber/Layout Fabrication Files}} |
**Note:** C302 and C303 are not installed as indicated in the Schematic and BOM. | **Note:** C302 and C303 are not installed as indicated in the Schematic and BOM. |
</WRAP> | </WRAP> |