Wiki

This version is outdated by a newer approved version.DiffThis version (02 Jan 2013 22:37) was approved by Robin Getz.The Previously approved version (04 Oct 2012 23:55) is available.Diff

This is an old revision of the document!


AD-FMComms1-EBZ : Using the reference design

The reference design is a combination of hardware (the FMComms1 Card + the FPGA base platform), the HDL, and the software that is either running on the Microblaze, or ARM Cores.

In all the demos that we support, Linux is a large piece.

Linux Device Drivers

Booting Linux

Normally, when the Linux image is booted, it will search both the LPC and HPC FMC slots for 2 cards. (the same reference design supports MIMO, as a single card). You should see something like this in the kernel log message - which indicates that a single card is plugged into the LPC FMC connector.

# dmesg
[snip]
at24 0-0051: 256 byte 24c02 EEPROM, writable, 1 bytes/write
spi-xcomm: probe of 1-0058 failed with error -5
at24 1-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
cf_axi_adc 7c820000.cf-ad9643-core-lpc: Device Tree Probing 'cf-ad9643-core-lpc'
platform 7c820000.cf-ad9643-core-lpc: Driver cf_axi_adc requests probe deferral
cf_axi_adc 7c800000.cf-ad9643-core-hpc: Device Tree Probing 'cf-ad9643-core-hpc'
platform 7c800000.cf-ad9643-core-hpc: Driver cf_axi_adc requests probe deferral
cf_axi_fft_core 7ee00000.axi-fft: Device Tree Probing 'axi-fft'
cf_axi_fft_core 7ee00000.axi-fft: ADI-FFT (0x10061) at 0x7EE00000 mapped to 0xf0160000, DMA-1, DMA-0 probed
ad9548 spi0.2: Rev. 0xC6 probed
ad9523 spi0.3: probed ad9523-lpc
cf_axi_dds 7a020000.cf-ad9122-core-lpc: Device Tree Probing 'cf-ad9122-core-lpc'
platform 7a020000.cf-ad9122-core-lpc: Driver cf_axi_dds requests probe deferral
cf_axi_dds 7a000000.cf-ad9122-core-hpc: Device Tree Probing 'cf-ad9122-core-hpc'
platform 7a000000.cf-ad9122-core-hpc: Driver cf_axi_dds requests probe deferral
TCP: cubic registered
NET: Registered protocol family 17
cf_axi_adc 7c820000.cf-ad9643-core-lpc: Device Tree Probing 'cf-ad9643-core-lpc'
——-ooooooooooo|oooooooooo—- DCO 0x91
cf_axi_adc 7c820000.cf-ad9643-core-lpc: ADI AIM (0x10061) at 0x7C820000 mapped to 0xf0180000, DMA-0 probed ADC AD9643 as MASTER
cf_axi_adc 7c800000.cf-ad9643-core-hpc: Device Tree Probing 'cf-ad9643-core-hpc'
platform 7c800000.cf-ad9643-core-hpc: Driver cf_axi_adc requests probe deferral
cf_axi_dds 7a020000.cf-ad9122-core-lpc: Device Tree Probing 'cf-ad9122-core-lpc'
-o|o DCI 2
cf_axi_dds 7a020000.cf-ad9122-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (0x10061) at 0x7A020000 mapped to 0xf01a0000, probed DDS AD9122
cf_axi_dds 7a000000.cf-ad9122-core-hpc: Device Tree Probing 'cf-ad9122-core-hpc'
platform 7a000000.cf-ad9122-core-hpc: Driver cf_axi_dds requests probe deferral
cf_axi_adc 7c800000.cf-ad9643-core-hpc: Device Tree Probing 'cf-ad9643-core-hpc'
platform 7c800000.cf-ad9643-core-hpc: Driver cf_axi_adc requests probe deferral
cf_axi_dds 7a000000.cf-ad9122-core-hpc: Device Tree Probing 'cf-ad9122-core-hpc'
platform 7a000000.cf-ad9122-core-hpc: Driver cf_axi_dds requests probe deferral
cf_axi_adc 7c800000.cf-ad9643-core-hpc: Device Tree Probing 'cf-ad9643-core-hpc'
platform 7c800000.cf-ad9643-core-hpc: Driver cf_axi_adc requests probe deferral

You can also check the status of things with:

# cd /sys/bus/iio/devices/
# grep “” iio\:device*/name
iio:device0/name:ad8366-lpc
iio:device1/name:ad9523-lpc
iio:device2/name:adf4351-rx-lpc
iio:device3/name:adf4351-tx-lpc
iio:device4/name:cf-ad9643-core-lpc
iio:device5/name:cf-ad9122-core-lp

Those are the devices that the Linux kernel found.

Running the demo

It's a simple matter of configuring the ethernet on the FPGA platform:

# ifconfig eth0 192.168.1.2 up
# ifconfig eth0
eth0      Link encap:Ethernet  HWaddr 00:0A:35:69:1C:00  
          inet addr:192.168.1.2  Bcast:192.168.1.255  Mask:255.255.255.0
          UP BROADCAST RUNNING  MTU:1500  Metric:1
          RX packets:11 errors:0 dropped:0 overruns:0 frame:0
          TX packets:1 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:3506 (3.4 KiB)  TX bytes:322 (322.0 B)
          Interrupt:10 Memory:40e00000-40e0ffff 
(or by running the udhcpc client)

and then ensuring that the your host PC is attached to the same subnet as the FPGA platform.

From here you can look at things in the time domain, frequency domain, and control the various “knobs” in the platform.

To find the various “knobs”, they are in the sysfs directory.

# cd /sys/devices/axi.0/40800000.i2c/i2c-0/0-0059/spi_master/spi0/spi0.3/iio:device2
# ls
dev
name
out_altvoltage0_ZD_OUTPUT_frequency
out_altvoltage0_ZD_OUTPUT_phase
out_altvoltage0_ZD_OUTPUT_raw
out_altvoltage0_clk_src_vcxo_en
out_altvoltage1_DAC_CLK_frequency
out_altvoltage1_DAC_CLK_phase
out_altvoltage1_DAC_CLK_raw
out_altvoltage1_clk_src_vcxo_en
out_altvoltage2_ADC_CLK_frequency
out_altvoltage2_ADC_CLK_phase
out_altvoltage2_ADC_CLK_raw
out_altvoltage2_clk_src_vcxo_en
out_altvoltage3_clk_src_vcxo_en
out_altvoltage4_DAC_REF_CLK_frequency
out_altvoltage4_DAC_REF_CLK_phase
out_altvoltage4_DAC_REF_CLK_raw
out_altvoltage4_clk_src_vco2_en
out_altvoltage5_TX_LO_REF_CLK_frequency
out_altvoltage5_TX_LO_REF_CLK_phase
out_altvoltage5_TX_LO_REF_CLK_raw
out_altvoltage5_clk_src_vco2_en
out_altvoltage6_DAC_DCO_CLK_frequency
out_altvoltage6_DAC_DCO_CLK_phase
out_altvoltage6_DAC_DCO_CLK_raw
out_altvoltage6_clk_src_vco2_en
out_altvoltage7_clk_src_vco2_en
out_altvoltage8_ADC_SYNC_CLK_frequency
out_altvoltage8_ADC_SYNC_CLK_phase
out_altvoltage8_ADC_SYNC_CLK_raw
out_altvoltage8_clk_src_vco2_en
out_altvoltage9_RX_LO_REF_CLK_frequency
out_altvoltage9_RX_LO_REF_CLK_phase
out_altvoltage9_RX_LO_REF_CLK_raw
out_altvoltage9_clk_src_vco2_en
status
store_eeprom
subsystem
sync
uevent
vco1_frequency
vco2_frequency
vco_frequency_available

You can echo or cat into these files to change the various options.

# cat out_altvoltage1_DAC_CLK_frequency
491520000
# echo 500000000 > out_altvoltage1_DAC_CLK_frequency
# cat out_altvoltage1_DAC_CLK_frequency
983040000
# echo 400000000 > out_altvoltage1_DAC_CLK_frequency
# cat out_altvoltage1_DAC_CLK_frequency
491520000

Just like if you were trying to program the part with specific frequencies, there are only so many options you can pick, so it attempts to pick the “closest” option.

FMC FRU EEPROM Utility

The FRU EEPROM responds to I2C Slave address 0x51.

Dump FRU Board Information

This specifies any shell prompt running on the target

# fru_dump -i /sys/bus/i2c/devices/0-0051/eeprom -b
read 256 bytes from /sys/bus/i2c/devices/0-0051/eeprom
Date of Man  : Tue Sep 18 16:30:00 2012
Manufacture  : Analog Devices
Product Name : FMC Comms 1
Serial Number: D836081
Part Number  : AD-FMCOMMS1-EBZ
Board Rev    : B

Dump FRU Power Information

This specifies any shell prompt running on the target

# fru_dump -i /sys/bus/i2c/devices/0-0051/eeprom -p
read 256 bytes from /sys/bus/i2c/devices/0-0051/eeprom
DC Load
  Output number: 0 (P1 VADJ)
  Nominal Volts:         2500 (mV)
  minimum voltage:       1800 (mV)
  maximum voltage:       2500 (mV)
  Ripple and Noise pk-pk 0000 (mV)
  Minimum current load   0000 (mA)
  Maximum current load   0000 (mA)
DC Load
  Output number: 1 (P1 3P3V)
  Nominal Volts:         3300 (mV)
  minimum voltage:       2970 (mV)
  maximum voltage:       3630 (mV)
  Ripple and Noise pk-pk 0000 (mV)
  Minimum current load   0000 (mA)
  Maximum current load   3000 (mA)
DC Load
  Output number: 2 (P1 12P0V)
  Nominal Volts:         12000 (mV)
  minimum voltage:       10800 (mV)
  maximum voltage:       13200 (mV)
  Ripple and Noise pk-pk 0000 (mV)
  Minimum current load   0000 (mA)
  Maximum current load   1000 (mA)
DC Output
  Output Number: 3 (P1 VIO_B_M2C)
  Nominal volts:              0 (mV)
  Maximum negative deviation: 0 (mV)
  Maximum positive deviation: 0 (mV)
  Ripple and Noise pk-pk:     0 (mV)
  Minimum current draw:       0 (mA)
  Maximum current draw:       0 (mA)
DC Output
  Output Number: 4 (P1 VREF_A_M2C)
  Nominal volts:              0 (mV)
  Maximum negative deviation: 0 (mV)
  Maximum positive deviation: 0 (mV)
  Ripple and Noise pk-pk:     0 (mV)
  Minimum current draw:       0 (mA)
  Maximum current draw:       0 (mA)
DC Output
  Output Number: 5 (P1 VREF_B_M2C)
  Nominal volts:              0 (mV)
  Maximum negative deviation: 0 (mV)
  Maximum positive deviation: 0 (mV)
  Ripple and Noise pk-pk:     0 (mV)
  Minimum current draw:       0 (mA)
  Maximum current draw:       0 (mA)

Dump FRU Connector Information

This specifies any shell prompt running on the target

# fru_dump -i /sys/bus/i2c/devices/0-0051/eeprom -c
read 256 bytes from /sys/bus/i2c/devices/0-0051/eeprom
Single Width Card
P1 is LPC
P1 Bank A Signals needed 68
P1 Bank B Signals needed 0
P1 GBT Transceivers needed 0
Max JTAG Clock 0

AD-FMCOMMS1-EBZ Calibration EEPROM Utility

The Calibration EEPROM responds to I2C Slave address 0x55.

Query best match calibration set for a given Frequency

This specifies any shell prompt running on the target

# xcomm_cal -f 2400 -s /sys/bus/i2c/devices/0-0055/eeprom

--- Best match ENTRY 1 ---
Calibration Frequency:  2400 MHz
DAC I Phase Adjust:             357
DAC Q Phase Adjust:             0
DAC I Offset:           214
DAC Q Offset:           25
DAC I Full Scale Adj:   401
DAC Q Full Scale Adj:   401
ADC I Offset:           -2
ADC Q Offset:           -34
ADC I Gain Adj: 32853
ADC Q Gain Adj: 32768

resources/fpga/xilinx/fmc/ad-fmcomms1-ebz/reference_design.1357162649.txt.gz · Last modified: 02 Jan 2013 22:37 by Robin Getz