FPGA Reference Designs on GitHub :
The repository will not contain Xilinx core generator and IP files. You must obtain these files from Xilinx.
The tar file contains, in most cases, the following files and/or directories. To rebuild the reference design simply double click the XMP file and run the tool. To build SDK, select a workspace and use the C file to build the elf file. Please refer to Xilinx EDK documentation for details.
In the case of Zynq, the same procedure applies, except that you must create a FSBL or run the PS7 initialization tcl scripts before the SDK program.
license.txt | ADI license & copyright information. |
system.mhs | MHS file. |
system.xmp | XMP file (use this file to build the reference design). |
data/ | UCF file and/or DDR MIG project files. |
docs/ | Documentation files (Please note that this wiki page is the documentation for the reference design). |
sw/ | Software (Xilinx SDK) & bit file(s). |
cf_lib/edk/pcores | pcores (if used). |