Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:fpga:peripherals:spi_engine [11 Oct 2021 15:04]
Iulia Moldovan Add footer
resources:fpga:peripherals:spi_engine [13 Oct 2021 08:45]
Iulia Moldovan Edit footer
Line 4: Line 4:
  
 The core component of the SPI Engine framework is a lean but powerful fully programmable execution module, which implements the SPI bus control logic. The SPI Engine execution module is controlled by a command stream which is generated by a separate module. Different command stream master modules are available and can be used depending on the system requirements. For example a software controlled memory mapped command stream offers high flexibility,​ while a offload core which executes a pre-programmed command stream when triggered by an external event allows for very low latency response times. By using a SPI Engine interconnect it is possible to connect multiple command stream master modules to a SPI Engine execution module. The core component of the SPI Engine framework is a lean but powerful fully programmable execution module, which implements the SPI bus control logic. The SPI Engine execution module is controlled by a command stream which is generated by a separate module. Different command stream master modules are available and can be used depending on the system requirements. For example a software controlled memory mapped command stream offers high flexibility,​ while a offload core which executes a pre-programmed command stream when triggered by an external event allows for very low latency response times. By using a SPI Engine interconnect it is possible to connect multiple command stream master modules to a SPI Engine execution module.
 +
  
 ===== Sub-modules ===== ===== Sub-modules =====
Line 11: Line 12:
   * [[.:​spi_engine:​offload|Offload Module]]: Stores a SPI Engine command stream, execution is triggered by an external event   * [[.:​spi_engine:​offload|Offload Module]]: Stores a SPI Engine command stream, execution is triggered by an external event
   * [[.:​spi_engine:​interconnect|Interconnect Module]]: Connects multiple SPI Engine command streams to a SPI Engine execution module   * [[.:​spi_engine:​interconnect|Interconnect Module]]: Connects multiple SPI Engine command streams to a SPI Engine execution module
 +
  
 ===== Interfaces ===== ===== Interfaces =====
Line 17: Line 19:
   * [[.:​spi_engine:​spi_engine_offload_control_interface|SPI Engine Offload Control Interface]]:​ Program the command stream stored in a offload module   * [[.:​spi_engine:​spi_engine_offload_control_interface|SPI Engine Offload Control Interface]]:​ Program the command stream stored in a offload module
   * [[.:​spi_engine:​spi_bus_interface|SPI Bus Interface]]:​ Low-level SPI bus interface   * [[.:​spi_engine:​spi_bus_interface|SPI Bus Interface]]:​ Low-level SPI bus interface
 +
  
 ===== Software ===== ===== Software =====
Line 31: Line 34:
  
   * [[util_sigma_delta_spi|Sigma-Delta SPI Util]]: Helper module for interfacing ADCs from the Analog Devices Sigma-Delta family   * [[util_sigma_delta_spi|Sigma-Delta SPI Util]]: Helper module for interfacing ADCs from the Analog Devices Sigma-Delta family
 +
  
 ===== Examples ===== ===== Examples =====
Line 39: Line 43:
   * [[resources:​eval:​user-guides:​ad7768-1]] - The AD7768-1 is a low power, high performance,​ Σ-Δ analog-to-digital converter (ADC).   * [[resources:​eval:​user-guides:​ad7768-1]] - The AD7768-1 is a low power, high performance,​ Σ-Δ analog-to-digital converter (ADC).
   * [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​projects/​ad40xx_fmc|AD40xx-FMC]] - Evaluation Board for the AD4000 Series 16-/​18-/​20-Bit Precision SAR ADCs   * [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​projects/​ad40xx_fmc|AD40xx-FMC]] - Evaluation Board for the AD4000 Series 16-/​18-/​20-Bit Precision SAR ADCs
 +
  
 ===== Additional Documents ===== ===== Additional Documents =====
  
   * {{:​resources:​fpga:​peripherals:​spi-engine3.pdf|Presentation:​ SPI Engine Design Philosophy}}   * {{:​resources:​fpga:​peripherals:​spi-engine3.pdf|Presentation:​ SPI Engine Design Philosophy}}
-  *  + 
-{{navigation HDL User Guide#​../​docs/​axi_ip|AXI IP cores#​hdl|Main page#​../​docs/​tips|Using and modifying the HDL design}}+ 
 +{{navigation HDL User Guide#​../​docs/​ip_cores|IP cores#../docs/hdl|Main page#​../​docs/​tips|Using and modifying the HDL design}}
resources/fpga/peripherals/spi_engine.txt · Last modified: 13 Oct 2021 08:45 by Iulia Moldovan