This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:peripherals:spi_engine:interconnect [26 May 2015 18:57] – [Files] Lars-Peter Clausen | resources:fpga:peripherals:spi_engine:interconnect [04 Sep 2019 12:47] (current) – Add configuration parameters, fix some grammar mistakes Istvan Csomortani | ||
---|---|---|---|
Line 3: | Line 3: | ||
{{ : | {{ : | ||
- | The SPI Engine Interconnect module allows | + | The SPI Engine Interconnect module allows |
- | Combining multiple command stream generators in a design and connecting them to a single execution | + | Combining multiple command stream generators in a design and connecting them to a single execution |
===== Files ===== | ===== Files ===== | ||
^ Name ^ Description ^ | ^ Name ^ Description ^ | ||
- | | [[github> | + | | [[github> |
- | | [[github> | + | | [[github> |
===== Configuration Parameters ===== | ===== Configuration Parameters ===== | ||
^ Name ^ Description ^ Default ^ | ^ Name ^ Description ^ Default ^ | ||
+ | | '' | ||
+ | | '' | ||
===== Signal and Interface Pins ===== | ===== Signal and Interface Pins ===== | ||
Line 21: | Line 23: | ||
^ Name ^ Type ^ Description ^ | ^ Name ^ Type ^ Description ^ | ||
| clk | Clock | A signals of the module are synchronous to this clock. | | | clk | Clock | A signals of the module are synchronous to this clock. | | ||
- | | resetn | Synchronous active low reset | Resets the internal state of the module. | | + | | resetn | Synchronous active-low reset | Resets the internal state of the module. | |
| s0_ctrl | [[SPI Engine Control Interface]] slave | Connects to the first control interface master | | | s0_ctrl | [[SPI Engine Control Interface]] slave | Connects to the first control interface master | | ||
| s1_ctrl | [[SPI Engine Control Interface]] slave | Connects to the second control interface master | | | s1_ctrl | [[SPI Engine Control Interface]] slave | Connects to the second control interface master | | ||
Line 28: | Line 30: | ||
===== Theory of Operation ===== | ===== Theory of Operation ===== | ||
- | The SPI Engine Interconnect module has multiple [[SPI Engine Control Interface]] slave ports and a single [[SPI Engine Control Interface]] master port. It can be used to connect multiple command stream generators to a single command execution engine. Arbitration between the streams is done on a priority basis, streams with a lower index have higher priority. This means if commands are present on two streams arbitration will be granted to the one with the lower index. Once arbitration has been granted the port it was granted to stays in control until it sends a SYNC command. When the interconnect module sees a SYNC command arbitration will re-evaluated after the SYNC command has been completed. This makes sure that once a SPI transaction consisting of multiple commands has been started it is able to complete without being interrupted by a higher priority stream. | + | The SPI Engine Interconnect module has multiple [[SPI Engine Control Interface]] slave ports and a single [[SPI Engine Control Interface]] master port. It can be used to connect multiple command stream generators to a single command execution engine. Arbitration between the streams is done on a priority basis, streams with a lower index have higher priority. This means if commands are present on two streams arbitration will be granted to the one with the lower index. Once arbitration has been granted the port it was granted to stays in control until it sends a SYNC command. When the interconnect module sees a SYNC command arbitration will be re-evaluated after the SYNC command has been completed. This makes sure that once a SPI transaction consisting of multiple commands has been started it is able to complete without being interrupted by a higher priority stream. |
===== More Information ===== | ===== More Information ===== | ||
* [[.|SPI Engine Framework]] | * [[.|SPI Engine Framework]] |