The reference design is a processor based embedded system. The sources are split into three different folders:
system_top.v
are also defined.The reference design is a processor based (ARM or Microblaze) embedded system. A functional block diagram of the system is given above. The shared transceivers are followed by the individual JESD204B and ADC/DAC IP cores. The cores are programmable through an AXI-lite interface.
The digital interface consists of 4 transmit and 4 receive lanes running at 10Gbps, by default. The transceivers interface the ADC/DAC cores at 128bits@250MHz. The data is sent or received based on the configuration of separate transmit and receive chains.
The entry point for project creation is system_project.tcl
. Some support scripts are first loaded then the project is created. Based on the suffix of the project, the carrier board is automatically detected. The constraint files and custom modules instantiated directly in the system_top module must be added to the project files list.
system_project.tcl file:
source ../../scripts/adi_env.tcl source $ad_hdl_dir/projects/scripts/adi_project.tcl source $ad_hdl_dir/projects/scripts/adi_board.tcl adi_project_xilinx daq2_zcu102 adi_project_files daq2_zcu102 [list \ "../common/daq2_spi.v" \ "system_top.v" \ "system_constr.xdc"\ "$ad_hdl_dir/library/xilinx/common/ad_iobuf.v" \ "$ad_hdl_dir/projects/common/zcu102/zcu102_system_constr.xdc" ] adi_project_run daq2_zcu102
When the project is created, system_bd.tcl
is sourced. system_bd.tcl
will generate the IP Integrator system. The resulting system will be instantiated in the system_top module.
Some parameters will be defined in the first part, which will configure the ADC/DAC FIFOs. These are part of the systems in which the DDR throughput is not enough to keep up with the ADC/DAC data rates.
set adc_fifo_name axi_ad9680_fifo set adc_fifo_address_width 16 set adc_data_width 128 set adc_dma_data_width 64 set dac_fifo_name axi_ad9144_fifo set dac_fifo_address_width 10 set dac_data_width 128 set dac_dma_data_width 128
The next step is to instantiate the ZCU102 base design:
source $ad_hdl_dir/projects/common/zcu102/zcu102_system_bd.tcl
If ADC/DAC FIFOs will be used in the system, the corresponding tcl files must be sourced.
source $ad_hdl_dir/projects/common/xilinx/adcfifo_bd.tcl source $ad_hdl_dir/projects/common/xilinx/dacfifo_bd.tcl
The next step is to source the DAQ2 specific design.
source ../common/daq2_bd.tcl
The generic design is optimized to supports the maximum number of carriers with minimal changes. If the specific carrier has different parameters than the default, some minor IP parameter changes need to be done. In the case below, the generic design uses parameters for 7 Series FPGAs, so parameters must be adjusted for Ultrascale+.
ad_ip_parameter axi_ad9144_xcvr CONFIG.XCVR_TYPE 2 ad_ip_parameter axi_ad9680_xcvr CONFIG.XCVR_TYPE 2 ad_ip_parameter util_daq2_xcvr CONFIG.XCVR_TYPE 2 ad_ip_parameter util_daq2_xcvr CONFIG.QPLL_FBDIV 20 ad_ip_parameter util_daq2_xcvr CONFIG.QPLL_REFCLK_DIV 1
When using the JESD204 Framework we need to source the JESD204 support script. In this script several procedures which simplify the design are defined:
source $ad_hdl_dir/library/jesd204/scripts/jesd204.tcl
The physical layer is responsible for instantiating and configuring the high speed serial transceivers in the FPGA. The physical layer is implemented with the use of two modules: AXI_ADXCVR and UTIL_ADXCVR. AXI_ADXCVR Provides an AXI interface for performing DRP reads and writes to the transceivers, allowing for dynamic reconfiguration. Given that the hardware implements 4 data lines, that's how we'll configure the NUM_OF_LANES parameter. QPLL_ENABLE parameter gives control to this IP of the QPLL reconfiguration for the Transceiver QUAD. If the QUAD is shared with other RX IPs (as it is in this design), the second ADXCVR IP will need to have QPLL_ENABLE set to 0.
ad_ip_instance axi_adxcvr axi_ad9144_xcvr ad_ip_parameter axi_ad9144_xcvr CONFIG.NUM_OF_LANES 4 ad_ip_parameter axi_ad9144_xcvr CONFIG.QPLL_ENABLE 1 ad_ip_parameter axi_ad9144_xcvr CONFIG.TX_OR_RX_N 1
Instantiation of the ADC transceiver controller. For this IP, QPLL_ENABLE is set to 0.
ad_ip_instance axi_adxcvr axi_ad9680_xcvr ad_ip_parameter axi_ad9680_xcvr CONFIG.NUM_OF_LANES 4 ad_ip_parameter axi_ad9680_xcvr CONFIG.QPLL_ENABLE 0 ad_ip_parameter axi_ad9680_xcvr CONFIG.TX_OR_RX_N 0
Given that the IP uses the same QUAD as the DAC, performing channel reconfiguration may affect the DAC and vice versa. When using the JESD204B framework, this is taken into consideration by software.
The actual transceiver blocks are instantiated in UTIL_ADXCVR.
ad_ip_instance util_adxcvr util_daq2_xcvr ad_ip_parameter util_daq2_xcvr CONFIG.RX_NUM_OF_LANES 4 ad_ip_parameter util_daq2_xcvr CONFIG.TX_NUM_OF_LANES 4
ad_connect sys_cpu_resetn util_daq2_xcvr/up_rstn ad_connect sys_cpu_clk util_daq2_xcvr/up_clk
Xilinx JESD204-PHY IP can be used as an alternative to implementing the physical layer, as it's part of Vivado without additional licensing. We don't currently provide software support for the Xilinx IP. The drawback when using the Xilinx IP is that it doesn't provide Eyescan functionality.
Reference clocks are needed to be feed to the QPLL/CPLL. In this design, we are using tx reference clock for QPLL and rx reference clock for QPLL. If the system works at 10Gbps, the QPLL clock will be used for both the RX and TX channels. What is important to note is that the reference clocks for the transceiver QUAD must be connected to the MGTREFCLK pins either for the QUAD or an adjacent QUAD.
create_bd_port -dir I tx_ref_clk_0 create_bd_port -dir I rx_ref_clk_0 ad_xcvrpll tx_ref_clk_0 util_daq2_xcvr/qpll_ref_clk_* ad_xcvrpll rx_ref_clk_0 util_daq2_xcvr/cpll_ref_clk_* ad_xcvrpll axi_ad9144_xcvr/up_pll_rst util_daq2_xcvr/up_qpll_rst_* ad_xcvrpll axi_ad9680_xcvr/up_pll_rst util_daq2_xcvr/up_cpll_rst_*
The JESD204 data link layer is instantiated in the next lines, for both TX and RX type of peripheral paths. The ADI AD-IP-JESD204 implements the data link layer, supporting subclass 0 or subclass 1 and runtime reconfigurability through an AXI memory mapped interface.
adi_axi_jesd204_tx_create axi_ad9144_jesd 4 adi_axi_jesd204_rx_create axi_ad9680_jesd 4
The IP is equivalent with the Xilinx licensed JESD204 IP.
The transport layer peripherals are responsible for converter specific data framing and de-framing and provide a generic FIFO interface to the rest of the system.
ad_ip_instance axi_ad9144 axi_ad9144_core
ad_ip_parameter axi_ad9144_core CONFIG.QUAD_OR_DUAL_N 0
ad_ip_instance axi_ad9680 axi_ad9680_core
When UTIL_ADXCVR is instantiated, the channel inside of the IP may be different than the hardware pin connection to lessen the layout burden. Because of this, the UTIL_ADXCVR IP will rearrange the inside channels so that they correspond to the outside pin connection for the RX path, keeping a common transport layer. Each channel from the QUAD has assigned a specific pin for TX and RX. After rearranging the channels so they correspond to the RX pins, the TX pins may not be in the order they are connected to the DAC. The below {0 2 3 1} parameter will connect the physical layer to the data link layer as if the channels and pin connections are in order.
ad_xcvrcon util_daq2_xcvr axi_ad9680_xcvr axi_ad9680_jesd ad_xcvrcon util_daq2_xcvr axi_ad9144_xcvr axi_ad9144_jesd {0 2 3 1}
For a complete system, we use additional modules to transfer data. The transport layer transfers data continuously from/to the ADC/DAC. CPACK/Upack will only send the enabled channels to the DMA which in turn will transfer it to the system memory. Depending on system specifics, data offload FIFOs may be inserted between upack/cpack and the DMA. When a FIFO is used, the DMA connection to the DDR can run at a lower speed, as data capture cannot be done continuously.
ad_ip_instance util_upack axi_ad9144_upack ad_ip_parameter axi_ad9144_upack CONFIG.CHANNEL_DATA_WIDTH 64 ad_ip_parameter axi_ad9144_upack CONFIG.NUM_OF_CHANNELS 2 ad_ip_instance axi_dmac axi_ad9144_dma ad_ip_parameter axi_ad9144_dma CONFIG.DMA_TYPE_SRC 0 ad_ip_parameter axi_ad9144_dma CONFIG.DMA_TYPE_DEST 1 ad_ip_parameter axi_ad9144_dma CONFIG.ID 1 ad_ip_parameter axi_ad9144_dma CONFIG.AXI_SLICE_SRC 0 ad_ip_parameter axi_ad9144_dma CONFIG.AXI_SLICE_DEST 0 ad_ip_parameter axi_ad9144_dma CONFIG.DMA_LENGTH_WIDTH 24 ad_ip_parameter axi_ad9144_dma CONFIG.DMA_2D_TRANSFER 0 ad_ip_parameter axi_ad9144_dma CONFIG.CYCLIC 0 ad_ip_parameter axi_ad9144_dma CONFIG.DMA_DATA_WIDTH_SRC 128 ad_ip_parameter axi_ad9144_dma CONFIG.DMA_DATA_WIDTH_DEST 128
ad_ip_instance util_cpack axi_ad9680_cpack ad_ip_parameter axi_ad9680_cpack CONFIG.CHANNEL_DATA_WIDTH 64 ad_ip_parameter axi_ad9680_cpack CONFIG.NUM_OF_CHANNELS 2 ad_ip_instance axi_dmac axi_ad9680_dma ad_ip_parameter axi_ad9680_dma CONFIG.DMA_TYPE_SRC 1 ad_ip_parameter axi_ad9680_dma CONFIG.DMA_TYPE_DEST 0 ad_ip_parameter axi_ad9680_dma CONFIG.ID 0 ad_ip_parameter axi_ad9680_dma CONFIG.AXI_SLICE_SRC 0 ad_ip_parameter axi_ad9680_dma CONFIG.AXI_SLICE_DEST 0 ad_ip_parameter axi_ad9680_dma CONFIG.SYNC_TRANSFER_START 0 ad_ip_parameter axi_ad9680_dma CONFIG.DMA_LENGTH_WIDTH 24 ad_ip_parameter axi_ad9680_dma CONFIG.DMA_2D_TRANSFER 0 ad_ip_parameter axi_ad9680_dma CONFIG.CYCLIC 0 ad_ip_parameter axi_ad9680_dma CONFIG.DMA_DATA_WIDTH_SRC 64 ad_ip_parameter axi_ad9680_dma CONFIG.DMA_DATA_WIDTH_DEST 64
ad_connect util_daq2_xcvr/tx_out_clk_0 axi_ad9144_core/tx_clk
ad_connect axi_ad9144_jesd/tx_data_tdata axi_ad9144_core/tx_data
ad_connect util_daq2_xcvr/tx_out_clk_0 axi_ad9144_upack/dac_clk
ad_connect axi_ad9144_core/dac_enable_0 axi_ad9144_upack/dac_enable_0
ad_connect axi_ad9144_core/dac_ddata_0 axi_ad9144_upack/dac_data_0
ad_connect axi_ad9144_core/dac_valid_0 axi_ad9144_upack/dac_valid_0
ad_connect axi_ad9144_core/dac_enable_1 axi_ad9144_upack/dac_enable_1
ad_connect axi_ad9144_core/dac_ddata_1 axi_ad9144_upack/dac_data_1
ad_connect axi_ad9144_core/dac_valid_1 axi_ad9144_upack/dac_valid_1
ad_connect util_daq2_xcvr/tx_out_clk_0 axi_ad9144_fifo/dac_clk
ad_connect axi_ad9144_jesd_rstgen/peripheral_reset axi_ad9144_fifo/dac_rst
ad_connect axi_ad9144_upack/dac_valid axi_ad9144_fifo/dac_valid
ad_connect axi_ad9144_upack/dac_data axi_ad9144_fifo/dac_data
ad_connect axi_ad9144_core/dac_dunf axi_ad9144_fifo/dac_dunf
ad_connect sys_cpu_clk axi_ad9144_fifo/dma_clk
ad_connect sys_cpu_reset axi_ad9144_fifo/dma_rst
ad_connect sys_cpu_clk axi_ad9144_dma/m_axis_aclk
ad_connect sys_cpu_resetn axi_ad9144_dma/m_src_axi_aresetn
ad_connect axi_ad9144_fifo/dma_xfer_req axi_ad9144_dma/m_axis_xfer_req
ad_connect axi_ad9144_fifo/dma_ready axi_ad9144_dma/m_axis_ready
ad_connect axi_ad9144_fifo/dma_data axi_ad9144_dma/m_axis_data
ad_connect axi_ad9144_fifo/dma_valid axi_ad9144_dma/m_axis_valid
ad_connect axi_ad9144_fifo/dma_xfer_last axi_ad9144_dma/m_axis_last
# connections (adc)
ad_connect util_daq2_xcvr/rx_out_clk_0 axi_ad9680_core/rx_clk
ad_connect axi_ad9680_jesd/rx_sof axi_ad9680_core/rx_sof
ad_connect axi_ad9680_jesd/rx_data_tdata axi_ad9680_core/rx_data
ad_connect util_daq2_xcvr/rx_out_clk_0 axi_ad9680_cpack/adc_clk
ad_connect axi_ad9680_jesd_rstgen/peripheral_reset axi_ad9680_cpack/adc_rst
ad_connect axi_ad9680_core/adc_enable_0 axi_ad9680_cpack/adc_enable_0
ad_connect axi_ad9680_core/adc_valid_0 axi_ad9680_cpack/adc_valid_0
ad_connect axi_ad9680_core/adc_data_0 axi_ad9680_cpack/adc_data_0
ad_connect axi_ad9680_core/adc_enable_1 axi_ad9680_cpack/adc_enable_1
ad_connect axi_ad9680_core/adc_valid_1 axi_ad9680_cpack/adc_valid_1
ad_connect axi_ad9680_core/adc_data_1 axi_ad9680_cpack/adc_data_1
ad_connect util_daq2_xcvr/rx_out_clk_0 axi_ad9680_fifo/adc_clk
ad_connect axi_ad9680_jesd_rstgen/peripheral_reset axi_ad9680_fifo/adc_rst
ad_connect axi_ad9680_cpack/adc_valid axi_ad9680_fifo/adc_wr
ad_connect axi_ad9680_cpack/adc_data axi_ad9680_fifo/adc_wdata
ad_connect sys_cpu_clk axi_ad9680_fifo/dma_clk
ad_connect sys_cpu_clk axi_ad9680_dma/s_axis_aclk
ad_connect sys_cpu_resetn axi_ad9680_dma/m_dest_axi_aresetn
ad_connect axi_ad9680_fifo/dma_wr axi_ad9680_dma/s_axis_valid
ad_connect axi_ad9680_fifo/dma_wdata axi_ad9680_dma/s_axis_data
ad_connect axi_ad9680_fifo/dma_wready axi_ad9680_dma/s_axis_ready
ad_connect axi_ad9680_fifo/dma_xfer_req axi_ad9680_dma/s_axis_xfer_req
ad_connect axi_ad9680_core/adc_dovf axi_ad9680_fifo/adc_wovf
The below instructions assign addresses to all AXI modules in the design. These will be used when generating the device tree in linux.
# interconnect (cpu)
ad_cpu_interconnect 0x44A60000 axi_ad9144_xcvr
ad_cpu_interconnect 0x44A00000 axi_ad9144_core
ad_cpu_interconnect 0x44A90000 axi_ad9144_jesd
ad_cpu_interconnect 0x7c420000 axi_ad9144_dma
ad_cpu_interconnect 0x44A50000 axi_ad9680_xcvr
ad_cpu_interconnect 0x44A10000 axi_ad9680_core
ad_cpu_interconnect 0x44AA0000 axi_ad9680_jesd
ad_cpu_interconnect 0x7c400000 axi_ad9680_dma
The below instructions assign an HP port to all AXI masters, through an interconnect. If there is a single master per interconnect, it will be bypassed in the interconnect. The HP3 connections allow the physical layer to transmit eyescan data to memory, without software interference.
# gt uses hp3, and 100MHz clock for both DRP and AXI4 ad_mem_hp3_interconnect sys_cpu_clk sys_ps7/S_AXI_HP3 ad_mem_hp3_interconnect sys_cpu_clk axi_ad9680_xcvr/m_axi # interconnect (mem/dac) ad_mem_hp1_interconnect sys_cpu_clk sys_ps7/S_AXI_HP1 ad_mem_hp1_interconnect sys_cpu_clk axi_ad9144_dma/m_src_axi ad_mem_hp2_interconnect sys_cpu_clk sys_ps7/S_AXI_HP2 ad_mem_hp2_interconnect sys_cpu_clk axi_ad9680_dma/m_dest_axi
ad_cpu_interrupt ps-10 mb-15 axi_ad9144_jesd/irq ad_cpu_interrupt ps-11 mb-14 axi_ad9680_jesd/irq ad_cpu_interrupt ps-12 mb-13 axi_ad9144_dma/irq ad_cpu_interrupt ps-13 mb-12 axi_ad9680_dma/irq
The reference clock that is used for the transceivers, must be captured by an IBUFDS_GTE4 block. Because UTIL_ADXCVR doesn't have the buffer instantiated, the best place to instantiate it is in system_top.v
.
IBUFDS_GTE4 i_ibufds_rx_ref_clk ( .CEB (1'd0), .I (rx_ref_clk_p), .IB (rx_ref_clk_n), .O (rx_ref_clk), .ODIV2 ());
We prefer using single ended signals as much as possible in the IPI system.
As shown below, the transceiver channels and ADC channels are not connected one to one.
set_property -dict {PACKAGE_PIN K2} [get_ports rx_data_p[0]] ; ## A10 FMC_HPC0_DP3_M2C_P set_property -dict {PACKAGE_PIN K1} [get_ports rx_data_n[0]] ; ## A11 FMC_HPC0_DP3_M2C_N set_property -dict {PACKAGE_PIN H2} [get_ports rx_data_p[1]] ; ## C06 FMC_HPC0_DP0_M2C_P set_property -dict {PACKAGE_PIN H1} [get_ports rx_data_n[1]] ; ## C07 FMC_HPC0_DP0_M2C_N set_property -dict {PACKAGE_PIN F2} [get_ports rx_data_p[2]] ; ## A06 FMC_HPC0_DP2_M2C_P set_property -dict {PACKAGE_PIN F1} [get_ports rx_data_n[2]] ; ## A07 FMC_HPC0_DP2_M2C_N set_property -dict {PACKAGE_PIN J4} [get_ports rx_data_p[3]] ; ## A02 FMC_HPC0_DP1_M2C_P set_property -dict {PACKAGE_PIN J3} [get_ports rx_data_n[3]] ; ## A03 FMC_HPC0_DP1_M2C_N set_property -dict {PACKAGE_PIN K6} [get_ports tx_data_p[0]] ; ## A30 FMC_HPC0_DP3_C2M_P (tx_data_p[0]) set_property -dict {PACKAGE_PIN K5} [get_ports tx_data_n[0]] ; ## A31 FMC_HPC0_DP3_C2M_N (tx_data_n[0]) set_property -dict {PACKAGE_PIN G4} [get_ports tx_data_p[1]] ; ## C02 FMC_HPC0_DP0_C2M_P (tx_data_p[3]) set_property -dict {PACKAGE_PIN G3} [get_ports tx_data_n[1]] ; ## C03 FMC_HPC0_DP0_C2M_N (tx_data_n[3]) set_property -dict {PACKAGE_PIN F6} [get_ports tx_data_p[2]] ; ## A26 FMC_HPC0_DP2_C2M_P (tx_data_p[1]) set_property -dict {PACKAGE_PIN F5} [get_ports tx_data_n[2]] ; ## A27 FMC_HPC0_DP2_C2M_N (tx_data_n[1]) set_property -dict {PACKAGE_PIN H6} [get_ports tx_data_p[3]] ; ## A22 FMC_HPC0_DP1_C2M_P (tx_data_p[2]) set_property -dict {PACKAGE_PIN H5} [get_ports tx_data_n[3]] ; ## A23 FMC_HPC0_DP1_C2M_N (tx_data_n[2])
The reference clocks run at 500 MHz, and the frame clock at 250, in the maximum throughput configuration(default).
create_clock -name tx_ref_clk -period 2.00 [get_ports tx_ref_clk_p] create_clock -name rx_ref_clk -period 2.00 [get_ports rx_ref_clk_p] create_clock -name tx_div_clk -period 4.00 [get_pins i_system_wrapper/system_i/util_daq2_xcvr/inst/i_xch_0/i_gthe4_channel/TXOUTCLK] create_clock -name rx_div_clk -period 4.00 [get_pins i_system_wrapper/system_i/util_daq2_xcvr/inst/i_xch_0/i_gthe4_channel/RXOUTCLK]
When building the project, you should always use the recommended version of the tools for the specific release. In this example, we'll use release 2018_r1, which has Vivado 2017.4.1 as the recommended version. If you're using different Vivado versions, it's possible that there are slight modifications on how the synthesis works, or different Xilinx IP changes, which affect the system functionality.
mkdir adi cd adi git clone https://github.com/analogdevicesinc/hdl.git cd hdl/ git status ## check for everything, including branch name git checkout hdl_2018_r1 ## change to the hdl_2018_r2 branch make -C projects/daq2/zcu102
The boot image BOOT.BIN
is build using the bootgen tool which requires several input files. For ease of use we provide a bash shell script which allows building BOOT.BIN
from system_top.hdf
, u-boot.elf
and either bl31.elf
or a path to the Arm Trusted Firmware repository.
The script can be downloaded from here:
NOTE: After downloading the script you need to make it executable
$ chmod +x build_zynqmp_boot_bin.sh
usage: build_zynqmp_boot_bin.sh system_top.hdf u-boot.elf (download | bl31.elf | <path-to-arm-trusted-firmware-source>) [output-archive]
system_top.hdf
and u-boot.elf
are required parameters.download
(which will git clone the ATF repository), bl31.elf
or the file system path
to the Arm Trusted Firmware source code repositoryname
parameter can be given to tar.gz the output directory. (name
.tar.gz)$ source /opt/Xilinx/Vivado/201x.x/settings64.sh
NOTE: u-boot.elf
For those who don't want to build u-boot themselves.
The u-boot.elf can be extracted from the project folder on the SD Card image, bootgen_sysfiles.tgz