This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:peripherals:jesd204:jesd204_troubleshooting [06 Feb 2020 16:52] – removed wraps Laszlo Nagy | resources:fpga:peripherals:jesd204:jesd204_troubleshooting [20 Dec 2021 08:19] (current) – [Link status stays in CGS and SYNC~ is de-asserts] Laszlo Nagy | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== Troubleshooting | + | ===== Troubleshooting |
Running one of the below commands on a Linux based system will return the status of the JESD link. | Running one of the below commands on a Linux based system will return the status of the JESD link. | ||
Line 21: | Line 21: | ||
==== Common symptoms ==== | ==== Common symptoms ==== | ||
- | Below table describes the most commonly occurred problems during link bring-up | + | Below table describes the most commonly occurred problems during link bring-up |
Line 63: | Line 63: | ||
</ | </ | ||
+ | ---- | ||
+ | |||
+ | ====Link is DISABLED, In Linux boot log following appears: | ||
+ | <WRAP center round box 100%> | ||
+ | **Cause:** QPLL can't find a configuration for desired lane rate with the given reference clock. | ||
+ | |||
+ | **Identify: | ||
+ | |||
+ | **Fix:** Configure the clock chip for different reference clock or switch to CPLL or QPLL0/1. | ||
+ | </ | ||
---- | ---- | ||
Line 116: | Line 126: | ||
* OutClkSel - // | * OutClkSel - // | ||
</ | </ | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ====Link status stays in CGS and SYNC~ is deasserted==== | ||
+ | <WRAP center round box 100%> | ||
+ | **Cause: | ||
+ | |||
+ | **Identify: | ||
+ | # | ||
+ | or | ||
+ | #grep "" | ||
+ | Link status: CGS | ||
+ | SYNC~: deasserted | ||
+ | |||
+ | **Fix:** Make sure SYNC~ is connected to the Link Transmit peripheral and is properly driven. | ||
+ | </ | ||
+ | |||
+ | <WRAP center round box 100%> | ||
+ | **Cause: | ||
+ | |||
+ | **Identify: | ||
+ | # | ||
+ | or | ||
+ | #grep "" | ||
+ | Link status: CGS | ||
+ | SYNC~: deasserted | ||
+ | |||
+ | **Fix:** Make sure software communicates correctly with the DAC, bring-up sequence was executed and JESD RX blocks configured and enabled. | ||
+ | </ | ||
+ | |||
+ | <WRAP center round box 100%> | ||
+ | **Cause: | ||
+ | |||
+ | **Identify: | ||
+ | # | ||
+ | or | ||
+ | #grep "" | ||
+ | Link status: CGS | ||
+ | SYNC~: deasserted | ||
+ | SYSREF captured | ||
+ | |||
+ | **Fix:** Make sure SYSREF is connected to the Link Transmit peripheral and is properly driven. | ||
+ | </ | ||
+ | |||
---- | ---- | ||
Line 202: | Line 256: | ||
===== Support ===== | ===== Support ===== | ||
- | Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the [[https://ez.analog.com/ | + | Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Video, Audio, etc) via the [[ez>community/ |
~~NOTOC~~ | ~~NOTOC~~ | ||