The Analog Devices JESD204B/C Link Receive Peripheral implements the link layer handling of a JESD204 receive logic device. Implements the 8B/10B based link layer defined in JESD204C standard that is similar to the link layer defined in JESD204B. This includes handling of the SYSREF and SYNC~ and controlling the link state machine accordingly as well as performing per lane descrambling and character replacement. Implements the 64B/66B based link layer defined in the JESD204C standard. This includes handling of the SYSREF, per lane decoding of sync header, descrambling, CRC checking of data blocks and error monitoring.
The type of link layer is selectable during implementation phase through the LINK_MODE
synthesis parameter.
It has been designed for interoperability with Analog Devices JESD204 ADC converter products. To form a complete JESD204 receive logic device it has to be combined with a PHY layer and transport layer peripheral.
Name | Description |
---|---|
axi_jesd204_rx.v | Verilog source for the peripheral. |
axi_jesd204_rx_ip.tcl | TCL script to generate the Vivado IP-integrator project for the peripheral. |
Name | Description | Default |
---|---|---|
ID | Instance identification number. | 0 |
NUM_LANES | Maximum number of lanes supported by the peripheral. | 1 |
NUM_LINKS | Maximum number of links supported by the peripheral. | 1 |
LINK_MODE | Decoder selection of the link layer. 1 - 8B/10B mode 2 - 64B/66B mode | 1 |
DATA_PATH_WIDTH | Data path width in bytes. Set it 4 in case of 8B/10B, 8 in case of 64B/66B | 4 |
TPL_DATA_PATH_WIDTH | Data path width in bytes towards transport layer. Must be greater or equal to DATA_PATH_WIDTH . Must be a power of 2 integer multiple of the F parameter. | 4 |
ASYNC_CLK | Set this parameter to 1 if the link clock and the device clocks have different frequencies, or if they have the same frequency but a different source. If set, synchronizing logic and a gearbox of ratio DATA_PATH_WIDTH :TPL_DATA_PATH_WIDTH is inserted to do the rate conversion. If not set, TPL_DATA_PATH_WIDTH must match DATA_PATH_WIDTH , the same clock must be connected to clk and device_clk inputs. | 0 |
Name | Type | Description |
---|---|---|
s_axi_aclk | Clock | All S_AXI signals and irq are synchronous to this clock. |
s_axi_aresetn | Synchronous active low reset | Resets the internal state of the peripheral. |
S_AXI | AXI4-Lite bus slave | Memory mapped AXI-lite bus that provides access to modules register map. |
irq | Level-High Interrupt | Interrupt output of the module. Is asserted when at least one of the modules interrupt is pending and enabled. |
clk | Clock | Link clock for the JESD204 interface. Must be line clock / 40 for correct operation in 8B/10B mode, line clock / 66 in 64B/66B mode. |
reset | Reset | Reset active high synchronous with the Link clock. |
device_clk | Clock | Device clock for the JESD204 interface. Its frequency must be link clock * DATA_PATH_WIDTH / TPL_DATA_PATH_WIDTH |
device_reset | Reset | Reset active high synchronous with the Device clock. |
RX_DATA | AXI4-Streaming interface | Received data. |
sync[m-1:0] | Output | JESD204 SYNC~ (or SYNC_N) signals, available in 8B/10B mode. (0 <= m < NUM_LINKS ) |
sysref | Input | JESD204 SYSREF signal. |
RX_PHYn | JESD204 receive PHY interface | n-th lane of the JESD204 interface (0 <= n < NUM_LANES ). |
phy_en_char_align | Output | Enable transceiver character alignment. |
phy_ready | Input | Transceiver status. |
Access Type | Name | Description |
---|---|---|
RO | Read-only | Reads will return the current register value. Writes have no effect. |
RW | Read-write | Reads will return the current register value. Writes will change the current register value. |
RW1C | Write-1-to-clear | Reads will return the current register value. Writing the register will clear those bits of the register which were set to 1 in the value written. |
V | Volatile | The V suffix indicates that the register is volatile and its content might change without software interaction. The value of a non-volatile register will not change without an explicit write done by software. |
The JESD204B/C receive peripheral consists of two main components. The register map and the link processor. Both components are fully asynchronous and are clocked by independent clocks. The register map is in the s_axi_aclk
clock domain, while the link processor is in the clk
and device_clk
clock domain.
The register map is used to configure the operational parameters of the link processor as well as to query the current state of the link processor. The link processor itself is responsible for handling the JESD204 link layer protocol.
The register map configuration interface can be accessed through the AXI4-Lite S_AXI
interface. The interface is synchronous to the s_axi_aclk
. The s_axi_aresetn
signal is used to reset the peripheral and should be asserted during system startup until the s_axi_aclk
is active and stable. De-assertion of the reset signal should be synchronous to s_axi_aclk
.
The sync
and sysref
signals correspond to the SYNC~ and SYSREF signals of the JESD204 specification.
The sync
signal is asserted by the peripheral during link initialization and must be connected to the corresponding JESD204 ADC converter devices on the same link.
The sysref
signal is generated externally and is optional. It is only required to achieve deterministic latency in subclass 1 mode operation. If the sysref
signal is not connected software needs to configure the peripheral accordingly to indicate this.
When the sysref
signal is used, in order to ensure correct operation, it is important that setup and hold of the external signal relative to the device_clk
signal are met. Otherwise, deterministic latency cannot be guaranteed.
For each lane, the peripheral has one corresponding RX_PHY interface. These interfaces accept the physical layer data from the downstream physical layer transceiver peripheral.
The physical layer is responsible for clock recovery, character alignment, de-serialization as well an 8b10b decoding.
User data is provided on the AXI4-Stream RX_DATA
interface. The interface is a reduced AXI4-Stream interface and only features the TVALID flow control signal, but not the TREADY flow control signal. The behavior of the interface is as if the TREADY signal was always asserted. This means as soon as rx_valid
is asserted a continuous stream of user data must be accepted from rx_data
.
After reset and during link initialization the rx_valid
signal is de-asserted. As soon as the User Data Phase is entered the rx_valid
will be asserted to indicate that the peripheral is now providing and the processed data at the rx_data
signal. The rx_valid
signal stays asserted until the link is either deactivated or re-initialized.
Typically the RX_DATA
interface is connected to a JESD204 transport layer peripheral that de-frames the data and passes it to the application layer. The internal data path width of the peripheral is four, this means that four octets per lane are processed in parallel. When in the user data phase the peripheral provides four octets for each lane in each beat.
This means that RX_DATA
interface is DATA_PATH_WIDTH
* 8 * NUM_LANES
bits wide. With each block of consecutive DATA_PATH_WIDTH
* 8 bits corresponding to one lane. The lowest DATA_PATH_WIDTH
* 8 bits correspond to the first lane, while the highest DATA_PATH_WIDTH
* 8 bits correspond to the last lane.
E.g. for 8B/10B mode where DATA_PATH_WIDTH
=4. Each lane specific 32-bit block corresponds to four octets each 8 bits wide. The temporal ordering of the octets is from LSB to MSB, this means the octet placed in the lowest 8 bits was received first, the octet placed in the highest 8 bits was received last.
Data corresponding to lanes that have been disabled should be ignored and their value is undefined.
The peripheral features a register map configuration interface that can be accessed through the AXI4-Lite S_AXI
port. The register map can be used to configure the peripherals operational parameters, query the current status of the device and query the features supported by the device.
The peripheral contains multiple registers that allow the identification of the peripheral as well as the discovery of features that were configured at HDL synthesis time. Apart from the SCRATCH
register all registers in this section are read-only and write access to them will be ignored.
The VERSION
(0x000
) register contains the version of the peripheral. The version determines the register map layout and general features supported by the peripheral. The version number follows semantic versioning. Increments in the major number indicate backward incompatible changes, increments in the minor number indicate backward compatible changes, patch letter increments indicate bug fix.
The PERIPHERAL_ID
(0x004
) register contains the value of the ID
HDL configuration parameter that was set during synthesis. Its primary function is to allow to distinguish between multiple instances of the peripheral in the same design.
The SCRATCH
(0x008
) register is a general purpose 32-bit register that can be set to an arbitrary values. Reading the register will yield the value previously written (The value will be cleared when the peripheral is reset). Its content does not affect the operation of the peripheral. It can be used by software to test whether the register map is accessible or store custom peripheral associated data.
The IDENTIFICATION
(0x00c
) register contains the value of “204R”
. This value is unique to this type of peripheral and can be used to ensure that the peripheral exists at the expected location in the memory mapped IO register space.
The SYNTH_NUM_LANES
(0x010
) register contains the value of the NUM_LANES
HDL configuration parameter that was set during synthesis. It corresponds to the maximum of lanes supported by the peripheral. Possible values are between 1
and 32
.
The SYNTH_DATA_PATH_WIDTH
(0x014
) register contains the value of the internal data path width per lane in octets. This is how many octets are processed in parallel on each lane and affects the restrictions of possible values for certain runtime configuration registers. The value is encoded as the log2() of the data path width. Possible values are:
The SYNTH_ELASTIC_BUFFER_SIZE
(0x040
) register describes the maximum amount of octets that the elastic buffer can hold. This puts a limit on the maximum local-multi-frame-clock (LMFC) / local-multiblock-clock (LEMC) period (subclass 1) as well as the maximum skew between individual lanes (subclass 0). Both must be less than the elastic buffer size.
Interrupt processing is handled by three closely related registers. All three registers follow the same layout, each bit in the register corresponds to one particular interrupt.
When an interrupt event occurs it is recorded in the IRQ_SOURCE
(0x088
) register. For a recorded interrupt event the corresponding bit is set to 1. If an interrupt event occurs while the bit is already set to 1 it will stay set to 1.
The IRQ_ENABLE
(0x080
) register controls how recorded interrupt events propagate. An interrupt is considered to be enabled if the corresponding bit in the IRQ_ENABLE
register is set to 1, it is considered to be disabled if the bit is set to 0.
Disabling an interrupt will not prevent it from being recorded, but only its propagation. This means if an interrupt event was previously recorded while the interrupt was disabled and the interrupt is being enabled the interrupt event will then propagate.
An interrupt event that has been recorded and is enabled propagates to the IRQ_PENDING
(0x084
) register. The corresponding bit for such an interrupt will read as 1. Disabled or interrupts for which no events have been recorded will read as 0. Also if at least one interrupt has been recorded and is enabled the external irq
signal will be asserted to signal the IRQ event to the upstream IRQ controller.
A recorded interrupt event can be cleared (or acknowledged) by writing a 1 to the corresponding bit to either the IRQ_SOURCE
or IRQ_PENDING
register. It is possible to clear multiple interrupt events at the same time by setting multiple bits in a single write operation.
For more details regarding interrupt operation see the interrupts section of this document.
The LINK_DISABLE
(0x0c0
) register is used to control the link state and switch between enabled and disabled. While the link is disabled its state machine will remain in reset and it will not react to any external event like the SYSREF
signal.
Writing a 0 to the LINK_DISABLE
register will enable the link. While the link state is changing from disabled to enabled it will go through a short initialization procedure, which will take a few clock cycles. To check whether the initialization procedure has completed and the link is fully operational the LINK_STATE
(0x0c4
) register can be checked. The LINK_STATE ([0]
) bit will contain a 0 when the link is fully enabled and will contain a 1 while it is disabled or going through the initialization procedure.
Writing a 1 to the LINK_DISABLE
register will immediately disable the link.
The EXTERNAL_RESET
([1]
) bit in the LINK_STATE
register indicates whether the external link reset signal is asserted (1
) or de-asserted (0
). When the external link reset is asserted the link is disabled regardless of the setting of LINK_DISABLE
. The external link reset is controlled by the fabric and might be asserted if the link clock is not stable yet.
A multi-link is a link where multiple converter devices are connected to a single logic device (FPGA). All links involved in a multi-link are synchronous and established at the same time. For an 8B/10B RX link, this means that the SYNC~
signal needs to be propagated from the FPGA to each converter.
For an 8B/10B link the MULTI_LINK_DISABLE
register allows activating or deactivating each SYNC~
lines independently. This is useful when depending on the use case profile some converter devices are supposed to be disabled.
The link configuration registers control certain aspects of the runtime behavior of the peripheral. Since the JESD204 standard does now allow changes to link configuration while the link is active the link configuration registers can only be modified while the link is disabled. As soon as it is enabled the configuration registers turn read-only and any writes to them will be ignored.
The LANES_DISABLE
(0x200
) register allows to disable individual lanes. Each bit in the register corresponds to a particular lane and indicates whether that lane is enabled or disabled. Bit 0 corresponds to the first lane, bit 1 to the second lane and so on. A value of 0 for a specific bit means the corresponding lane is enabled, a value of 1 means the lane is disabled. A disabled lane will not receive any data when the link is otherwise active. By default, all lanes are enabled.
The LINK_CONF0
register configures the octets-per-frame and frames-per-multi-frame settings of the link. The OCTETS_PER_FRAME
([18:16]
) field should be set to the number of octets-per-frame minus 1 (F - 1). The OCTETS_PER_MULTIFRAME
([7:0]
) field should be set to the number of octets-per-frame multiplied by the number of frames-per-multi-frame minus 1 (FxK - 1). For correct operation FxK must be a multiple of 4. In 64B/66B mode this field matches and also represents the number of octets per extended multiblock (Ex32x8 - 1).
The LINK_CONF1
register allows disabling optional link level processing stages. The DESCRAMBLER_DISABLE
([0]
) bit controls whether descrambling of the received user data is enabled or disabled. A value of 0 enables descrambling and a value of 1 disables it. In 64B/66B mode descrambling must be always enabled. The CHAR_REPLACEMENT_DISABLE
([1]
) bit controls whether alignment character replacement is performed or not. A value of 0 enables character replacement and a value of 1 disables it. If character replacement is disabled and an alignment character is received (/F/ or /A/) a unexpected K-character error is raised.
Both the transmitter as well as receiver device on the JESD204 link need to be configured with the same settings for scrambling/descrambling and character replacement for correct operation.
Character replacement is used only in 8B/10B links and completely disregarded in 64B/66B mode.
The LINK_CONF2
register controls the behavior of elastic buffer. The BUFFER_EARLY_RELEASE
([16]
) bit configures when the data is released from the elastic buffer to the RX_DATA port. If the bit is set to 0 the data will be released at the earliest configured release point after all lanes are ready. When the bit is set to 1 the data will be released as soon as all lanes are ready. The former gives deterministic latency and is required for subclass 1 operation, the later gives minimum latency.
The BUFFER_DELAY
([11:0]
) field allows to configure the buffer release opportunity point relative to the local-multi frame-clock (LMFC)/ local-multiblock-clock (LEMC). A setting of 0 indicates that the release opportunity is aligned to the LMFC/LEMC edge. A setting of X indicates that it trails the LMFC/LEMC edge by X octets.
The BUFFER_DELAY
field must be set to a multiple of 4. Writing a value that is not a multiple of 4 will be rounded down to the next multiple of 4. For correct operation, the BUFFER_DELAY
field must also be set to a value smaller than the number of octets per multi-frame (F
xK
).
This mechanism can be used to reduce overall latency while still maintaining deterministic latency if the maximum link latency (overall valid PVT settings) is known.
The external SYSREF signal is used to align the internal local multiframe clocks (LMFC)/ local-multiblock-clock (LEMC) between multiple devices on the same link.
The SYSREF_CONF
(0x100
) register allows to configure the behavior of the SYSREF capture circuitry. Setting the SYSREF_DISABLE
([0]
) bit to 1 disables the SYSREF handling. All external SYSREF events are ignored and the LMFC/LEMC is generated internally. For Subclass 1 operation SYSREF handling should be enabled and for Subclass 0 operation it should be disabled.
The SYSREF_LMFC_OFFSET
(0x104
) register allows to modify the offset between the SYSREF rising edge and the rising edge of the LMFC/LEMC.
For optimal operation it is recommended that all device on a JESD204 link should be configured in a way so that the total offset between
The value of the SYSREF_LMFC_OFFSET
register must be set to a value smaller than the configured number of octets-per-multiframe (OCTETS_PER_MULTIFRAME
), otherwise undefined behavior might occur.
The SYSREF_STATUS
(0x108
) register allows to monitor the status of the SYSREF signals. SYSREF_DETECTED
([0]
) bit indicates that the peripheral as observed a SYSREF event. The SYSREF_ALIGNMENT_ERROR
([1]
) bit indicates that a SYSREF event has been observed which was unaligned, in regards to the LMFC/LEMC period, to a previously recorded SYSREF event.
All bits in the SYSREF_STATUS
register are write-to-clear. All bits will also be cleared when the link is disabled.
Note that the SYSREF_STATUS
register will not record any events if SYSREF operation is disabled or the JESD204 link is disabled.
All link status registers are read-only. While the link is disabled some of the link status registers might contain bogus values. Their content should be ignored until the link is fully enabled.
The STATUS_STATE
([1:0]
) field of the LINK_STATUS
(0x280
) register indicates the state of the 8B/10B link state machine or 64B/66B link state machine depending on the selected decoder.
Possible values for a 8B/10B link are:
Possible values for a 64B/66B link are:
The state of each individual lane can be queried from the lane status registers.
Each lane has a independent status register (LANEn_STATUS
(0x300
)) that indicates the current state of the lane.
The CGS_STATE
([1:0]
) indicates the current state of the lane code group synchronization:
The IFS_READY
([4]
) bit indicates that initial frame synchronization has completed for the lane and the lane is receiving either ILAS data or user data.
The LANEn_LATENCY
(0x304
) register holds the duration in octets between when the SYNC~ signal was de-asserted and when the frame synchronization for this particular lane has completed. The LANEn_LATENCY
register only holds valid data if the IFS_READY
bit of the LANEn_STATUS
register is set.
The EMB_STATE
([10:8]
) indicates the current state of the Extended Multi-Block alignment state machine:
If the JESD204 transmitter emits an initial lane alignment sequence (ILAS) the configuration data embedded in the second multi-frame of the ILA sequence is captured by the peripheral and stored in a set of four per-lane registers (LANEn_ILAS0
, LANEn_ILAS1
, LANEn_ILAS2
and LANEn_ILAS3
). ILAS_READY
([5]
) bit in the corresponding LANEn_STATUS
register indicates whether the ILAS configuration data has been captured for a specific lane. The data in the LANEn_ILASx
registers is only valid when that bit is asserted.
The received ILAS configuration data can be used to verify that the transmitter device is using the expected configuration and that the lane and device mapping is correct.
The LINK_CLK_FREQ
(0x0c8
) register allows to determine the clock rate of the link clock (clk
) relative to the AXI interface clock (s_axi_aclk
). This can be used to verify that the link clock is running at the expected rate.
The DEVICE_CLK_FREQ
(0x0cc
) register allows to determine the clock rate of the device clock (device_clk
) relative to the AXI interface clock (s_axi_aclk
). This can be used to verify that the device clock is running at the expected rate.
The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock this corresponds to a resolution of 1.523kHz per LSB. A raw value of 0 indicates that the link clock is currently not active.
The core does not generates interrupts.
The peripheral can be in one of four main operating phases: RESET, WAIT FOR PHY, CGS, or DATA. Upon reset the peripheral starts in the RESET phase. The WAIT FOR PHY and CGS phases are used during the initialization of the JESD204 link. The DATA phase is used during normal operation when user data is received across the JESD204 link.
The RESET phase is the default state entered during reset. While disabled the peripheral will stay in the RESET phase. When enabled the peripheral will transition from the RESET phase to the WAIT FOR PHY phase.
If at any point the peripheral is disabled it will automatically transition back to the RESET state.
Lanes that have been disabled in the register map configuration interface will behave as if the link was in the RESET state regardless of the actual state.
During the WAIT FOR PHY phase the peripheral will wait for all PHY controllers for all enabled lanes to be ready for operation. Once this condition is satisfied the controlled will transition to the CGS phase.
During the CGS phase the peripheral will assert the external ~SYNC signal and expects the connected JESD204 transmitter to send /K/ characters.
Each lane will independently the incoming data stream for /K/ characters and adjust its state machine according to the received characters.
Once all enabled lanes have entered the DATA state the link state will transition from the CGS phase to the DATA phase.
The DATA phase is the main operating mode of the peripheral. In this phase it will transmit transport layer data at the RX_DATA port. When the peripheral enters the DATA phase the valid
signal of the RX_DATA
interface will be asserted to indicate that transport layer data is now available.
By default the data received on each lane will is descrambled. Descrambling can optionally be disabled via the register map configuration interface. Descrambling is enabled or disabled for all lanes equally.
Scrambling reduces data-dependent effects, which can affect both the analog performance of the data converter as well as the bit-error rate of JESD204 serial link, therefore it is highly recommended to enable scrambling for the link.
The peripheral also performs per-lane alignment character monitoring. When alignment character replacement is enabled the JESD204 transmitter replaces under certain predictable conditions (i.e. the receiver can recover the replaced character) the last octet in a frame or multi-frame. Replaced characters at the end of a frame, that is also the end of a multi-frame, are replaced by the /A/ character. Replaced characters at the end of a frame, that is not the end of a multi-frame, are replaced by the /F/ character. If a alignment character is received the peripheral checks that the it is in the expected position, either the end of a frame or the end of a multi-frame, and reports an error if a lane has become misaligned. This allows to detect alignment errors and allows the application to re-initialize the link.
Alignment character monitoring can optionally be disabled via the register map configuration interface. Alignment character monitoring is enabled or disabled for all lanes equally. If alignment character monitoring is disabled no errors are reported when a misaligned alignment character is received.
Data on the RX_DATA
port corresponding to a disabled lanes are undefined and should be ignored.
In a multi-endpoint configuration one link receive peripheral connects to several endpoints/converter devices.
In such cases the link is established only when all enabled endpoints reach the DATA phase. For that all endpoints must pass through CGS and ILAS stages. Depending on the software implementation that controls the converter devices the endpoints can be enabled at different moments. The link receive peripheral will receive the CGS characters and do character alignment until for all enabled endpoints lanes succeeds that and signalize that through the de-assertion of SYNC~
signal.
In the below example we have a multi-point link of four endpoints (NUM_LINKS
= 4):
Note. The physical layer is not depicted on purpose. JTXn represents the link layer counterpart in the converter device/endpoint n
The steps of the link bring-up are presented below:
SYNC~
signal to indicate to the endpoints it is ready to receive and align to the CGS
characters. All SYNC~
signal to all enabled endpoints assert in the same time. CGS
characters until its SYNC~
pin is not pulled low. The timing depends on the software implementation that controls the DAC. SYSREF
is captured and LMFC
in the FPGA and converter device is adjusted. CGS
characters are received correctly on all enabled lanes, on the next Frame clock boundary in SC0 or LMFC
boundary in SC1 the SYNC~
is de-asserted. All SYNC~
signal to all enabled endpoints de-assert in the same time. In SC1 if SYSREF
is not captured the link receive peripheral will stay in CGS state and will keep SYNC~
asserted. MULTI_LINK_DISABLE
) observe the de-assert of the SYNC~
signal, on the next Frame clock boundary for SC0 or the next LMFC
boundary for SC1, will start sending the ILAS
sequence, then after typically 4 LMFC
periods later the actual DATA
. The 64 bit wide datapath of the link layer is fairly simple, the data received from the PHY is sent through a mandatory descrambler block to an elastic buffer that serves as an aligner cross lanes. Each beat of the datapath contains a block of data of 8 octets.
For each lane the control path starts from the 2 bit sync header connected to the header decoder that tracks and monitors multiblock and extended multiblock markers from the stream, reconstructs the 32 bits sync word corresponding to every multiblock and extracts the received CRC from it. The CRC is calculated for every multiblock and is compared against the received CRC. The mismatches are recorded by the error monitor block.
Beside the CRC errors the error monitor records invalid end of multiblock, end of extended multiblock and invalid sync header errors. The source of every error can be masked from the corresponding bit of the LINK_CONF3
register.
The peripheral can be in one of four main operating phases: RESET, WAIT BS, BLOCK SYNC, or DATA. Upon reset the peripheral starts in the RESET phase. The WAIT BS and BLOCK SYNC phases are used during the initialization of the JESD204 link. The DATA phase is used during normal operation when user data is received across the JESD204 link.
The RESET phase is the default state entered during reset. While disabled the peripheral will stay in the RESET phase. When enabled the peripheral will transition from the RESET phase to the WAIT FOR PHY phase.
If at any point the peripheral is disabled it will automatically transition back to the RESET state.
During the WAIT BS phase the peripheral will wait for all PHY controllers for all enabled lanes to reach sync header alignment state ensuring the sync header stream separation from the data blocks. Once this condition is satisfied the controlled will transition to the BLOCK SYNC phase.
If one of the enabled lanes loses the the sync header alignment the link will fall back to WAIT BS state.
The BLOCK SYNC state ensures all enabled lanes achieved sync header alignment or block synchronization phase in other terms. During this state the peripheral will wait for all enabled lanes to reach extended multiblock alignment and the elastic buffer get released. Once each enabled lane is extended multiblock aligned for each lane the data blocks are stored in the elastic buffer then are released at a well defined moment relative to the SYSREF
signal.
The DATA phase is the main operating mode of the peripheral. In this phase it will transmit transport layer data at the RX_DATA
port. When the peripheral enters the DATA phase the valid
signal of the RX_DATA
interface will be asserted to indicate that transport layer data is now available.
For each lane a state machine is used to detect the boundary of the extended multiblocks by tracking well defined markers in the sync header stream. Once the boundary is detected for each lane the corresponding data stream can be aligned across all enabled lanes. This is done through the elastic buffer.
The EMB INIT is the default state of the state machine, all disabled lanes stay in this state. The state is left only when the lane is enabled, the PHY controller of the corresponding lane is sync header aligned and a valid end of extended multiblock marker is detected in the sync header stream.
At any moment the PHY loses sync header alignment the state machine will fall back to the EMB INIT state.
In the EMB HUNT state the state machine will look after four consecutive correct extended multiblock indicators, once this is achieved the state machine enters the EMB LOCK state. In case invalid end of multiblock or end of extended multiblock markers are detected the state machine falls back to the EMB INIT state.
In the EMB LOCK state the monitoring of multiblock and extended multiblock indicators is continued. In case of eight consecutive indicators are incorrect the state machine will return in the EMB INIT state. This state ensures the validity of the 32 bit sync words constructed from the sync header stream. For each multiblock the calculated CRC of the previous multiblock is extracted from the current sync word.
In case ASYNC_CLK
parameter is set, a gearbox with 4:N (204B) or 8:N (204C) ratio is enabled in the link layer peripherals, where N depends on the F parameter of the link.
The goal of the gearbox is to have at the transport layer interface a data width that contains an integer number of frames per every device clock cycle (each beat) so an integer number of samples can be delivered/consumed to/from the application layer aligned to SYSREF ensuring deterministic latency in modes where N'=12 or F!=1,2,4.
The gearbox ratio corresponds with the ratio of the link layer interface data width towards physical layer and transport layer in octets. The interface width towards the physical layer in 8B/10B (204B) mode depends on the DATA_PATH_WIDTH synthesis parameter, and can be either 4 octets (default) or 8 octets. In 204B mode the util_adxcvr supports only data width of 4 octets. In 64b66b (aka 204C) mode the data width towards the physical interface is always 8 octets.
The data path width towards the transport layer is defined by the TPL_DATA_PATH_WIDTH synthesis parameter.
The following rules apply:
The link clock and device clock ratio should be the inverse of the DATA_PATH_WIDTH : TPL_DATA_PATH_WIDTH ratio.
In this context the link clock will be lane rate/40 or lane rate/80 for 204B depending on DATA_PATH_WIDTH and lane rate / 66 for 204C 64B/66B, however the device clock could vary based in the F parameter.
Deterministic latency can be reduced by adjusting the release point of the elastic buffer in RX link layer.
By default the release point of the elastic buffer is at the edge of LEMC.
In case of 64b66b link the LATENCY
register will indicate how many octets will the elastic buffer store before the default release point for that specific lane. The release point can be adjusted to bring it closer to the last arrival lane (that will have the least octets in the buffer) so minimizing the buffer usage and the latency in turn. The LATENCY
must be measured over multiple power-ups and bring-up sequence. Identify the slowest arrival lane (min value of the register). If multiple parallel links must be synchronized all lanes from all links must be included in the process.
Once the slowest lane delay is identified, before enabling the links, SW needs to set the register BUFFER_DEALY
(0x240) from all parallel Rx links if exists based on the following formula:
Where:
SYNTH_DATA_PATH_WIDTH
(0x14) reg TPL_DATA_PATH_WIDTH
field.This value it the absolute minimum. It is recommended to increase it slightly to have a better margin against power-up to power-up latency variations.
During the design of the peripheral the deliberate decision was made to support only a subset of the features mandated by the JESD204 standard for receiver logic devices. The reasoning here is that the peripheral has been designed to interface to Analog Devices JESD204 ADC converter devices and features that are either not required or not supported by those converter devices would otherwise lie dormant in peripheral and never be used. Instead the decision was made to not implement those unneeded features even when the JESD204 standard requires them for general purpose JESD204 receiver logic devices. As Analog Devices ADC converter devices with new requirements are released the peripheral will be adjusted accordingly.
This approach allows for a leaner design using less resources, allowing for lower pipeline latency and a higher maximum device clock frequency.
The following lists where the peripheral deviates from the standard:
Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Clock, etc) via the EngineerZone under the GPL license. If you would like deterministic support when using this core with an ADI component, please investigate a commercial license. Using a non-ADI JESD204 device with this core is possible under the GPL, but Analog Devices will not help with issues you may encounter.