Wiki

This version is outdated by a newer approved version.DiffThis version (12 Apr 2022 13:19) was approved by Alin-Tudor Sferle.The Previously approved version (18 Mar 2022 12:54) is available.Diff

This is an old revision of the document!


UTIL_MII_TO_RMII

The util_mii_to_rmii IP core is designed to interface the Zynq-7000/Zynq UltraScale+ MPSoC - PS Gigabit Ethernet MAC and Reduced Media Independent Interface (RMII) ADIN1300 PHY from the CN0506 Dual PHY Ethernet evaluation board.

Features

  • configurable interface for the MAC block (Media Independent Interface - MII or Gigabit Media Independent Interface - GMII)
  • configurable data rate for the MAC block and PHY chip

Files

Name Description
mac_phy_link.v Verilog source for the conversion between MII MAC block interface and RMII PHY chip interface.
phy_mac_link.v Verilog source for the conversion between RMII PHY chip interface and MII MAC block interface.
util_mii_to_rmii.v Verilog source for the main module made of the MII and RMII interfaces.

Block Diagram

Configuration Parameters

Name Description Default
INTF_CFG MAC Block Interface Selection (0 = GMII, 1 = MII). 0
RATE_10_100 Data Rate Selection (0 = 100 Mbps, 1 = 10 Mbps). 0

Interfaces

Interface Pin Type Description
MAC-PHY Link (MII MAC Block to RMII PHY) MII to RMII conversion signals
mac_txd input [3:0] MII Transmit Data
mac_tx_en input MII Transmit Enable
mac_tx_er input MII Transmit Error
mii_tx_clk output MII Transmit Clock
rmii_txd output [1:0] RMII (PHY) Transmit Data
rmii_tx_en output RMII (PHY) Transmit Enable
PHY-MAC Link (RMII PHY to MII MAC Block) RMII to MII conversion signals
mii_col output MII Collision Detect signal (only in half-duplex mode)
mii_crs output MII Carrier Sense signal (only in half-duplex mode)
mii_rxd input [3:0] MII Receive Data
mii_rx_clk input MII Receive Clock
mii_rx_dv input MII Receive Data Valid
mii_rx_er input MII Receive Error
phy_crs_dv output PHY (RMII) Carrier Sense/Data Valid
phy_rxd output[1:0] PHY (RMII) Receive Data
phy_rx_er output PHY (RMII) Receive Error
External
ref_clk input Reference Clock for MII to RMII IP core
reset_n input Active-Low reset for MII to RMII IP core

Register Map

There is no register map defined for this IP core.

Theory of operation

The following timing diagrams illustrate different signal protocols for MII and RMII interfaces at data rates of 100 and 10 Mbps.

Receive Transactions

  • RMII (PHY) receive transaction at 100 Mbps with no errors and phy_crs_dv asserted until the final packet dibit. According to the RMII Specification Rev. 1.2, after the assertion of phy_crs_dv, several 00's dibits can precede the preamble 01's dibits. The preamble is composed of 28 “01” dibits and the start of frame delimiter of 3 “01” dibits and one “11” dibit followed by the frame containing 64-1522 bytes:

  • RMII (PHY) receive transaction at 100 Mbps with no errors and phy_crs_dv toggling at 25 MHz starting on a nibble boundary and indicates the PHY has lost the carrier but has accumulated nibbles to transfer:

  • At a data rate of 10 Mbps (ref_clk frequency divided by 10), mii_rxd will be sampled every 10^th cycle.
  • MII receive transaction converted from RMII (PHY) receive transaction at 100 Mbps. In the MII mode mii_rx_dv and mii_rxd will be sampled on the falling edge of the 25 MHz mii_rx_clk and when mii_rx_dv is de-asserted, mii_rxd will present 0b0000 to the Ethernet MAC:

Transmit Transactions

  • MII transmit transaction at 100 Mbps. In the MII mode mii_tx_en and mii_txd will be sampled on the rising edge of the 25 MHz mii_tx_clk:

  • In case of errors detection, mii_tx_er will be asserted and mii_txd dibits will be “01” for the rest of transmission to RMII interface.
  • At a data rate of 10 Mbps (ref_clk frequency divided by 10), mii_txd will be sampled every 10^th cycle.
  • RMII transmit transaction converted from MII transmit transaction at 100 Mbps. In the RMII mode rmii_tx_en and rmii_txd will be sampled on the rising edge of the 50 MHz ref_clk:

Software Support

Analog Devices recommends to use the provided software drivers.

References

resources/fpga/docs/util_mii_to_rmii.1649762349.txt.gz · Last modified: 12 Apr 2022 13:19 by Alin-Tudor Sferle