This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:docs:util_extract [14 Jan 2021 05:24] – use / interwiki links Robin Getz | resources:fpga:docs:util_extract [13 Oct 2021 08:33] (current) – Edit footer Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== UTIL_EXTRACT ===== | + | ====== UTIL_EXTRACT |
The UTIL_EXTRACT IP allows the extraction of the trigger signal and restoration of the data signal that was embedded in the data stream by the AXI_ADC_TRIGGER IP. | The UTIL_EXTRACT IP allows the extraction of the trigger signal and restoration of the data signal that was embedded in the data stream by the AXI_ADC_TRIGGER IP. | ||
- | ==== Configuration Parameters ==== | + | |
+ | ===== Configuration Parameters | ||
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ | ||
Line 9: | Line 10: | ||
| '' | | '' | ||
- | ==== Interface ==== | + | |
+ | ===== Interface | ||
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
Line 22: | Line 24: | ||
| | '' | | | '' | ||
- | ==== References ==== | + | |
+ | ===== References | ||
* [[https:// | * [[https:// | ||
* [[/ | * [[/ | ||
- | {{navigation #axi_ip|AXI IP#hdl|Main page#tips|Tips}} | + | {{navigation |