Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:docs:git [14 Jan 2021 05:24]
Robin Getz use ez> / interwiki links
resources:fpga:docs:git [11 Jul 2022 09:22]
Iulia Moldovan Cosmetic changes
Line 9: Line 9:
  
 If you want to pull down the sources as soon as possible, just do the following few steps: If you want to pull down the sources as soon as possible, just do the following few steps:
-  - Install Git from [[https://​git-scm.com/​|here]].+  - Install Git from [[https://​git-scm.com/​|here]]
   - Open up Git bash, change your current directory to a place where you want to keep the hdl source   - Open up Git bash, change your current directory to a place where you want to keep the hdl source
   - Clone the repository using [[https://​help.github.com/​articles/​cloning-a-repository/​|these]] instructions   - Clone the repository using [[https://​help.github.com/​articles/​cloning-a-repository/​|these]] instructions
Line 19: Line 19:
 <block 60%> <block 60%>
   .   .
 +  ├─ .github
 +  ├─ docs
   ├─ projects   ├─ projects
   ├─ library   ├─ library
Line 85: Line 87:
 </​block>​ </​block>​
  
-The library folder contains all the IP cores and common modules. An IP, in general, contains Verilog files, which describe the hardware logic, constraint files, to ease timing closure, and Tcl scripts, which generate all the other files required for IP integration(*_ip.tcl for Vivado and *_hw.tcl for Quartus) ​+The library folder contains all the IP cores and common modules. An IP, in general, contains Verilog files, which describe the hardware logic, constraint files, to ease timing closure, and Tcl scripts, which generate all the other files required for IP integration (*_ip.tcl for Vivado and *_hw.tcl for Quartus) ​.
  
-<note tip>In case of Vivado, all the IPs must be '​packed'​ before being used in a design. To find more information about how to build the libraries please visit the [[/​resources/​fpga/​docs/​build|Building & Generating programming files]] section.</​note>  ​+<note tip>Regarding ​Vivado, all the IPs must be '​packed'​ before being used in a design. To find more information about how to build the libraries please visit the [[/​resources/​fpga/​docs/​build|Building & Generating programming files]] section.</​note>  ​
  
 ===== Repository Releases and Branches ===== ===== Repository Releases and Branches =====
Line 95: Line 97:
 All our release branches have the following naming convention: **hdl_**[year_of_release]**_r**[1 or 2]. (e.g. [[https://​github.com/​analogdevicesinc/​hdl/​tree/​hdl_2014_r2|hdl_2014_r2]]) All our release branches have the following naming convention: **hdl_**[year_of_release]**_r**[1 or 2]. (e.g. [[https://​github.com/​analogdevicesinc/​hdl/​tree/​hdl_2014_r2|hdl_2014_r2]])
  
-ADI does two releases each year when all the projects get an update to support the latest tools and get additional new features. ** The master branch is always ​synced ​with the latest release.** ​   +ADI does two releases each year when all the projects get an update to support the latest tools and get additional new features. ** The master branch is always ​synchronized ​with the latest release.** ​   
-If you are in doubt, ask us on [[ez>​community/​fpga|Engineer Zone]]. ​+If you are in doubt, ask us on [[ez>​community/​fpga|FPGA Engineer Zone]]. ​
  
 <note tip> <note tip>
resources/fpga/docs/git.txt · Last modified: 11 Jul 2022 09:22 by Iulia Moldovan