This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:docs:axi_clkgen [07 Jul 2017 13:20] – Fix link to landing page Istvan Csomortani | resources:fpga:docs:axi_clkgen [12 Oct 2021 16:45] (current) – Edit title Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== AXI_CLKGEN | + | ====== AXI CLKGEN |
The [[https:// | The [[https:// | ||
- | ==== Block Diagram ==== | ||
- | {{ : | + | ===== Block Diagram ===== |
+ | |||
+ | {{ : | ||
\\ | \\ | ||
- | The top module, axi_clkgen, instantiates a mmcm wrapper, the CLKGEN register map and the AXI handling interface. | + | The top module, axi_clkgen, instantiates a [[https:// |
- | The ad_mmcm_drp is a wrapper over MMCM, which can instantiate a Virtex 6 MMCM or 7 Series MMCM. Detailed information regarding the 7 Series MMCM can be found in Xilinx UG472 and UG953. | + | The ad_mmcm_drp is a wrapper over MMCM, which can instantiate a Virtex 6 MMCM or 7 Series MMCM. Detailed information regarding the 7 Series MMCM can be found in Xilinx |
The register map allows resetting the MMCM, changing the clock source, checking the status of the MMCM lock and controlling the DRP interface. | The register map allows resetting the MMCM, changing the clock source, checking the status of the MMCM lock and controlling the DRP interface. | ||
- | ==== Configuration | + | |
+ | ===== Configuration | ||
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ | ||
Line 27: | Line 29: | ||
| '' | | '' | ||
| '' | | '' | ||
- | | '' | ||
- | | '' | ||
- | ==== Signal and Interface Pins ==== | + | |
+ | ===== Signal and Interface Pins ===== | ||
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
- | | '' | + | | '' |
- | | | '' | + | | |
- | | | '' | + | | |
- | | | '' | + | | |
- | | | '' | + | | |
- | | '' | + | | '' |
+ | |||
+ | |||
+ | ===== Register Map ===== | ||
- | ==== Register Map ==== | ||
{{page>: | {{page>: | ||
{{page>: | {{page>: | ||
- | {{navigation #axi_ip|AXI IP#hdl|Main page# | ||
+ | ===== References ===== | ||
+ | |||
+ | * [[xilinx> | ||
+ | * [[xilinx> | ||
+ | {{navigation HDL User Guide# |