This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:fpga:docs:axi_adc_trigger [31 May 2017 10:41] – Adrian Costina | resources:fpga:docs:axi_adc_trigger [13 Oct 2021 09:56] (current) – Edit footer & add reference to generic ADC Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== AXI_ADC_TRIGGER ===== | + | ====== AXI_ADC_TRIGGER |
- | The AXI_ADC_TRIGGER IP implements triggering for the ADC path and also controls two I/O triggering pins. | + | The AXI_ADC_TRIGGER IP implements triggering for the ADC path and also controls two I/O triggering pins.\\ |
+ | \\ | ||
+ | More about the generic framework interfacing ADCs can be read here: [[: | ||
- | ==== Features ==== | + | |
+ | ===== Features | ||
* AXI Lite control/ | * AXI Lite control/ | ||
Line 18: | Line 21: | ||
* Falling edge | * Falling edge | ||
* Mixing analog and digital triggers | * Mixing analog and digital triggers | ||
+ | * Instrument trigger (from Logic Analyzer) | ||
* Controls two IO trigger pins | * Controls two IO trigger pins | ||
- | ==== Block Diagram ==== | ||
- | {{ : | + | ===== Block Diagram ===== |
- | ==== Interface ==== | + | {{: |
+ | |||
+ | ==== AXI ADC Tigger submodules ==== | ||
+ | |||
+ | * [[: | ||
+ | * **Channel trigger** | ||
+ | * Channel A | ||
+ | * Amplitude limit - REG_LIMIT_A(0x0014) - Defines the treashold level for the ADC trigger | ||
+ | * Function - TRIGGER_FUNCTION_A(0x0018) - Lower, higher than limit; pass through limit | ||
+ | * Hysteresis - TRIGGER_FUNCTION_A (0x001c) - " | ||
+ | * Channel B | ||
+ | * Amplitude limit - REG_LIMIT_A(0x0024) - Defines the treashold level for the ADC trigger | ||
+ | * Function - TRIGGER_FUNCTION_A(0x0028) - Lower, higher than limit; pass through limit | ||
+ | * Hysteresis - TRIGGER_FUNCTION_A (0x002c) - " | ||
+ | |||
+ | * **External trigger** | ||
+ | * Pin 0 (Ti) \\ Configurations - REG_CONFIG_TRIGGER_I(0x004) allows for: | ||
+ | * falling edge (bit 8) | ||
+ | * rising edge (bit 6) | ||
+ | * any edge (bit 4) | ||
+ | * high level (bit 2) | ||
+ | * low level (bit 0) | ||
+ | * Pin 1 (To) \\ Configurations - REG_CONFIG_TRIGGER_I(0x004) allows for: | ||
+ | * falling edge (bit 9) | ||
+ | * rising edge (bit 7) | ||
+ | * any edge (bit 5) | ||
+ | * high level (bit 3) | ||
+ | * low level (bit 1) | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | * **Channel A MUX** - REG_TRIGGER_MUX_A(0x0020) - Selects between a combination of ADC trigger and the external trigger | ||
+ | * **Channel B MUX** - REG_TRIGGER_MUX_B(0x0030) - Selects between a combination of ADC trigger and the external trigger | ||
+ | |||
+ | * **Output MUX** - REG_TRIGGER_OUT_CONTROL(0x0034) - Selects a combination between the channel A and/or B MUX's and the input of the instrument trigger | ||
+ | * **Holdoff counter** (32 bit) - REG_TRIGGER_HOLDOFF(0x0048) - Controls the trigger out silent period after an event. | ||
+ | * **Delay counter** (32 bit) - REG_TRIGGER_DELAY(0x0040) - Controls the trigger delay | ||
+ | |||
+ | * **External trigger control** | ||
+ | * REG_IO_SELECTION(0x000c) - Controls the direction of the external trigger pins, and the source(for each pin configured as output) | ||
+ | * REG_TRIGGER_OUT_HOLD_PINS(0x004c) - Controls the hold period after a transition to a new logic level. | ||
+ | |||
+ | |||
+ | ===== Interface | ||
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
Line 43: | Line 89: | ||
| | '' | | | '' | ||
| | '' | | | '' | ||
- | | **Trigger Offset** |||| | + | | | '' |
- | | |'' | + | | | '' |
+ | | **Fifo Depth** |||| | ||
+ | | |'' | ||
| **AXI_S_MM interface** |||| | | **AXI_S_MM interface** |||| | ||
| | '' | | | '' | ||
- | ==== Detailed Description ==== | ||
- | The AXI_ADC_TRIGGER IP implements triggering for the ADC path based on two trigger pins or based on the analog channel. | + | ===== Detailed Description ===== |
+ | |||
+ | The AXI_ADC_TRIGGER IP implements triggering for the ADC path. The trigger is generated | ||
+ | |||
+ | The external trigger pins are controlled by the core and can be both input or output. For external triggering, they must be set to inputs(independently). | ||
+ | |||
+ | The analog triggering is based on comparison with a limit. The data format must be 2's complement and the maximum number of bits of the analog channel | ||
+ | The trigger can be transmitted independent or embedded in the output word, at bit 15. When embedded, the triggers must be extracted and data must be reconstructed, | ||
+ | Embedding the trigger in the data allows for additional IPs with unknown pipeline length to be introduced in the path. | ||
+ | |||
+ | If a history for data before the trigger is needed, a [[: | ||
+ | |||
+ | |||
+ | ===== Register Map ===== | ||
- | The trigger | + | |< 100% 5% 5% 5% 25% 5% 5% 50% >| |
+ | |Address ||Bits |Name |Type |Default |Description | | ||
+ | |DWORD |BYTE |::: |::: |::: |::: |::: | | ||
+ | ^0x0000 ^0x0000 ^REG_VERSION ^^^^Version Register ^ | ||
+ | | | |[31:0] |VERSION |RO |0x00 |Version number | | ||
+ | ^0x0001 ^0x0004 ^REG_SCRATCH ^^^^Scratch Register ^ | ||
+ | | | |[31:0] |SCRATCH |RW |0x00 |Scratch register | | ||
+ | ^0x0002 ^0x0008 ^REG_TRIGGER_O ^^^^Control TRIGGER_O Value ^ | ||
+ | | | |[1] |TRIGGER_O[1] |RW |0x00 |Set TRIGGER_O[1] value | | ||
+ | |::: |::: |[0] |TRIGGER_O[0] |RW |0x00 |Set TRIGGER_O[0] value | | ||
+ | ^0x0003 ^0x000c ^REG_IO_SELECTION ^^^^Control Trigger Pins Direction ^ | ||
+ | | | |[7:5] |TRIGGER_O[1] (To PIN) |RW |0x00 |Select output | ||
+ | |::: |::: |[4:2] |TRIGGER_O[0] (Ti PIN) |RW |0x00 |Select output trigger pin 0 \\ 0: SOFTWARE TRIGGER - TRRIGER_O[0](0x0004) \\ 1: TRIGGER_I[0] (PIN) \\ 2: TRIGGER_I[1] (PIN) \\ 3: TRIGGER_OUT (axi_adc_trigger) | ||
+ | |::: |::: |[1] |IO_SELECTION[1] |RW |0x00 |Drives | ||
+ | |::: |::: |[0] |IO_SELECTION[0] |RW |0x00 |Drives the TRIGGER_T[0](Ti) pin | | ||
+ | ^0x0004 ^0x0010 ^REG_CONFIG_TRIGGER_I ^^^^Configure Digital Triggering ^ | ||
+ | | | |[9:8] |FALL_EDGE |RW |0x00 |Enable falling edge triggering for TRIGGER[0] | ||
+ | |::: |::: |[7:6] |RISE_EDGE |RW |0x00 |Enable rising edge triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
+ | |::: |::: |[5:4] |ANY_EDGE |RW |0x00 |Enable any edge triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
+ | |::: |::: |[3:2] |HIGH_LEVEL |RW |0x00 |Enable high level triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
+ | |::: |::: |[1:0] |LOW_LEVEL |RW |0x00 |Enable low level triggering for TRIGGER[0] or TRIGGER[1] pin | | ||
+ | ^0x0005 ^0x0014 ^REG_LIMIT_A ^^^^Analog Trigger Level for Channel ^ | ||
+ | | | |[15:0] |LIMIT_A[15: | ||
+ | ^0x0006 ^0x0018 ^REG_FUNCTION_A ^^^^Analog Triggering Function ^ | ||
+ | | | |[1:0] |TRIGGER_FUNCTION_A |RW |0x00 |Analog triggering function for channel A: \\ 0: Lower than limit \\ 1: higher than limit \\ 2: pass through high limit \\ 3: passthrough low limit | | ||
+ | ^0x0007 ^0x001c ^REG_HYSTERESIS_A ^^^^Analog Trigger Hysteresis for Channel ^ | ||
+ | | | |[31:0] |HYSTERESIS_A |RW |0x00 |Used for the passthrough functions | | ||
+ | ^0x0008 ^0x0020 ^REG_TRIGGER_MUX_A ^^^^Trigger Selection for Path ^ | ||
+ | | | |[3:0] |TRIGGER_MUX_A |RW |0x00 |Selects trigger a mode: \\ 0: Always on \\ 1: Digital | ||
+ | ^0x0009 ^0x0024 ^REG_LIMIT_B ^^^^Analog Trigger Level for Channel ^ | ||
+ | | | |[15:0] |LIMIT_B[15: | ||
+ | ^0x000A ^0x0028 ^REG_FUNCTION_B ^^^^Analog Triggering Function ^ | ||
+ | | | |[1:0] |TRIGGER_FUNCTION_B |RW |0x00 |Analog triggering function for channel B: \\ 0: Lower than limit \\ 1: higher than limit \\ 2: pass through high limit \\ 3: passthrough low limit | | ||
+ | ^0x000B ^0x002c ^REG_HYSTERESIS_B ^^^^Analog Trigger Hysteresis for Channel ^ | ||
+ | | | |[31:0] |HYSTERESIS_B |RW |0x00 |Used for the passthrough functions | | ||
+ | ^0x000C ^0x0030 ^REG_TRIGGER_MUX_B ^^^^Trigger Selection for Path ^ | ||
+ | | | |[3:0] |TRIGGER_MUX_B |RW |0x00 |Selects trigger B mode: \\ 0: Always on \\ 1: Digital triggering, based on trigger[1] \\ 2: ADC triggering, based on channel B \\ 3: Reserved \\ 4: Digital triggering OR ADC triggering \\ 5: Digital triggering AND ADC triggering \\ 6: Digital triggering XOR ADC triggering \\ 7: Option 4 negated \\ 8: Option 5 negated \\ 9: Option 6 negated | | ||
+ | ^0x000D ^0x0034 ^REG_TRIGGER_OUT_CONTROL ^^^^Selection Multiplexer and embedded trigger selection ^ | ||
+ | | | |[16] |EMBEDDE_TRIGGER |RW |0x00 |When set the bit 15 of the out channel data will be the trigger. This alows to keep the data in sync with the trigger in future data processing, before feeding the data to the DMA.\\ When set a util_extract module is required in the system. | | ||
+ | |::: |::: |[3:0] |TRIGGER_MUX_OUT |RW |0x00 |Final Trigger Selection Multiplexer \\ Selects trigger a mode: \\ 0: Trigger A \\ 1: Trigger B \\ 2: Trigger A OR Trigger B \\ 3: Trigger A AND Trigger B \\ 4: Trigger A XOR Trigger B \\ 5: Trigger LA \\ 6: Trigger A OR Trigger LA \\ 7: Trigger B OR Trigger LA \\ 8: Trigger A OR Trigger B OR Trigger LA | | ||
+ | ^0x000E ^0x0038 ^REG_FIFO_DEPTH ^^^^Controls the Dynamic Depth of the History FIFO ^ | ||
+ | | | |[31:0] |FIFO_DEPTH |RW |0x00 |Controls the depth of the history FIFO. Should be less than the maximum FIFO depth. If set to 0, the FIFO is bypassed. | | ||
+ | ^0x000F ^0x003c ^REG_TRIGGERED ^^^^Indicates Triggering Status ^ | ||
+ | | | |[0] |TRIGGERED |RW1C |0x00 |Indicates if the trigger has been triggered since the last time this register has been reset. | | ||
+ | ^0x0010 ^0x0040 ^REG_TRIGGER_DELAY ^^^^Control the Trigger Delay ^ | ||
+ | | | |[31:0] |TRIGGER_DELAY |RW |0x00 |Delays the start of data capture with TRIGGER_DELAY number of samples after the trigger. | | ||
+ | ^0x0011 ^0x0044 ^REG_STREAMING ^^^^Controls Streaming Mode ^ | ||
+ | | | |[0] |STREAMING |RW |0x00 |If the streaming bit is set, after the trigger condition is met data will be continuously captured by the DMA. The streaming bit must be set to 0 to reset triggering. | ||
+ | ^0x0012 ^0x0048 ^REG_TRIGGER_HOLDOFF ^^^^Controls hold off time ^ | ||
+ | | | |[31:0] |TRIGGER_HOLDOFF |RW |0x00 |Defines the time interval, after a trigger event, where the next trigger events will be ignored, until the end of the interval. The time interval is set by counter. Down-counting on the ADC clock(100MHz). The value written in the register is loaded in the counter at a trigger event. | | ||
+ | ^0x0013 ^0x004c ^REG_TRIGGER_OUT_HOLD_PINS ^^^^Controls external trigger hold time ^ | ||
+ | | | |[19:0] |TRIGGER_OUT_HOLD_PINS |RW |0x00 |Defines a time period, in which the external trigger pins, configured as outputs, will hold the new logic level after a transition. The down-counter, | ||
+ | ^Tue Sep 1 09:58:53 2020 ^^^^^^ | ||
- | The analog triggering is based on comparison with a limit. The data format must be 2's complement and maximum number of bits of the analog channel is 15. | ||
- | The trigger is embedded in the output word, at bit 15. Before forwarding the data to the DMA, the triggers must be extracted and data must be reconstructed. The UTIL_EXTRACT IP can be used for this purpose. | ||
- | Embedding the trigger with the data allows for additional IPs with unknown pipeline length to be introduced in the path. | ||
- | If a history for data before the trigger is needed to be transfered, a variable FIFO IP should be used. The FIFO depth is controlled using the trigger_offset bus of this IP. | + | ===== Aditional notes ===== |
- | ==== Register Map ==== | + | <note important> |
- | ==== Analog Trigger (axi_adc_trigger) ==== | ||
- | |< 100% 5% 5% 5% 25% 5% 55% >| | + | ===== References ===== |
- | |Address ||Bits |Name |Type |Description | | + | |
- | |DWORD |BYTE |::: |::: |::: |::: | | + | |
- | ^0x0000 ^0x0000 ^REG_VERSION ^^^Version Register ^ | + | |
- | | | |[31:0] |VERSION |RO |Version number. | | + | |
- | ^0x0001 ^0x0004 ^REG_SCRATCH ^^^Scratch Register ^ | + | |
- | | | |[31:0] |SCRATCH |RW |Instance identifier number. | | + | |
- | ^0x0002 ^0x0008 ^REG_TRIGGER_O ^^^Control TRIGGER_O value ^ | + | |
- | | | |[1] |TRIGGER_O |RW |Set TRIGGER_O[1] value | | + | |
- | |::: |::: |[0] |RSTN |RW |Set TRIGGER_O[0] value | | + | |
- | ^0x0003 ^0x000c ^REG_IO_SELECTION ^^^Clock Select ^ | + | |
- | | | |[1] |IO_SELECTION |RW |Drives the TRIGGER_T[1] pin | | + | |
- | |::: |::: |[0] |IO_SELECTION |RW |Drives the TRIGGER_T[0] pin | | + | |
- | ^0x0004 ^0x0010 ^REG_CONFIG_TRIGGER ^^^Configures the digital triggering mechanism ^ | + | |
- | | | |[9:8] |FALL_EDGE |RW |Enable falling edge triggering for TRIGGER[0] or TRIGGER[1] pin | | + | |
- | |::: |::: |[7:6] |RISE_EDGE |RW |Enable rising edge triggering for TRIGGER[0] or TRIGGER[1] pin | | + | |
- | |::: |::: |[5:4] |ANY_EDGE |RW |Enable any edge triggering for TRIGGER[0] or TRIGGER[1] pin | | + | |
- | |::: |::: |[3:2] |HIGH_LEVEL |RW |Enable high level triggering for TRIGGER[0] or TRIGGER[1] pin | | + | |
- | |::: |::: |[1:0] |LOW_LEVEL |RW |Enable low level triggering for TRIGGER[0] or TRIGGER[1] pin | | + | |
- | ^0x0005 ^0x0014 ^REG_LIMIT_A ^^^Analog trigger level for channel A ^ | + | |
- | | | |[15:0] |LIMIT_A[15: | + | |
- | ^0x0006 ^0x0018 ^REG_FUNCTION_A ^^^Analog triggering function A ^ | + | |
- | | | |[1:0] |TRIGGER_FUNCTION_A |RW |Analog triggering function for channel A:\\ 0: Lower than limit\\ 1: higher than limit\\ 2: pass through high limit\\ 3: passthrough low limit | | + | |
- | ^0x0007 ^0x001c ^REG_HYSTERESIS_A ^^^Analog trigger histeresys for channel A ^ | + | |
- | | | |[31:0] |HISTERESYS_A |RW |Used for the passthrough functions | | + | |
- | ^0x0008 ^0x0020 ^REG_TRIGGER_MUX_A ^^^Trigger selection ^ | + | |
- | | | |[3:0] |TRIGGER_MUX_A |RW |Selects trigger a mode:\\ 0: Always on\\ 1: Digital triggering, based on trigger[0]\\ 2: | + | |
- | ^0x0009 ^0x0024 ^REG_LIMIT_B ^^^Analog trigger level for channel B ^ | + | |
- | | | |[15:0] |LIMIT_B[15: | + | |
- | ^0x000A ^0x0028 ^REG_FUNCTION_B ^^^Analog triggering function B ^ | + | |
- | | | |[1:0] |TRIGGER_FUNCTION_B |RW |Analog triggering function for channel B:\\ 0: Lower than limit\\ 1: higher than limit\\ 2: pass through high limit\\ 3: passthrough low limit | | + | |
- | ^0x000B ^0x002c ^REG_HYSTERESIS_B ^^^Analog trigger histeresys for channel B ^ | + | |
- | | | |[31:0] |HISTERESYS_B |RW |Used for the passthrough functions | | + | |
- | ^0x000C ^0x0030 ^REG_TRIGGER_MUX_B ^^^Trigger selection ^ | + | |
- | | | |[3:0] |TRIGGER_MUX_B |RW |Selects trigger a mode:\\ 0: Always on\\ 1: Digital triggering, based on trigger[1]\\ 2: ADC triggering, based on channel B\\ 3: Reserved\\ 4: Digital triggering OR ADC triggering\\ 5: Digital triggering AND ADC triggering\\ 6: | + | |
- | ^0x000D ^0x0034 ^REG_TRIGGER_MUX_OUT ^^^Final trigger selection mux ^ | + | |
- | | | |[2:0] |TRIGGER_MUX_OUT |RW |Selects trigger a mode:\\ 0: Trigger A\\ 1: Trigger B\\ 2: Trigger A OR Trigger B \\ 3: Trigger A AND Trigger B\\ 4: Trigger A XOR Trigger B | | + | |
- | ^0x000E ^0x0038 ^REG_TRIGGER_DELAY ^^^Controls the depth of the history FIFO ^ | + | |
- | | | |[31:0] |Controls the depth of the history FIFO. If set to 0, the FIFO is bypassed. |RW |Selects trigger a mode:\\ 0: Trigger A\\ 1: Trigger B\\ 2: Trigger A OR Trigger B\\ 3: Trigger A AND Trigger B\\ 4: Trigger A XOR Trigger B | | + | |
- | ==== References ==== | + | |
- | | + | * [[/ |
- | * [[https:// | + | |
* [[https:// | * [[https:// | ||
- | {{navigation #axi_ip|AXI IP#hdl|Main page#tips|Tips}} | + | {{navigation |