Wiki

This version is outdated by a newer approved version.DiffThis version (31 Aug 2020 15:07) was approved by Andrei Grozav.The Previously approved version (06 Jun 2018 12:52) is available.Diff

This is an old revision of the document!


AXI_ADC_DECIMATE

The AXI_ADC_DECIMATE IP allows decimating of the input data by 10/100/1000/10000/100000, with filtering and arbitrary decimation by dropping samples.

Features

  • AXI Lite control/status interface
  • Allows decimation by 10/100/1000/10000/100000 with filtering
  • Allows arbitrary decimation by dropping samples
  • Filtering is implemented by a 6 sections CIC programmable rate filter and a compensation FIR filter.

Block Diagram

Configuration Parameters

Name Description Default Value
CORRECTION_DISABLE Disable scale correction of the CIC output 1

Interface

Interface Pin Type Description
Clock
adc_clk input Clock input
Reset
adc_rst input Reset, synchronous on the adc_clk clock domain
Data Inputs
adc_data_a input[15:0] Analog data for channel A
adc_data_b input[15:0] Analog data for channel B
adc_data_valid_a input Data valid signal for channel A
adc_data_valid_b input Data valid signal for channel B
Decimated Outputs
adc_dec_data_a output[15:0] Decimated data for channel A
adc_dec_data_b output[15:0] Decimated data for channel B
adc_dec_valid_a output Data valid for channel A
adc_dec_valid_b output Data valid for channel B
adc_data_rate output[2:0] Data rate (decimation ratio)
adc_oversampling_en output Data oversampling enabled
AXI_S_MM interface
s_axi_* Standard AXI Slave Memory Map interface

Detailed Description

For some applications, the maximum sampling rate is not required and leads to lots of samples transferred to memory. In order to avoid that, the decimation IP is used.

The decimation block allows decimating the input data so that the sampling frequency to be reduced by 10, 100, 1000, 10000, 100000, with filtering.

The filtering is implemented by a 6 sections CIC programmable rate filter which allows decimation by 5/50/500/5000/50000 and a compensation FIR filter (decimation by 2).

At the end of the filter chain, there is an arbitrary decimation block. The arbitrary decimation can be activated independently and it does not implement any type of filtering.

Register Map

Address Bits Name Type Description
DWORD BYTE
0x0000 0x0000 REG_VERSION Version Register
[31:0] VERSION RO Version number
0x0001 0x0004 REG_SCRATCH Scratch Register
[31:0] SCRATCH RW Scratch register
0x0010 0x0040 REG_DECIMATION_RATIO Control Arbitrary Decimation Ratio
[31:0] DECIMATION_RATIO RW Set the arbitrary decimation ratio at the end of the decimation chain. Simply drop samples
0x0011 0x0044 REG_DECIMATION_STAGE_ENABLE Control Filtered Decimation
[2:0] FILTERED_DECIMATION_RATIO RW Enables the filtered decimation:
0: No filtered decimation
1: Decimation by 10. Result should be corrected by a 1.05 factor
2: Decimation by 100. Result should be corrected by a 1.1 factor
3: Decimation by 1000. Result should be corrected by a 1.15 factor
6: Decimation by 10000. Result should be corrected by a 1.2 factor
7: Decimation by 100000. Result should be corrected by a 1.26 factor
default: No filtered decimation
0x0012 0x0048 REG_CONFIG Configuration Register
[1] CORRECTION_ENABLE_B RW If set to 1, correction is enabled on channel B. The decimated data will be multiplied with the value from the CORRECTION_COEFFICIENT_B register.
[0] CORRECTION_ENABLE_A RW If set to 1, correction is enabled on channel A. The decimated data will be multiplied with the value from the CORRECTION_COEFFICIENT_A register.
0x0013 0x004c REG_CORRECTION_COEFFICIENT_A Correction Coefficient A
[15:0] CORRECTION_COEFFICIENT RW Scale correction (if equipped) coefficient for channel A. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification.
0x0014 0x0050 REG_CORRECTION_COEFFICIENT_B Correction Coefficient B
[15:0] CORRECTION_COEFFICIENT RW Scale correction (if equipped) coefficient for channel B. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification.

References

resources/fpga/docs/axi_adc_decimate.1598879192.txt.gz · Last modified: 31 Aug 2020 15:06 by Andrei Grozav