Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:docs:axi_adc_decimate [11 Oct 2021 15:10]
Iulia Moldovan Edit footer
resources:fpga:docs:axi_adc_decimate [13 Oct 2021 09:51]
Iulia Moldovan Edit footer & add reference to generic ADC
Line 1: Line 1:
-===== AXI_ADC_DECIMATE =====+====== AXI_ADC_DECIMATE ​======
  
-The AXI_ADC_DECIMATE IP allows decimating of the input data by 10/​100/​1000/​10000/​100000,​ with filtering and arbitrary decimation by dropping samples.+The AXI_ADC_DECIMATE IP allows decimating of the input data by 10/​100/​1000/​10000/​100000,​ with filtering and arbitrary decimation by dropping samples.\\ 
 +\\ 
 +More about the generic framework interfacing ADCs can be read here: [[:​resources:​fpga:​docs:​axi_adc_ip]].
  
-==== Features ====+ 
 +===== Features ​=====
  
   * AXI Lite control/​status interface   * AXI Lite control/​status interface
Line 10: Line 13:
   * Filtering is implemented by a 6 sections CIC programmable rate filter and a compensation FIR filter.   * Filtering is implemented by a 6 sections CIC programmable rate filter and a compensation FIR filter.
  
-==== Block Diagram ====+ 
 +===== Block Diagram ​=====
  
 {{ :​resources:​fpga:​docs:​axi_adc_decimate.svg | AXI_ADC_DECIMATE Block diagram }} {{ :​resources:​fpga:​docs:​axi_adc_decimate.svg | AXI_ADC_DECIMATE Block diagram }}
  
-=== Configuration Parameters ====+ 
 +==== Configuration Parameters ​=====
  
 ^ Name ^ Description ^ Default Value^ ^ Name ^ Description ^ Default Value^
 | ''​CORRECTION_DISABLE''​ | Disable scale correction of the CIC output | 1 | | ''​CORRECTION_DISABLE''​ | Disable scale correction of the CIC output | 1 |
  
-==== Interface ====+ 
 +===== Interface ​=====
  
 ^ Interface ^ Pin ^ Type ^ Description ^ ^ Interface ^ Pin ^ Type ^ Description ^
Line 41: Line 47:
 |              | ''​s_axi_*''​ || Standard AXI Slave Memory Map interface | |              | ''​s_axi_*''​ || Standard AXI Slave Memory Map interface |
  
-==== Detailed Description ====+ 
 +===== Detailed Description ​=====
  
 For some applications,​ the maximum sampling rate is not required and leads to lots of samples transferred to memory. In order to avoid that, the decimation IP is used. For some applications,​ the maximum sampling rate is not required and leads to lots of samples transferred to memory. In order to avoid that, the decimation IP is used.
Line 51: Line 58:
 At the end of the filter chain, there is an arbitrary decimation block. The arbitrary decimation can be activated independently and it does not implement any type of filtering. At the end of the filter chain, there is an arbitrary decimation block. The arbitrary decimation can be activated independently and it does not implement any type of filtering.
  
-==== Register Map ====+ 
 +===== Register Map =====
  
 |< 100% 5% 5% 5% 25% 5% 55% >| |< 100% 5% 5% 5% 25% 5% 55% >|
Line 72: Line 80:
 | | |[15:0] |CORRECTION_COEFFICIENT |RW |Scale correction (if equipped) coefficient for channel B. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification. | | | |[15:0] |CORRECTION_COEFFICIENT |RW |Scale correction (if equipped) coefficient for channel B. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification. |
  
-==== References ====+ 
 +===== References ​=====
   * [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​library/​axi_adc_decimate| AXI_ADC_DECIMATE IP source code]] \\   * [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​library/​axi_adc_decimate| AXI_ADC_DECIMATE IP source code]] \\
   * [[/​resources/​fpga/​docs/​arch | ADI Reference designs architecture ]] \\   * [[/​resources/​fpga/​docs/​arch | ADI Reference designs architecture ]] \\
Line 78: Line 87:
   * [[xilinx>​support/​documentation/​sw_manuals/​xilinx2016_2/​ug953-vivado-7series-libraries.pdf | 7 Series libraries]] \\   * [[xilinx>​support/​documentation/​sw_manuals/​xilinx2016_2/​ug953-vivado-7series-libraries.pdf | 7 Series libraries]] \\
  
-{{navigation #axi_ip|AXI IP#hdl|Main page#​tips|Using and modifying the HDL design}}+{{navigation ​HDL User Guide#ip_cores|IP cores#hdl|Main page#​tips|Using and modifying the HDL design}}
resources/fpga/docs/axi_adc_decimate.txt · Last modified: 13 Oct 2021 09:51 by Iulia Moldovan