Wiki

This version is outdated by a newer approved version.DiffThis version (13 Oct 2021 10:53) was approved by Adrian Costina.The Previously approved version (11 Oct 2021 14:41) is available.Diff

This is an old revision of the document!


AXI_AD9361

The axi_ad9361 IP core interfaces to the AD9361 device. This documentation only covers the IP core and requires that one must be familiar with the device for a complete and better understanding.

More about the generic framework interfacing ADCs can be read here: axi_adc_ip, and for DACs: axi_dac_ip.

Features

  • AXI Lite control/status interface
  • PRBS monitoring
  • Hardware and software DC filtering
  • IQ correction
  • Internal DDS
  • Programmable line delays
  • Receive and transmit loop back
  • Supports both Altera and Xilinx devices

Block Diagram

 AXI_AD9361 Block diagram

Functional Description

The axi_ad9361 cores architecture contains:

Device (AD9361) Interface Description

The IP supports both LVDS and CMOS interfaces (configurable, see parameters section). It avoids all the programmable flavors of the device interface mess. The interface is in fact quite simple, in LVDS mode samples require two active clock edges and in CMOS mode a single edge. The samples are then delineated in-order using the FRAME signal. This is applicable to both DDR and SDR modes. There is a limitation though, the IP core does NOT support swapping of the data ports in CMOS mode. This option is left as a constraint. As an example the PZSDR projects uses SWAP on some boards based on the board layout.

Let's consider the 2R2T configuration, each frame consists of 4 samples in each direction. In LVDS-DDR mode that is 8 clock edges (4 full clock cycles) identified by a frame pattern of 8'b11110000. The IP interface logic simply collects data on consecutive 8 edges and deframes using the FRAME signal and outputs the samples. The device does the same in the transmit direction. In CMOS mode, the same is done over 4 clock edges.

The interface also provides a single clock tree for the entire core. This clock uses a global buffer that has the minimum skew all across the die. On Altera devices, this is done via the PLL and because the LVDS cores do NOT support a serialization factor of 2, runs at half the interface clock frequency. On Xilinx devices, this is done via the BUFG and the core and interface runs at the same clock frequency.

Altera

The core is tested to work only on Cyclone V Arrow SOC Kit. Since Altera does half-thought board designs that do not favor FMC bank allocations, we are incapable of validating the core on other devices.

Xilinx

Alternative Clocking Methods

1. Using MMCM 2. Using BUFIO/BUFR

Alternative Use Models

1. Interface Logic Only 2. Disable DSP Functions 3. Removing AXI interface and Processor Control

Internal Interface Description

The main purpose of all (including this) ADI IP cores is to provide a common, well-defined internal interface within the FPGA. This interface consists of the following signals per channel.

ENABLE

The enable signal is strictly for software use and is controlled by the corresponding register bit. The core simply reflects the programmed bit as an output port. In ADI reference projects, this bit is used to activate the channel of interest. It is then used by the PACK/UNPACK cores to route the data based on total number of channels and the selected number of channels. As an example, AXI_AD9361 supports a total of 4 channels 16bits each. This corresponds to a packed channel data width of 64bits. If software enables only two channels the packed 64bits of data is exclusively shared by the enabled 2 channels (each channel gets 32bits of data).

VALID

The valid signal is sourced by the core to indicate a valid sample on the DATA port. In the receive (ADC) direction this indicates a valid sample and in the transmit (DAC) direction this indicates the current sample is being read by the core. The valid is simply a 'reflective' of the 'sampling rate'. Note that he cores always run at the interface clock. This is to avoid any customized clock handling or transfer within this core. However in many cases interface clock may not be the sampling clock. As an example for AD9361 the interface clock is 244Mhz for a sampling clock of 61MHz. That is each channel's sampling rate is 61MHz. This translates into the VALID signal being asserted once every 4 clocks. In cores where sampling rate is same as the interface clock, VALID is always asserted and may be safely ignored.

A common interpretation of this is that all channels has the same VALID behavior. This is NOT necessarily true. A majority of use cases may have this as a result of data path equivalency. However, if software decides to enable/disable functions differently among channels, the VALID signals of those channels will NOT be the same.

DATA

The DATA is the raw Analog samples. It follows two simple rules.

  1. The samples are always 16bits, regardless of the ADC/DAC data width. That is the source or destination is intended to handle samples as 16bits. In the transmit direction, if the DAC data width is less than 16bits, the most significant bits are used. In the receive direction, if the ADC data width is less than 16bits, the most significant bits are sign extended. This allows the same source or destination portable across different ADC/DAC data widths. In other words, if the source is generating a 16bits tone the signal appears the same across a 12bit, 14bit or 16bit DAC with only the corresponding amplitude change. The source can thus be independent of the number of bits supported by DAC. In the receive direction, the samples are sign extended. Thus the destination always receives a 16bit sample with different amplitude levels corresponding to the number of bits supported by the ADC. This may seem to break the symmetry rule, but in most DSP functions the samples are rounded up towards the MSB as only precision is allowed to lost or gained at the expense of the LSB bits. The MSB bits retains all the physical nature of the signal.
  2. The DATA is received and transmitted with most significant sample “newest” regardless of the channel width. In other words the most significant sample is the “newest” sample. If the total channel width is 64bits, it carries 4 samples (16bits) per clock. If we were to name these samples as S3 (bits 63 down to 48), S2 (bits 47 down to 32), S1 (bits 31 down to 16) and S0 (bits 15 down to 0), the following is true. In the transmit direction, S0 is sent first and S3 is sent last to the DAC. The analog samples are S0, S1, S2 and S3 across time with S0 being the oldest and S3 being the newest sample. In the receive direction, S0 carries the oldest sample received and S3 carries the newest sample from the ADC.

Parameters

Name Description Default Value
ID Core ID should be unique for each AD9361 IP in the system 0
DEVICE_TYPE Used to select between 7 Series (0), Virtex 6 (1) or Ultrascale (2) for Xilinx devices 0
MODE_1R1T Used to select between 2RX2TX (0) and 1RX1TX (1) mode. 0
TDD_DISABLE Setting this parameter the TDD control will not be implemented in the core. 0
CMOS_OR_LVDS_N Defines the physical interface type, set 1 for CMOS and 0 for LVDS 0
ADC_DATAPATH_DISABLE If set, the data path processing logic is not generated in the RX path, and the raw data is pushed directly to the DMA interface. 0
ADC_USERPORTS_DISABLE Disable the User Control ports in receive path. 0
ADC_DATAFORMAT_DISABLE Disable the Data Format control module. 0
ADC_DCFILTER_DISABLE Disable the DC Filter module. 0
ADC_IQCORRECTION_DISABLE Disable the IQ Correction module in receive path. 0
DAC_DATAPATH_DISABLE If set, the data path processing logic is not generated in the TX path, and the raw data is pushed directly to the physical interface. 0
DAC_IODELAY_ENABLE Set IO_DELAY control in transmit path. 0
DAC_DDS_DISABLE Disable the DDS modules in transmit path. 0
DAC_USERPORTS_DISABLE Disable the User Control ports in transmit path. 0
DAC_IQCORRECTION_DISABLE Disable the IQ Correction module in transmit path. 0
IO_DELAY_GROUP The delay group name which is set for the delay controller “dev_if_delay_group”

I/O Interface

Interface Pin Type Description
LVDS RX interface
rx_clk_in_* input LVDS input clock
rx_frame_in_* input LVDS input frame signal
rx_data_in_* input[ 5:0] LVDS input data lines
CMOS RX interface
rx_clk_in input CMOS input clock
rx_frame_in input CMOS input frame signal
rx_data_in input[11:0] CMOS input data lines
LVDS TX interface signals
tx_clk_in_* output LVDS output clock
tx_frame_in_* output LVDS output frame signal
tx_data_in_* output[ 5:0] LVDS output data lines
CMOS TX interface signals
tx_clk_in output CMOS input clock
tx_frame_in output CMOS input frame signal
tx_data_in output[11:0] CMOS input data lines
TDD control interface
enable output ENSM control signal, see User Guide for more information
txnrx output ENSM control signal, see User Guide for more information
TDD sync interface
tdd_sync input SYNC input for frame synchronization in TDD mode
tdd_sync_cntr output SYNC output for frame synchronization in TDD mode
Delay Clock
delay_clk input Delay clock input for IO_DELAY control, connect to 200 Mhz clock
Transmit master/slave
dac_sync_in input Synchronization signal of the transmit path for slave devices (ID>0)
dac_sync_out output Synchronization signal of the transmit path for master device (ID==0)
Core clock and reset
l_clk output This clock should be used for further data processing
clk input Must be driven by l_clk
rst output Core reset signal
DMA_RX interface
adc_enable_* output If set, the channel is enabled (one for each channel)
adc_valid_* output Indicates valid data at the current channel (one for each channel)
adc_data_* output[15:0] Received data output (one for each channel)
adc_dovf input Data overflow, must be connected to the DMA
adc_dunf input Data underflow, must be connected to the DMA
adc_r1_mode output If set, core is functioning in single channel mode (one I/Q pair)
DMA_TX interface
dac_enable_* output If set, the channel is enabled (one for each channel)
dac_valid_* output Indicates valid data request at the current channel (one for each channel)
dac_data_* input[15:0] Transmitted data output (one for each channel)
dac_dovf input Data overflow, must be connected to the DMA
dac_dunf input Data underflow, must be connected to the DMA
dac_r1_mode output If set, core is functioning in single channel mode (one I/Q pair)
AXI_S_MM interface
s_axi_* Standard AXI Slave Memory Map interface
GPIO interface
up_enable input GPI control of the ENABLE line in TDD mode, when HDL TDD control is DISABLED
up_txnrx input GPI control of the TXNRX line in TDD mode, when HDL TDD control is DISABLED
up_dac_gpio_in input[31:0] GPI ports connected to the AXI memory map for custom use
up_dac_gpio_out output[31:0] GPI ports connected to the AXI memory map for custom use
up_adc_gpio_in input[31:0] GPI ports connected to the AXI memory map for custom use
up_adc_gpio_out output[31:0] GPO ports connected to the AXI memory map for custom use

Register Map

Register map

The register map of the core contains instances of several generic register maps like ADC common, ADC channel, DAC common, DAC channel etc. The following table presents the base addresses of each instance, after that can be found the detailed description of each generic register map. The absolute address of a register should be calculated by adding the instance base address to the registers relative address.

Register Map base addresses for axi_ad9361

Address Name Description
DWORD BYTE
0x0000 0x0000 BASE See the Base (common to all cores) table for more detail
0x0000 0x0000 RX COMMON See the ADC Common table for more detail
0x0000 0x0000 RX CHANNELS See the ADC Channel table for more detail
0x1000 0x4000 TX COMMON See the DAC Common table for more detail
0x1000 0x4000 TX CHANNELS See the DAC Channel table for more detail
0x2000 0x8000 TDD CONTROL See the Transceiver TDD Control table for more detail

Base (common to all cores)

Click to expand regmap

ADC Common (axi_ad*)

Click to expand regmap

ADC Channel (axi_ad*)

Click to expand regmap

DAC Common (axi_ad)

Click to expand regmap

DAC Channel (axi_ad*)

Click to expand regmap

Transceiver TDD Control (axi_ad*)

Click to expand regmap

Software Guidelines

The software for this IP can be found as part of the FMCOMMS2/3/4/5 Reference Design at: No-Os Software.
Linux is supported also using ADI Linux repository

References

resources/fpga/docs/axi_ad9361.1634110694.txt.gz · Last modified: 13 Oct 2021 09:38 by Iulia Moldovan