This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:fpga:docs:axi_ad7616 [11 Oct 2021 15:09] – Add footer Iulia Moldovan | resources:fpga:docs:axi_ad7616 [13 Oct 2021 09:14] – Edit footer & add reference to generic ADC Iulia Moldovan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== AXI_AD7616 IP core ===== | + | ====== AXI_AD7616 IP core ====== |
- | The [[https:// | + | The [[https:// |
+ | \\ | ||
+ | More about the generic framework interfacing ADCs can be read here: [[: | ||
+ | |||
+ | |||
+ | ===== AXI_AD7616 with Serial Interface ===== | ||
- | ==== AXI_AD7616 with Serial Interface ==== | ||
{{: | {{: | ||
- | ==== AXI_AD7616 with Parallel Interface ==== | + | |
+ | ===== AXI_AD7616 with Parallel Interface ===== | ||
{{: | {{: | ||
- | ==== Configuration Parameter ==== | + | |
+ | ===== Configuration Parameter | ||
^ Name ^ Description ^ Default Value^ | ^ Name ^ Description ^ Default Value^ | ||
Line 16: | Line 23: | ||
- | ==== Signal and Interface Pins ==== | + | ===== Signal and Interface Pins ===== |
^ Interface ^ Pin ^ Type ^ Description ^ | ^ Interface ^ Pin ^ Type ^ Description ^ | ||
Line 41: | Line 48: | ||
| '' | | '' | ||
- | ==== Memory Map Registers ==== | + | |
+ | ===== Memory Map Registers | ||
If the SPI engine is active from offset **0x0000** can be found the [[/ | If the SPI engine is active from offset **0x0000** can be found the [[/ | ||
Line 71: | Line 79: | ||
- | {{navigation #axi_ip|AXI IP#hdl|Main page# | + | {{navigation |