Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
Last revision Both sides next revision
resources:fpga:docs:axi_ad7616 [14 Sep 2022 09:40]
Alin-Tudor Sferle axi_ad7616: Update adc_sync port type name
resources:fpga:docs:axi_ad7616 [13 Dec 2022 11:45]
sergiu arpadi
Line 1: Line 1:
 ====== AXI_AD7616 IP core ====== ====== AXI_AD7616 IP core ======
  
-The [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​library/​axi_ad7616|axi_ad7616]] IP core can be used to interface the [[adi>​AD7616]] device using an FPGA. The core has a AXI Memory Map interface for configuration,​ supports ​both the serial and parallel data interface of the device, and has a simple FIFO interface for the DMAC. \\+The [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​library/​axi_ad7616|axi_ad7616]] IP core can be used to interface the [[adi>​AD7616]] device using an FPGA. The core has a AXI Memory Map interface for configuration,​ supports the parallel data interface of the device, and has a simple FIFO interface for the DMAC. \\
 \\ \\
 More about the generic framework interfacing ADCs can be read here: [[:​resources:​fpga:​docs:​axi_adc_ip]]. More about the generic framework interfacing ADCs can be read here: [[:​resources:​fpga:​docs:​axi_adc_ip]].
- 
- 
-===== AXI_AD7616 with Serial Interface ===== 
- 
-{{:​resources:​fpga:​docs:​axi_ad7616_ser_v2.svg|AXI_AD7616 with Serial Interface}} 
  
  
 ===== AXI_AD7616 with Parallel Interface ===== ===== AXI_AD7616 with Parallel Interface =====
  
-{{:​resources:​fpga:​docs:​axi_ad7616_par_v2.svg|AXI_AD7616 with Parallel Interface}}+{{:​resources:​fpga:​docs:​axi_ad7616_ip.svg|AXI_AD7616 with Parallel Interface}}
  
  
Line 20: Line 15:
 ^ Name ^ Description ^ Default Value^ ^ Name ^ Description ^ Default Value^
 | ''​ID''​ | Core ID, it can be used in case of multiple cores on a system | 0 | | ''​ID''​ | Core ID, it can be used in case of multiple cores on a system | 0 |
-| ''​IF_TYPE''​ | If **0** the **SERIAL** interface is active, otherwise the **PARALLEL** ​ | 0 | 
  
  
Line 26: Line 20:
  
 ^ Interface ^ Pin ^ Type ^ Description ^ ^ Interface ^ Pin ^ Type ^ Description ^
-| ''​rx_serial''​ | **A 3-wire serial interface with two SDI line** ​ |||  
-|         | ''​rx_sclk'' ​ |''​output''​ | Clock | 
-|         | ''​rx_cs_n'' ​ |''​output''​ | Chip select | 
-|         | ''​rx_sdo'' ​  ​|''​output''​ | Serial data out | 
-|         | ''​rx_sdi_0''​ |''​input''​ | First serial data in | 
-|         | ''​rx_sdi_1''​ |''​input''​ | Second serial data in | 
 | ''​rx_parallel''​ | **Parallel interface** ​ ||| | ''​rx_parallel''​ | **Parallel interface** ​ |||
 |         | ''​rx_db_o'' ​ |''​output[15:​0]''​ | Parallel data out | |         | ''​rx_db_o'' ​ |''​output[15:​0]''​ | Parallel data out |
Line 38: Line 26:
 |         | ''​rx_rd_n'' ​       |''​output''​ | Active low parallel data read control | |         | ''​rx_rd_n'' ​       |''​output''​ | Active low parallel data read control |
 |         | ''​rx_wr_n'' ​       |''​output''​ | Active low parallel data write control | |         | ''​rx_wr_n'' ​       |''​output''​ | Active low parallel data write control |
 +|         | ''​rx_cs_n'' ​       |''​output''​ | Active low chip select |
 | ''​rx_control''​ | **Control interface** | | ''​rx_control''​ | **Control interface** |
-|         | ''​rx_cnvst'' ​|''​output''​ | Conversion start signal | +|         | ''​rx_trigger ​''​ |''​input''​ | End of conversion ​signal |
-|         | ''​rx_busy''  ​|''​input''​ | Conversion ready signal |+
 | ''​s_axi_*''​ | **AXI Slave Memory Map interface** ||| | ''​s_axi_*''​ | **AXI Slave Memory Map interface** |||
 | ''​adc_fifo''​ | **Write FIFO interface for the DMAC** ||| | ''​adc_fifo''​ | **Write FIFO interface for the DMAC** |||
Line 46: Line 34:
 |              | ''​adc_data''​ | ''​output[15:​0]''​ | Data bus |  |              | ''​adc_data''​ | ''​output[15:​0]''​ | Data bus | 
 |              | ''​adc_sync''​ | ''​output''​ | Shows the first valid beat on a sequence |  |              | ''​adc_sync''​ | ''​output''​ | Shows the first valid beat on a sequence | 
-| ''​irq''​ | IRQ signal ​from the SPI engine ​|||+| ''​irq''​ | IRQ signal |||
  
  
 ===== Memory Map Registers ===== ===== Memory Map Registers =====
- 
-If the SPI engine is active from offset **0x0000** can be found the [[/​resources/​fpga/​peripherals/​spi_engine/​axi#​register_map|SPI engine memory space]]. 
- 
-The following register space is active in both PARALLEL and SERIAL mode. 
  
 |< 100% 5% 5% 5% 25% 5% 55% >| |< 100% 5% 5% 5% 25% 5% 55% >|
Line 64: Line 48:
 ^0x0102 ^0x0408 ^REG_SCRATCH ^^^Version and Scratch Registers ^ ^0x0102 ^0x0408 ^REG_SCRATCH ^^^Version and Scratch Registers ^
 | | |[31:0] |SCRATCH[31:​0] |RW |Scratch register. | | | |[31:0] |SCRATCH[31:​0] |RW |Scratch register. |
-^0x0103 ^0x040C ^REG_IF_TYPE ^^^ADC Interface Control & Status ^ 
-| | |[31:0] |IF_TYPE |RO | Actual interface type, if **0** SERIAL interface is active, PARALLEL otherwise | 
 ^0x0110 ^0x0440 ^REG_UP_CNTRL ^^^ADC Interface Control & Status ^ ^0x0110 ^0x0440 ^REG_UP_CNTRL ^^^ADC Interface Control & Status ^
 | | |[0] |RESETN |RW | Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. | | | |[0] |RESETN |RW | Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. |
resources/fpga/docs/axi_ad7616.txt · Last modified: 25 Apr 2023 09:34 by Iulia Moldovan