Wiki

This version (11 Oct 2021 15:56) was approved by Adrian Costina.The Previously approved version (02 Mar 2017 22:20) is available.Diff

This is an old revision of the document!


Avalon Transceiver Core (avl_adxcvr)

The Avalon ADI Transceiver (avl_adxcvr) core is implements a JESD link between an Altera (Intel) device and the converter device. It instantiates the Altera transceivers and the JESD core. This core is a 'direct-hdl-inference' core. That is, it does NOT have any HDL files. The core infers the Altera IP cores and generates a top level wrapper file on the fly. This method is necessary for some of the Altera IP cores that do not support direct HDL inference (some actually do, but you may end up with a lot of mess). The core also support 'transceiver sharing' by which you may instantiate multiple links (separate pairs) but merge them together (joined pairs). The core also allows transceiver sharing across asymmetrical and multiple links across the receive and transmit pairs.

Features

  • Supports Altera (Arria 10 and above) devices
  • Supports transceiver sharing and dynamic reconfiguration
  • Supports up to 16 transceiver lanes per link

Components

The core instantiates one or more of the following components.

  • clock_source
  • altera_clock_bridge
  • altera_iopll
  • altera_pll
  • altera_pll_reconfig
  • altera_xcvr_reset_control
  • altera_xcvr_atx_pll_a10
  • altera_jesd204
  • alt_xcvr_reconfig
  • avl_adxphy (ADI IP core)

Transceiver Sharing

An Altera transceiver PHY is a transmit and receive pair. If you infer a PHY in a transmit only core for a DAC device link, you are also consuming a receive channel even if NOT used. The same applies to a receive only core for an ADC device link. This IP core is meant to provide the 'sharing' of these transmit and receive channels across multiple instantiations. As an example you may infer a transmit only core of 4 lanes (T1), a receive only core of 2 lanes (R1) and another receive only core of 2 lanes (R2). It is possible to merge these three instantiations to use only 4 PHY channels. However, the software may access them as if they are independent and separate. The core also supports a lane multiplexing so that the transmit and receive cores may occupy any channels within their range.

Parameters

Name Description Default Value
DEVICE_FAMILY System specific, inferred from project settings. Arria 10
TX_OR_RX_N Indicates transmit (0x1) or receive (0x0) link type 0
ID An unique identifier for the core. 0
PCS_CONFIG Altera specific, PCS soft or hard core options (see note 1). JESD_PCS_CFG2
LANE_RATE Altera specific, lane rate in Mbps (see note 1). 10000
SYSCLK_FREQUENCY Altera specific, cpu clock frequency in MHz (see note 1). 100
PLLCLK_FREQUENCY Altera specific, transceiver pll clock frequency in MHz, usually 'LANE_RATE/2' (see note 1). 5000
REFCLK_FREQUENCY Altera specific, transceiver reference clock frequency in MHz (see note 1). 500
CORECLK_FREQUENCY Altera specific, transceiver data path clock frequency in MHz, usually 'LANE_RATE/40' (see note 1). 250
NUM_OF_LANES Altera specific, number of lanes in the link (see note 1). 4
NUM_OF_CONVS Altera specific, number of converters in the link (see note 1). 2
FRM_BCNT Altera specific, number of bytes in a frame (see note 1). 1
FRM_SCNT Altera specific, number of samples in a frame (see note 1). 1
MF_FCNT Altera specific, number of frames in a multi-frame (see note 1). 32
HD Altera specific, high density (0x1) mode, samples are distributed across lanes in a link (see note 1). 1

Notes:

  1. These parameters are passed to the Altera cores 'altera_jesd204' and 'altera_xcvr_atx_pll_a10'. Please refer to the documentation of these cores for a description of these parameters.

Interface

Interface/Pin Type Description
sys_resetn Input System reset (active low), must be the same as the processor reset.
sys_clk Input System clock, must be the same as the processor clock.
ref_clk Input Transceiver reference clock, primary IO must come from an external source.
core_clk Output Transceiver core clock, data path is synchronous to this clock.
rst Input Transceiver reset (active high), usually sourced by axi_adxcvr core.
ready Output Transceiver ready (active high), indicates an active link.
core_pll_locked Output Transceiver core pll locked (active high), indicates pll lock status.
lane_pll_reconfig Input-Interface Transceiver lane PLL reconfiguration avalon interface (transmit only).
core_pll_reconfig Input-Interface Transceiver core PLL reconfiguration avalon interface.
phy_reconfig_${n} Input-Interface Transceiver PHY reconfiguration avalon interface (for each of the 'NUM_OF_LANES' in a link).
ip_reconfig Input-Interface Transceiver IP programming avalon interface.
tx_data_${n} Output Transceiver transmit lane primary IO (transmit only).
rx_data_${n} Input Transceiver receive lane primary IO (receive only).
sysref Input Transceiver SYSREF signal (subclass-1 only).
sync Mixed Transceiver SYNC (input for transmit cores and output for receive cores).
ip_sof Output Transceiver Start-Of-Frame (receive only).
ip_data Mixed Transceiver data (input for transmit cores and output for receive cores).
tx_ip_s_${n} Input Transceiver transmit PHY swap port (if not really concerned, simply match up).
tx_ip_d_${n} Output Transceiver transmit PHY swap port (if not really concerned, simply match up).
tx_phy_s_${n} Input Transceiver transmit PHY swap port (if not really concerned, simply match up).
tx_phy_d_${n} Output Transceiver transmit PHY swap port (if not really concerned, simply match up).

Notes:

  1. The ports 'sys_clk', 'ref_clk' and 'core_clk' corresponds to the 'SYSCLK_FREQUENCY', 'REFCLK_FREQUENCY' and 'CORECLK_FREQUENCY' parameters respectively.
  2. All reconfiguration interfaces are 'AVALON' slave interfaces and must be connected to the CPU.
  3. The 'tx_ip_' and 'tx_phy_' ports allow lane swapping within a link. If no swapping is desired, simply match them up with their indices. That is, tx_ip_s_0 == tx_phy_s_0 and tx_ip_d_0 == tx_phy_d_0. If swapping is desired the '_s_' and '_p_' pairs serve as a cross-bar switch for the IP and the PHY.

Register Map

This core is a wrapper function for the above mentioned Altera IP cores. The register map of this core is one or more of its sub-cores.

Software Guidelines

The core supports 'transceiver sharing' as described above, hence the same PHY is accessable from two different address regions. In other words, a transmit core can potentially access a receive core and corrupt the settings. There is no 'protection' of functionalities within the core.

More Information

/srv/wiki.analog.com/data/pages/resources/fpga/docs/avl_adxcvr.txt · Last modified: 13 Oct 2021 08:55 by Iulia Moldovan