This is an old revision of the document!
Board name | FMC connector 1 | FMC connector 2 |
---|---|---|
A10GX | LPC () | HPC (8 x 17.4 Gbps) |
A10SOC | HPC (16 GTX ???) | LPC (16 GTX ???) |
Stratix10SoC | FMC+ (24 @ 28.3 Gbps) | FMC+ (24 @ 28.3 Gbps) |
Board name | FMC 1 | FMC 2 |
---|---|---|
A10GX | *1.8V/1.5V/1.35V/1.2V | *1.8V/1.5V/1.35V/1.2V |
A10SOC | *1.8V/1.5V/1.35V/1.25V/1.2V/1.1V | *1.8V/1.5V/1.35V/1.2V/1.1V |
Stratix10SoC | *3.3V/1.8V/1.2V | *3.3V/1.8V/1.2V |
(* bold) = default VADJ
FMC1 & FMC2 columns → depending on the power supply of the device connected to the FMC, the custom VADJ will have the value supported by both the carrier and the device(s)