This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:fpga:altera:software_setup [02 Oct 2019 13:45] – Antoniu Miclaus | resources:fpga:altera:software_setup [02 Oct 2019 14:08] (current) – Antoniu Miclaus | ||
---|---|---|---|
Line 36: | Line 36: | ||
* At the **Project** tab define your current project name and application executable. (.elf) | * At the **Project** tab define your current project name and application executable. (.elf) | ||
- | + | ||
- | * The output of the example program can be viewed in the SDK console. | + | * On the Target Connection tab, press the **Refresh Connections** button. You may need to expand the window or scroll to the right to see this button. |
+ | |||
+ | * Check the **Ignore mismatched system ID** option. | ||
+ | |||
+ | * Check the **Ignore mismatched system timestamp** option. | ||
+ | |||
+ | * The output of the example program can be viewed in the Console Window. | ||
* When the run configuration is done, the software can be started by clicking the **Run** button. | * When the run configuration is done, the software can be started by clicking the **Run** button. | ||
* Your new bare metal application should run | * Your new bare metal application should run |