Differences
This shows you the differences between two versions of the page.
| |
resources:fpga:altera:ced1z:common_software_design [20 Aug 2012 16:26] – created Adrian Costina | resources:fpga:altera:ced1z:common_software_design [03 Jan 2013 20:42] (current) – external edit 127.0.0.1 |
---|
Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera -> Nios II EDS 11.0 -> Nios II 11.0 | Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera -> Nios II EDS 11.0 -> Nios II 11.0 |
Software Build Tools for Eclipse (SBT)//**. | Software Build Tools for Eclipse (SBT)//**. |
<note tip>NOTE: Windows 7 users will need to right-click and select **//Run as administrator//**. Another method is to right-click and select **//Properties//** and click on the //**Compatibility**// tab and select the **//Run This Program As An Administrator//** checkbox, which will make this a permanent change.</note> | <WRAP tip>NOTE: Windows 7 users will need to right-click and select **//Run as administrator//**. Another method is to right-click and select **//Properties//** and click on the //**Compatibility**// tab and select the **//Run This Program As An Administrator//** checkbox, which will make this a permanent change.</WRAP> |
| |
=== 1. Initialize Eclipse workspace === | === 1. Initialize Eclipse workspace === |
{{:resources:fpga:altera:bemicro:eclipsebuildproj.png?400}} | {{:resources:fpga:altera:bemicro:eclipsebuildproj.png?400}} |
| |
<note important>In case an error appears at compile time with a description like : **//section .rodata loaded at [00400164,00400477] overlaps section .text loaded at [00400164,004054d7] //** the enable_alt_load_copy_exceptions option must be unchecked from BSP Editor -> Main -> Settings -> Advanced-> hal.linker </note> | <WRAP important>In case an error appears at compile time with a description like : **//section .rodata loaded at [00400164,00400477] overlaps section .text loaded at [00400164,004054d7] //** the enable_alt_load_copy_exceptions option must be unchecked from BSP Editor -> Main -> Settings -> Advanced-> hal.linker </WRAP> |
| |
=== 2. Verify the Board Connection === | === 2. Verify the Board Connection === |
| |
| |
<note>The code size and start address might be different than the ones displayed in the above screenshot.</note> | <WRAP round help>The code size and start address might be different than the ones displayed in the above screenshot.</WRAP> |