Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:fpga:altera:ced1z:ad7938 [21 Aug 2012 12:47]
Adrian Costina Added version to uC-Probe software
resources:fpga:altera:ced1z:ad7938 [26 Jan 2021 01:23]
Robin Getz update arrow links after their web site update
Line 3: Line 3:
 ====== Overview ===== ====== Overview =====
  
-This document presents the steps to setup an environment for using the **[[adi>​AD7938|EVAL-AD7938CBZ]]** evaluation board together with the **[[adi>​EVAL-CED|EVAL-CED Converter Evaluation and Development (CED) Board]]**, the Nios II Embedded Development Suite (EDS) and the [[http://​micrium.com/​page/​products/tools/probe|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD7938 Evaluation Board with the CED1 board.+This document presents the steps to setup an environment for using the **[[adi>​AD7938|EVAL-AD7938CBZ]]** evaluation board together with the **[[adi>​EVAL-CED|EVAL-CED Converter Evaluation and Development (CED) Board]]**, the Nios II Embedded Development Suite (EDS) and the [[https://www.micrium.com/​ucprobe/about/|Micrium µC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD7938 Evaluation Board with the CED1 board.
  
 {{ :​resources:​fpga:​altera:​ced1z:​img_0024.png?​500 }} {{ :​resources:​fpga:​altera:​ced1z:​img_0024.png?​500 }}
Line 18: Line 18:
   * [[adi>/​static/​imported-files/​eval_boards/​17099365EVAL_AD7938CB_AD7939CB_AD7938_6CB.pdf|EVAL-AD7938CBZ evaluation board user guide]]   * [[adi>/​static/​imported-files/​eval_boards/​17099365EVAL_AD7938CB_AD7939CB_AD7938_6CB.pdf|EVAL-AD7938CBZ evaluation board user guide]]
   * [[http://​www.altera.com/​devices/​processor/​nios2|Nios II Embedded Development Suite (EDS)]]   * [[http://​www.altera.com/​devices/​processor/​nios2|Nios II Embedded Development Suite (EDS)]]
-  * [[http://​micrium.com/​page/​products/tools/probe|Micrium uC-Probe v2.5]]+  * [[https://www.micrium.com/​ucprobe/about/|Micrium uC-Probe v2.5]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 37: Line 37:
   * [[http://​www.altera.com/​products/​software/​quartus-ii/​web-edition/​qts-we-index.html|Quartus II Web Edition]] design software v11.0   * [[http://​www.altera.com/​products/​software/​quartus-ii/​web-edition/​qts-we-index.html|Quartus II Web Edition]] design software v11.0
   * [[https://​www.altera.com/​download/​software/​nios-ii|Nios II EDS]] v11.0   * [[https://​www.altera.com/​download/​software/​nios-ii|Nios II EDS]] v11.0
-  * [[http://​micrium.com/​page/​products/tools/probe|uC-Probe v2.5]] run-time monitoring tool+  * [[https://www.micrium.com/​ucprobe/about/|uC-Probe v2.5]] run-time monitoring tool
    
 The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web.  The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. 
Line 168: Line 168:
 Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera -> Nios II EDS 11.0 -> Nios II 11.0 Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera -> Nios II EDS 11.0 -> Nios II 11.0
 Software Build Tools for Eclipse (SBT)//**. Software Build Tools for Eclipse (SBT)//**.
-<note tip>​NOTE:​ Windows 7 users will need to right-click and select **//Run as administrator//​**. Another method is to right-click and select **//​Properties//​** and click on the //​**Compatibility**//​ tab and select the **//Run This Program As An Administrator//​** checkbox, which will make this a permanent change.</​note>+<WRAP tip>​NOTE:​ Windows 7 users will need to right-click and select **//Run as administrator//​**. Another method is to right-click and select **//​Properties//​** and click on the //​**Compatibility**//​ tab and select the **//Run This Program As An Administrator//​** checkbox, which will make this a permanent change.</​WRAP>
  
 === 1. Initialize Eclipse workspace === === 1. Initialize Eclipse workspace ===
Line 302: Line 302:
 {{ :​resources:​fpga:​altera:​cedz:​image063.png?​500 }} {{ :​resources:​fpga:​altera:​cedz:​image063.png?​500 }}
  
-<note>The code size and start address might be different than the ones displayed in the above screenshot.</​note>+<WRAP round help>The code size and start address might be different than the ones displayed in the above screenshot.</​WRAP>
  
  
resources/fpga/altera/ced1z/ad7938.txt · Last modified: 26 Jan 2021 01:23 by Robin Getz