Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:altera:bemicro:common_usb [09 Nov 2011 13:48] – Approved Andrei Cozma | resources:fpga:altera:bemicro:common_usb [21 Jun 2013 13:15] (current) – Change the 11.0 to //<version number>// Istvan Csomortani |
---|
{{ :resources:fpga:altera:bemicro:image009.png?500 }} | {{ :resources:fpga:altera:bemicro:image009.png?500 }} |
| |
In the next dialog box select the option **//Browse my computer for driver software//**. A new dialog will open where it is possible to point to the driver’s location. Set the location to **altera\11.0\quartus\drivers\usb-blaster** and press **//Next//**. | In the next dialog box select the option **//Browse my computer for driver software//**. A new dialog will open where it is possible to point to the driver’s location. Set the location to **altera\//<version number>//\quartus\drivers\usb-blaster** and press **//Next//**. |
| |
{{:resources:fpga:altera:bemicro:image011.png?400}}{{:resources:fpga:altera:bemicro:image013.png?400}} | {{:resources:fpga:altera:bemicro:image011.png?400}}{{:resources:fpga:altera:bemicro:image013.png?400}} |
<WRAP clear></WRAP> | <WRAP clear></WRAP> |
<note tip>If Windows presents you with a message that the drivers have not passed Windows Logo testing, please click “**//Install this driver software anyway//**”. Upon installation completion a message will be displayed to inform that the installation is finished.</note> | <WRAP tip>If Windows presents you with a message that the drivers have not passed Windows Logo testing, please click “**//Install this driver software anyway//**”. Upon installation completion a message will be displayed to inform that the installation is finished.</WRAP> |
| |
{{:resources:fpga:altera:bemicro:image017.png?400}}{{:resources:fpga:altera:bemicro:image016.jpg?400}} | {{:resources:fpga:altera:bemicro:image017.png?400}}{{:resources:fpga:altera:bemicro:image016.jpg?400}} |
| |