Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

resources:fpga:altera:bemicro:common_software_design [04 Sep 2012 09:08] – created common page for Quartus 12sp2 projects Adrian Costinaresources:fpga:altera:bemicro:common_software_design [03 Jan 2013 20:42] (current) – external edit 127.0.0.1
Line 6: Line 6:
 Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera 12.0sp2-> Nios II EDS 12.0sp2 -> Nios II 12.0sp2 Launch the **Nios II SBT** from the **//Start -> All Programs -> Altera 12.0sp2-> Nios II EDS 12.0sp2 -> Nios II 12.0sp2
 Software Build Tools for Eclipse (SBT)//**. Software Build Tools for Eclipse (SBT)//**.
-<note tip>NOTE: Windows 7 users will need to right-click and select **//Run as administrator//**. Another method is to right-click and select **//Properties//** and click on the //**Compatibility**// tab and select the **//Run This Program As An Administrator//** checkbox, which will make this a permanent change.</note>+<WRAP tip>NOTE: Windows 7 users will need to right-click and select **//Run as administrator//**. Another method is to right-click and select **//Properties//** and click on the //**Compatibility**// tab and select the **//Run This Program As An Administrator//** checkbox, which will make this a permanent change.</WRAP>
  
 === 1. Initialize Eclipse workspace === === 1. Initialize Eclipse workspace ===
Line 135: Line 135:
 {{ :resources:fpga:altera:bemicro:image063.png?400 }} {{ :resources:fpga:altera:bemicro:image063.png?400 }}
  
-<note>The code size and start address might be different than the ones displayed in the above screenshot.</note>+<WRAP round help>The code size and start address might be different than the ones displayed in the above screenshot.</WRAP>
  
resources/fpga/altera/bemicro/common_software_design.txt · Last modified: 03 Jan 2013 20:42 by 127.0.0.1