This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:fpga:altera:bemicro:cn0203 [11 Jan 2021 09:05] Ioana Chelaru Fixed bad links for AD5660-1 |
resources:fpga:altera:bemicro:cn0203 [25 Jan 2021 14:12] Ioana Chelaru Fixed bad links |
||
---|---|---|---|
Line 10: | Line 10: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This lab presents the steps to setup an environment for using the **[[adi>EVAL-CN0203-SDPZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-CN0203-SDPZ Evaluation Board with the BeMicro SDK Platform. | + | This lab presents the steps to setup an environment for using the **[[adi>EVAL-CN0203-SDPZ]]** evaluation board together with the **[https://www.arrow.com/en/datasheets/89166696/arrow-development-tools/bemicrosdk|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-CN0203-SDPZ Evaluation Board with the BeMicro SDK Platform. |
{{ :resources:fpga:altera:bemicro:cn0203_bemicro.jpg?400 }} | {{ :resources:fpga:altera:bemicro:cn0203_bemicro.jpg?400 }} | ||
Line 47: | Line 47: | ||
* [[adi>AD5750-1|AD5750-1 Product Info]] - pricing, samples, datasheet | * [[adi>AD5750-1|AD5750-1 Product Info]] - pricing, samples, datasheet | ||
* [[adi>CN0203|EVAL-CN0203-SDPZ evaluation board user guide]] | * [[adi>CN0203|EVAL-CN0203-SDPZ evaluation board user guide]] | ||
- | * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]] | + | * [[https://www.arrow.com/en/datasheets/89166696/arrow-development-tools/bemicrosdk|BeMicro SDK]] |
* [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]] | * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]] | ||
* [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]] | * [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]] | ||
Line 59: | Line 59: | ||
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: | ||
- | * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | + | * Arrow Electronics [[https://www.arrow.com/en/datasheets/89166696/arrow-development-tools/bemicrosdk|BeMicro SDK]] FPGA-based MCU Evaluation Board |
- | * [[http://www.arrownac.com/solutions/adi_interposer/|BeMicro SDK/SDP Interposer]] adapter board | + | * [[https://www.arrow.com/en/datasheets/2957953708/analog-devices/bemicrosdksdpinterposer|BeMicro SDK/SDP Interposer]] adapter board |
* **EVAL-CN0203-SDPZ** evaluation board | * **EVAL-CN0203-SDPZ** evaluation board | ||
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory |