Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:altera:bemicro:ad7982 [28 Sep 2012 09:21] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costina | resources:fpga:altera:bemicro:ad7982 [26 Jan 2021 01:22] (current) – update arrow links after their web site update Robin Getz |
---|
====== Overview ====== | ====== Overview ====== |
| |
This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD7982SDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick and the Nios II Embedded Development Suite (EDS). Below is presented a picture of the EVAL-AD7982SDZ Evaluation Board with the BeMicro SDK Platform. | This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD7982SDZ]]** evaluation board together with the **[[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]** USB stick and the Nios II Embedded Development Suite (EDS). Below is presented a picture of the EVAL-AD7982SDZ Evaluation Board with the BeMicro SDK Platform. |
| |
{{ :resources:fpga:altera:bemicro:ad7982_bemicro.jpg?400 }} | {{ :resources:fpga:altera:bemicro:ad7982_bemicro.jpg?400 }} |
* [[adi>AD7982|AD7982 Product Info]] - pricing, samples, datasheet | * [[adi>AD7982|AD7982 Product Info]] - pricing, samples, datasheet |
* {{:resources:fpga:altera:bemicro:user_guide_eval_10lead_pulsar.pdf|EVAL-AD7982SDZ evaluation board user guide}} | * {{:resources:fpga:altera:bemicro:user_guide_eval_10lead_pulsar.pdf|EVAL-AD7982SDZ evaluation board user guide}} |
* [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]] | * [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] |
* [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]] | * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]] |
| |
| |
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: |
* Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | * Arrow Electronics [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] FPGA-based MCU Evaluation Board |
* [[http://www.arrownac.com/solutions/adi_interposer/|BeMicro SDK/SDP Interposer]] adapter board | * [[adi>sdp-bemicro|BeMicro SDK/SDP Interposer]] adapter board |
* **EVAL-AD7982SDZ** evaluation board | * **EVAL-AD7982SDZ** evaluation board |
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory |
| ADC_CLK_I | IN | 1 | Clock to be sent to the ADC during the conversion process. | | | ADC_CLK_I | IN | 1 | Clock to be sent to the ADC during the conversion process. | |
| //**IP control and data ports**// |||| | | //**IP control and data ports**// |||| |
| DATA_O | OUT | 16 | Outputs the data read from the ADC. The channel ID is stored on the 4 most significant bits and the read data is stored on the 12 least significant bits. If the ADC is driven in word read mode then the channel ID will always be 0. | | | DATA_O | OUT | 18 | Outputs the data read from the ADC. | |
| DATA_RD_READY_O | OUT | 1 | Active high signal to indicate the status of a read operation from the AD7982. The IP continuously reads the conversion results from the ADC and outputs them on the DATA_O bus. When this signal is high data can be read from the DATA_O bus. | | | DATA_RD_READY_O | OUT | 1 | Active high signal to indicate the status of a read operation from the AD7982. The IP continuously reads the conversion results from the ADC and outputs them on the DATA_O bus. When this signal is high data can be read from the DATA_O bus. | |
| //**AD7982 control and data ports**// |||| | | //**AD7982 control and data ports**// |||| |
| ADC_SDI | IN | 1 | ADC Serial Data Input. This pin is currently not used in the design. | | | ADC_SDI | IN | 1 | ADC Serial Data Input. This pin is currently not used in the design. | |
| ADC_SCLK_O | OUT | 1 | ADC Serial Data Clock Input. When the part is selected, the conversion result is shifted out by this clock. | | | ADC_SCLK_O | OUT | 1 | ADC Serial Data Clock Input. When the part is selected, the conversion result is shifted out by this clock. | |
| ADC_CNV_O | OUT | 1 | ADC Convert Input. This input has multiple functions. On its leading edge, it initiates the conversions and selects the interface mode of the part, chain, or CS mode. In CS mode, it enables the SDO pin when low. In chain mode, the data should be read when CNV is high. | | | ADC_CNVST_O | OUT | 1 | ADC Convert Input. This input has multiple functions. On its leading edge, it initiates the conversions and selects the interface mode of the part, chain, or CS mode. In CS mode, it enables the SDO pin when low. In chain mode, the data should be read when CNV is high. | |
| **Table 2 AD7982 driver ports description** |||| | | **Table 2 AD7982 driver ports description** |||| |
| |