This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:fpga:altera:bemicro:ad7683 [08 Jan 2013 13:57] – created Adrian Costina | resources:fpga:altera:bemicro:ad7683 [08 Jan 2013 14:45] – Added sampling frequency note in the Demonstration Project User Interface section Adrian Costina | ||
---|---|---|---|
Line 164: | Line 164: | ||
====== Demonstration Project User Interface ====== | ====== Demonstration Project User Interface ====== | ||
- | * Execute **// | + | * Execute **// |
* The data captured from the ADC is saved into a comma separated values (.csv) file named **// | * The data captured from the ADC is saved into a comma separated values (.csv) file named **// | ||
* The data capture status is also displayed in the opened command window as shown in the figure below. | * The data capture status is also displayed in the opened command window as shown in the figure below. |