Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Last revisionBoth sides next revision
resources:fpga:altera:bemicro:ad7683 [08 Jan 2013 13:57] – created Adrian Costinaresources:fpga:altera:bemicro:ad7683 [08 Jan 2013 14:45] – Added sampling frequency note in the Demonstration Project User Interface section Adrian Costina
Line 164: Line 164:
 ====== Demonstration Project User Interface ====== ====== Demonstration Project User Interface ======
  
-* Execute **//data_capture.bat//** script. At this point 8192 samples will be acquired from the ADC and saved into the BeMicro SDK memory. The data stored in the BeMicro SDK memory is transfered to the PC. After the data is transferred to the PC it is converted to 16 bit values.+* Execute **//data_capture.bat//** script. At this point 8192 samples will be acquired at 99 KSPS from the ADC and saved into the BeMicro SDK memory. The data stored in the BeMicro SDK memory is transfered to the PC. After the data is transferred to the PC it is converted to 16 bit values. 
   * The data captured from the ADC is saved into a comma separated values (.csv) file named **//Acquisition.csv//**, located in the same folder as the //**data_capture.bat**// file.   * The data captured from the ADC is saved into a comma separated values (.csv) file named **//Acquisition.csv//**, located in the same folder as the //**data_capture.bat**// file.
   * The data capture status is also displayed in the opened command window as shown in the figure below.   * The data capture status is also displayed in the opened command window as shown in the figure below.
resources/fpga/altera/bemicro/ad7683.txt · Last modified: 26 Jan 2021 01:22 by Robin Getz