Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:fpga:altera:bemicro:ad7492 [28 Sep 2012 09:15] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costinaresources:fpga:altera:bemicro:ad7492 [26 Jan 2021 01:21] (current) – update arrow links after their web site update Robin Getz
Line 11: Line 11:
 ====== Overview ====== ====== Overview ======
  
-This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD7492SDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick and the the Nios II Embedded Development Suite (EDS). Below is presented a picture of the EVAL-AD7492SDZ Evaluation Board with the BeMicro SDK Platform.+This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD7492SDZ]]** evaluation board together with the **[[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]** USB stick and the the Nios II Embedded Development Suite (EDS). Below is presented a picture of the EVAL-AD7492SDZ Evaluation Board with the BeMicro SDK Platform.
  
 {{ :resources:fpga:altera:bemicro:ad7492_bemicro.jpg?400 }} {{ :resources:fpga:altera:bemicro:ad7492_bemicro.jpg?400 }}
Line 29: Line 29:
   * [[adi>AD7492|AD7492 Product Info]] - pricing, samples, datasheet   * [[adi>AD7492|AD7492 Product Info]] - pricing, samples, datasheet
   * EVAL-AD7492SDZ evaluation board user guide is included on the CD as part of the Evaluation Board Kit   * EVAL-AD7492SDZ evaluation board user guide is included on the CD as part of the Evaluation Board Kit
-  * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]+  * [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]
   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]
  
Line 39: Line 39:
  
 Below is presented the list of required hardware items: Below is presented the list of required hardware items:
-  * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board +  * Arrow Electronics [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] FPGA-based MCU Evaluation Board 
-  * [[http://www.arrownac.com/solutions/adi_interposer/|BeMicro SDK/SDP Interposer]] adapter board+  * [[adi>sdp-bemicro|BeMicro SDK/SDP Interposer]] adapter board
   * **EVAL-AD7492SDZ** evaluation board   * **EVAL-AD7492SDZ** evaluation board
   * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory   * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory
resources/fpga/altera/bemicro/ad7492.txt · Last modified: 26 Jan 2021 01:21 by Robin Getz