This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:fpga:altera:bemicro:ad5755 [01 Jul 2013 09:11] – Adding a table with commands to the Quick Evaluation section Istvan Csomortani | resources:fpga:altera:bemicro:ad5755 [26 Jan 2021 01:21] (current) – update arrow links after their web site update Robin Getz | ||
---|---|---|---|
Line 13: | Line 13: | ||
====== Overview ====== | ====== Overview ====== | ||
- | This lab presents the steps to setup an environment for using the **[[adi> | + | This lab presents the steps to setup an environment for using the **[[adi> |
{{ : | {{ : | ||
Line 31: | Line 31: | ||
* [[adi> | * [[adi> | ||
* [[adi>/ | * [[adi>/ | ||
- | * [[http://www.arrownac.com/solutions/ | + | * [[https://www.intel.com/content/ |
* [[http:// | * [[http:// | ||
Line 42: | Line 42: | ||
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: | ||
- | * Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | + | * Arrow Electronics [[https://www.intel.com/content/www/ |
- | * [[http:// | + | * [[adi> |
* **EVAL-AD5755SDZ** evaluation board | * **EVAL-AD5755SDZ** evaluation board | ||
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory |