Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Last revisionBoth sides next revision
resources:fpga:altera:bemicro:ad5541a [28 Sep 2012 09:30] – Added common section for describing the evaluation setup and System Demonstration Platform Adrian Costinaresources:fpga:altera:bemicro:ad5541a [15 Feb 2013 14:58] – Updated uC/Probe related links Adrian Costina
Line 11: Line 11:
 ====== Overview ====== ====== Overview ======
  
-This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD5541ASDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/page/products/tools/probe|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5541ASDZ Evaluation Board with the BeMicro SDK Platform.+This lab presents the steps to setup an environment for using the **[[adi>EVAL-AD5541ASDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5541ASDZ Evaluation Board with the BeMicro SDK Platform.
  
 {{ :resources:fpga:altera:bemicro:ad5541a_bemicro.png?400 }} {{ :resources:fpga:altera:bemicro:ad5541a_bemicro.png?400 }}
Line 30: Line 30:
   * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]   * [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]]
   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]   * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]]
-  * [[http://micrium.com/page/products/tools/probe|Micrium uC-Probe]]+  * [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]]
  
 ====== Getting Started ====== ====== Getting Started ======
Line 51: Line 51:
   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0   * [[http://www.altera.com/products/software/quartus-ii/web-edition/qts-we-index.html|Quartus II Web Edition]] design software v11.0
   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0   * [[https://www.altera.com/download/software/nios-ii|Nios II EDS]] v11.0
-  * [[http://micrium.com/page/products/tools/probe|uC-Probe]] run-time monitoring tool+  * [[http://micrium.com/tools/ucprobe/trial/|uC-Probe]] run-time monitoring tool, version 2.5
  
 The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web.  The **Quartus II** design software and the **Nios II EDS** is available via the Altera Complete Design Suite DVD or by downloading from the web. 
  
-The **Micrium uC/Probe Trial** version is available via download from the web at [[http://micrium.com/download/Micrium-uC-Probe-Setup-Trial.exe]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.+The **Micrium uC/Probe Trial** version 2.5 is available via download from the web at [[http://micrium.com/tools/ucprobe/trial/]].  After installation add to the “Path” system variable the entry "//%QUARTUS_ROOTDIR%\bin\//“ on the third position in the list.
  
 ===== Downloads ===== ===== Downloads =====
Line 139: Line 139:
  
 {{page>troubleshooting}} {{page>troubleshooting}}
- 
resources/fpga/altera/bemicro/ad5541a.txt · Last modified: 26 Jan 2021 01:21 by Robin Getz