Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:fpga:altera:bemicro:ad5425 [15 Feb 2013 14:34] – Updated uC/probe related links Adrian Costina | resources:fpga:altera:bemicro:ad5425 [26 Jan 2021 01:21] (current) – update arrow links after their web site update Robin Getz |
---|
===== Evaluation Boards ===== | ===== Evaluation Boards ===== |
| |
* [[adi>EVAL-AD5449SDZ]] | * [[adi>EVAL-AD5449|EVAL-AD5449SDZ]] |
| |
====== Overview ====== | ====== Overview ====== |
| |
This lab presents the steps to setup an environment for using the **[[adi>AD5425|EVAL-AD5425SDZ]]** evaluation board together with the **[[http://www.arrownac.com/solutions/bemicro-sdk/|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5425SDZ Evaluation Board with the BeMicro SDK Platform. | This lab presents the steps to setup an environment for using the **[[adi>AD5425|EVAL-AD5425SDZ]]** evaluation board together with the **[[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]]** USB stick, the Nios II Embedded Development Suite (EDS) and the [[http://micrium.com/tools/ucprobe/overview/|Micrium μC-Probe]] run-time monitoring tool. Below is presented a picture of the EVAL-AD5425SDZ Evaluation Board with the BeMicro SDK Platform. |
| |
{{ :resources:fpga:altera:bemicro:ad5449_bemicro.png?400 }} | {{ :resources:fpga:altera:bemicro:ad5449_bemicro.png?400 }} |
* [[adi>AD5425|AD5425 Product Info]] - pricing, samples, datasheet | * [[adi>AD5425|AD5425 Product Info]] - pricing, samples, datasheet |
* [[adi>/static/imported-files/user_guides/UG-297.pdf|EVAL-AD5449SDZ evaluation board user guide]] | * [[adi>/static/imported-files/user_guides/UG-297.pdf|EVAL-AD5449SDZ evaluation board user guide]] |
* [[http://www.arrownac.com/solutions/bemicro-sdk|BeMicro SDK]] | * [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] |
* [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]] | * [[http://www.altera.com/devices/processor/nios2|Nios II Embedded Development Suite (EDS)]] |
* [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]] | * [[http://micrium.com/tools/ucprobe/overview/|Micrium uC-Probe]] |
| |
Below is presented the list of required hardware items: | Below is presented the list of required hardware items: |
* Arrow Electronics [[http://www.arrow.com/bemicrosdk/|BeMicro SDK]] FPGA-based MCU Evaluation Board | * Arrow Electronics [[https://www.intel.com/content/www/us/en/programmable/b/bemicro-sdk.html|BeMicro SDK]] FPGA-based MCU Evaluation Board |
* [[http://www.arrownac.com/solutions/adi_interposer/|BeMicro SDK/SDP Interposer]] adapter board | * [[adi>sdp-bemicro|BeMicro SDK/SDP Interposer]] adapter board |
* **EVAL-AD5449** evaluation board | * **EVAL-AD5449** evaluation board |
* Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory | * Intel Pentium III or compatible Windows PC, running at 866MHz or faster, with a minimum of 512MB of system memory |