Wiki

This version (03 Jun 2015 13:53) was approved by bdaly.The Previously approved version (15 Apr 2015 12:40) is available.Diff

EV-ADRN-WSN-1Z Evaluation Kit

THis is the page for the EV-ADRN-WSN-1Z kit


ADuCRF101 based WSN demo kit
Out-of-the-box WSN Demo Kit
1 Basestation and 2 Sensor Nodes running ADRadioNET
1 ADuCRF101 Minikit board (Pre-programmed Basestation Node)
1 BunchWSN board (Pre-programmed ADXL362 Sensor Node).
1 BunchWSN board (Pre-programmed Humidity & Temp Sensor Node)
1 UART/USB board for programming interface / GUI
Everything comes pre-loaded with ADRadioNET, so it works out of the box. Compatible with IBM Bluemix
SAP Code: EV-ADRN-WSN-1Z

User Guide:

user_guide-adrn-wsn-1.pdf

Quickstart Tutorial:



Binary Files


Here are the default binary files that have been pre-programmed into the nodes.



Individual Sensor Nodes



Individual nodes can be ordered to expand the number of sensors or gateways in a system
Pre-programmed to automatically connect to WSN kits out of the box.
Unique MAC address for each node.

  • Name Description SAP Code
  • Bunch Accelerometer Node ADXL362 Data EV-BUNCH-WSN-1Z
  • Bunch Humidity Node SHT21 Data EV-BUNCH-WSN-2Z

Return to the WSN wiki homepage: http://wiki.analog.com/resources/eval/user-guides/wsn

resources/eval/user-guides/wsn/ev-adrn-wsn-1z.txt · Last modified: 03 Jun 2015 13:53 by bdaly