Wiki

This version (16 Apr 2015 16:53) was approved by bdaly.The Previously approved version (15 Apr 2015 13:45) is available.Diff

Wireless Sensor Network Platform

Welcome to the wiki page for the WSN platform from Analog Devices. This site contains all of the latest information related to the WSN platform

Features

  • Plug and Play Wireless Sensor Network
  • Built on ADuCRF101 platform
  • Built on ADF7024 platform
  • Several Sensor Types supported
  • Runs ADRadioNET wireless communications protocol
  • RoHS compliant
  • USB connection to PC
  • Microsoft Windows-based evaluation software with simple graphical user interface
  • IoT expansion with IBM Bluemix recipe







GENERAL DESCRIPTION


The Wireless Sensor Network (WSN) demo platform is a flexible, modular system for evaluating all aspects of a WSN. It offers both an out-of-the-box demonstration system, and can also be used as a development platform. It contains all of the hardware and software necessary to implement a plug-and-play WSN. It comes with one CenterPoint node and two End Nodes that have been pre-configured to communicate with each other. The End Nodes are compatible with several sensor daughter cards. Once connected, the sensor data will begin streaming to the CenterPoint. The software tools allow configuration and evaluation of the network. The CenterPoint GUI tool offers a host of node and network evaluation tools. These allow the user to see all of the data streaming from the nodes, and lots of other useful data about the node and the network performance. The ANodeConfig tool allows the network to be reconfigured for different data rates, sleep times etc. through an intuitive GUI, so that no code writing is necessary.







HARDWARE



Click here for all information about the hardware platforms, including schematics, layout files etc.

http://wiki.analog.com/resources/eval/user-guides/wsn/hardware






EVALUATION KITS


There are two versions of the evaluation kit available.
http://wiki.analog.com/resources/eval/user-guides/wsn/ev-adrn-wsn-1z
This kit is based on the ADuCRF101, using the BunchWSN boards.

http://wiki.analog.com/resources/eval/user-guides/wsn/ev-adrn-wsn-2z
This kit is based on the ADF7024 and RL78 MCU, using the ClusterWSN boards.






DATASHEETS


ADuCRF101. Precision Analog Microcontroller ARM Cortex M3 with RF Transceiver


ADF7023. High Performance, Low Power, ISM Band FSK/GFSK/OOK/MSK/GMSK Transceiver IC


ADF7024. Easy-To-Use, Low Power, Sub GHz, ISM/SRD, FSK/GFSK, Transceiver IC


ADP5090. Energy Harvesting. Ultra Low Power Boost Regulator With MPPT and Charge Management


ADP160. Ultra Low Quiescent Current 150 mA, CMOS Linear Regulator


ADXL362. Micropower, 3-Axis, ±2 g/±4 g/±8 g Digital Output MEMS Accelerometer






EVALUATION BOARD SOFTWARE


http://sdk.analog.com/dw/sdks.aspx?file=AMEDK

Note: New Software update coming very soon. Please check back soon




PROTOCOL STACKS


THis page contains more information related to the protocol stacks supported by the WSN platform. http://wiki.analog.com/resources/eval/user-guides/wsn/protocols






BATTERY CALCULATOR TOOL


ADI has developed a tool to help users determine their battery lifetimes at a system level. This page contains a link to download the software, and contains more information about the tool.

http://wiki.analog.com/resources/eval/user-guides/wsn/BatteryTool







IoT EXPANSION WITH IBM BLUEMIX


This page contains all of the information to connect the WSN platform to the Cloud using a Raspberry Pi and IBM Bluemix:

http://wiki.analog.com/resources/eval/user-guides/wsn/IoT







ENERGY HARVESTING


This page contains all of the information to power the WSN platform using ADI's energy harvesting platform, based on the ADP5090.

http://wiki.analog.com/resources/eval/user-guides/wsn/EnergyHarvesting





BLUETOOTH CONNECTIVITY


This page contains all of the information related to our “Fenway” BTLE platform





resources/eval/user-guides/wsn.txt · Last modified: 16 Apr 2015 16:53 by bdaly