Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:44]
Andrei Cozma
resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:59]
Andrei Cozma
Line 25: Line 25:
   * Update the HDL design to Vivado 2015.2 by running the //​sdsoc_platform/​update_hdl.tcl//​ script. This step needs to be ran only once after downloading the HDL reference design.   * Update the HDL design to Vivado 2015.2 by running the //​sdsoc_platform/​update_hdl.tcl//​ script. This step needs to be ran only once after downloading the HDL reference design.
   * Regenerate the IP libraries following the steps described here: http://​wiki.analog.com/​resources/​fpga/​docs/​hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified.   * Regenerate the IP libraries following the steps described here: http://​wiki.analog.com/​resources/​fpga/​docs/​hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified.
-  * Generate the SDSoC platform by running the //​sdsoc_platform/​sdsoc_platform.tcl//​ script. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<​board>​_<​carrier>//,​ where //<​board>//​ is the name of the FMCOMMSx board and //<​carrier>//​ is the name of the Xilinx carrier, //eg. fmcomms2_zc702//​+  * Generate the SDSoC platform by running the //​sdsoc_platform/​sdsoc_platform.tcl//​ script. Before running the script you need to edit it and change line 26 "//set argv [list C:/​Xilinx/​SDSoC/​2015.2/​platforms]//"​ to point to your SDSoC platforms folder. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<​board>​_<​carrier>//,​ where //<​board>//​ is the name of the FMCOMMSx board and //<​carrier>//​ is the name of the Xilinx carrier, //eg. fmcomms2_zc702//​
 {{ :​resources:​eval:​user-guides:​targetting:​tcl_update_hdl.png?​500 |}} {{ :​resources:​eval:​user-guides:​targetting:​tcl_update_hdl.png?​500 |}}
  
resources/eval/user-guides/targetting/xilinx_sdsoc.txt · Last modified: 07 Aug 2015 15:59 by Andrei Cozma