Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:targetting:xilinx_sdsoc [17 Jul 2015 17:33] – [FMCOMMSx SDSoC Platforms] Andrei Cozma | resources:eval:user-guides:targetting:xilinx_sdsoc [07 Aug 2015 15:59] (current) – Andrei Cozma |
---|
* Open Vivado and in the tcl console //cd// to the target project sdsoc folder, //eg. \hdl\projects\fmcomms2\zc702// | * Open Vivado and in the tcl console //cd// to the target project sdsoc folder, //eg. \hdl\projects\fmcomms2\zc702// |
* Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design. | * Update the HDL design to Vivado 2015.2 by running the //sdsoc_platform/update_hdl.tcl// script. This step needs to be ran only once after downloading the HDL reference design. |
* Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/reference_hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified. | * Regenerate the IP libraries following the steps described here: http://wiki.analog.com/resources/fpga/docs/hdl. This step needs to be ran only once after downloading the HDL reference design, or every time the IP libraries are modified. |
* Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702// | * Generate the SDSoC platform by running the //sdsoc_platform/sdsoc_platform.tcl// script. Before running the script you need to edit it and change line 26 "//set argv [list C:/Xilinx/SDSoC/2015.2/platforms]//" to point to your SDSoC platforms folder. At the end of the process the new platform will be placed in the SDSoC platforms folder and will be named //<board>_<carrier>//, where //<board>// is the name of the FMCOMMSx board and //<carrier>// is the name of the Xilinx carrier, //eg. fmcomms2_zc702// |
{{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} | {{ :resources:eval:user-guides:targetting:tcl_update_hdl.png?500 |}} |
| |