This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:stingray:data [21 May 2022 15:50] Sam Ringwood |
resources:eval:user-guides:stingray:data [24 Jan 2023 20:12] Sam Ringwood Added switching speed plots |
||
---|---|---|---|
Line 55: | Line 55: | ||
<WRAP centeralign>**//Figure 10: Output Power vs Input Power, Transmit Channel at 10 GHz//**</WRAP> | <WRAP centeralign>**//Figure 10: Output Power vs Input Power, Transmit Channel at 10 GHz//**</WRAP> | ||
+ | |||
+ | ===== Switching Speed ===== | ||
+ | |||
+ | This measurement was conducted using a single cell (1x ADAR1000, 4x ADTR1107) on the ADAR1000EVAL1Z board. All tests were conducted at 10 GHz RF Frequency. The Tx output was combined using a 4:1 combiner and feed into a [[adi>adl6010|ADL6010]] envelope detector. The detector Vout was connected to the high impedance input of an oscilloscope. The oscilloscope trigger signal was the TR pin of the ADAR1000. | ||
+ | |||
+ | Pulse characteristics are a 1 kHz pulse repetition frequency with a 50 us pulse width (5% duty cycle). | ||
+ | |||
+ | {{ :resources:eval:user-guides:stingray:stingray_pulsemeasurement_1khz_pri_50us_pw_4channels_rxtx_m25dbm_input.png |}} | ||
+ | |||
+ | <WRAP centeralign>**//Figure 11: Rx-Tx Switching Time, 4 Coherently Combined Channels, 10 GHz RF, -25 dBm Input Power//**</WRAP> | ||
+ | |||
+ | {{ :resources:eval:user-guides:stingray:stingray_pulsemeasurement_1khz_pri_50us_pw_4channels_txrx_m25dbm_input.png |}} | ||
+ | |||
+ | <WRAP centeralign>**//Figure 12: Tx-Rx Switching Time, 4 Coherently Combined Channels, 10 GHz RF, -25 dBm Input Power//**</WRAP> | ||
+ | |||
+ | {{ :resources:eval:user-guides:stingray:stingray_pulsemeasurement_1khz_pri_50us_pw_4channels_rxtx_m7dbm_input_200nsdiv.png |}} | ||
+ | |||
+ | <WRAP centeralign>**//Figure 13: Rx-Tx Switching Time, 4 Coherently Combined Channels, 10 GHz RF, -7 dBm Input Power//**</WRAP> | ||
+ | |||
+ | {{ :resources:eval:user-guides:stingray:stingray_pulsemeasurement_1khz_pri_50us_pw_4channels_txrx_m7dbm_input_200nsdiv.png |}} | ||
+ | |||
+ | <WRAP centeralign>**//Figure 14: Tx-Rx Switching Time, 4 Coherently Combined Channels, 10 GHz RF, -7 dBm Input Power//**</WRAP> |