Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
resources:eval:user-guides:rf-trx-vcxo-and-profiles [24 May 2019 10:02] – [Updating the default RF Transceiver Profile] Michael Hennerichresources:eval:user-guides:rf-trx-vcxo-and-profiles [24 May 2019 10:14] – [Changing the VCXO frequency] Michael Hennerich
Line 2: Line 2:
  
 ===== Changing the VCXO frequency ===== ===== Changing the VCXO frequency =====
 +
 +{{ :resources:eval:user-guides:ad9528_fbl.png?400 |}}
  
 The ADRV9009, ADRV9008-1, ADRV9008-2, AD9371, AD9375 evaluation boards contains an on-board VCXO (Voltage Controlled Crystal Oscillator) as well as the AD9528 chip responsible for the device clock and SYSREF signal generation and distribution. With the hardware configuration provided on the evaluation board, a user can generate device clock frequencies such as 122.88MHz, 153.6MHz, 184.32MHz, 245.76MHz, and 307.2MHz. The ADRV9009, ADRV9008-1, ADRV9008-2, AD9371, AD9375 evaluation boards contains an on-board VCXO (Voltage Controlled Crystal Oscillator) as well as the AD9528 chip responsible for the device clock and SYSREF signal generation and distribution. With the hardware configuration provided on the evaluation board, a user can generate device clock frequencies such as 122.88MHz, 153.6MHz, 184.32MHz, 245.76MHz, and 307.2MHz.
resources/eval/user-guides/rf-trx-vcxo-and-profiles.txt · Last modified: 14 Nov 2022 10:59 by Liviu-Mihai Iacob