This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:rf-trx-vcxo-and-profiles [24 May 2019 10:02] – [Updating the default RF Transceiver Profile] Michael Hennerich | resources:eval:user-guides:rf-trx-vcxo-and-profiles [24 May 2019 10:14] – [Changing the VCXO frequency] Michael Hennerich | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== Changing the VCXO frequency ===== | ===== Changing the VCXO frequency ===== | ||
+ | |||
+ | {{ : | ||
The ADRV9009, ADRV9008-1, ADRV9008-2, AD9371, AD9375 evaluation boards contains an on-board VCXO (Voltage Controlled Crystal Oscillator) as well as the AD9528 chip responsible for the device clock and SYSREF signal generation and distribution. With the hardware configuration provided on the evaluation board, a user can generate device clock frequencies such as 122.88MHz, 153.6MHz, 184.32MHz, 245.76MHz, and 307.2MHz. | The ADRV9009, ADRV9008-1, ADRV9008-2, AD9371, AD9375 evaluation boards contains an on-board VCXO (Voltage Controlled Crystal Oscillator) as well as the AD9528 chip responsible for the device clock and SYSREF signal generation and distribution. With the hardware configuration provided on the evaluation board, a user can generate device clock frequencies such as 122.88MHz, 153.6MHz, 184.32MHz, 245.76MHz, and 307.2MHz. |