Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:pzsdr:carriers:packrf:system-software-architecture [29 Aug 2019 20:25] – Fixed link Travis Collins | resources:eval:user-guides:pzsdr:carriers:packrf:system-software-architecture [30 Oct 2019 08:47] (current) – [Portable Radio Software] Rename HDL project to PACKRF Adrian Costina |
---|
| |
The software for the ADRV-PACKRF is provided by Analog Devices as an open source reference design that can be used in various applications. The system source code consists of several components, which are used together to control onboard devices and provide connectivity to external tools for development. The following components are either used to build the ADRV-PACKRF firmware or can be used remotely from a host PC through a network connection: | The software for the ADRV-PACKRF is provided by Analog Devices as an open source reference design that can be used in various applications. The system source code consists of several components, which are used together to control onboard devices and provide connectivity to external tools for development. The following components are either used to build the ADRV-PACKRF firmware or can be used remotely from a host PC through a network connection: |
* FPGA HDL Code ([[https://github.com/analogdevicesinc/hdl/tree/master/projects/adrv9361z7035/ccbox_lvds|Standard Reference Design]], [[https://github.com/analogdevicesinc/TransceiverToolbox/tree/master/CI/projects/adrv9361z7035/ccbox_lvds_modem|Modem Enhancements]]) | * FPGA HDL Code [[https://github.com/analogdevicesinc/hdl/tree/master/projects/adrv9361z7035/ccpackrf_lvds |Standard Reference Design]], [[https://github.com/analogdevicesinc/TransceiverToolbox/tree/master/CI/projects/adrv9361z7035/ccbox_lvds_modem|Modem Enhancements]]) |
* Linux Kernel/Device Drivers ([[resources:tools-software:linux-drivers:iio-transceiver:ad9361|Transceiver]], [[https://github.com/analogdevicesinc/rfsom-box-gui/tree/master/tun_tap|Modem Controller]]) | * Linux Kernel/Device Drivers ([[resources:tools-software:linux-drivers:iio-transceiver:ad9361|Transceiver]], [[https://github.com/analogdevicesinc/rfsom-box-gui/tree/master/tun_tap|Modem Controller]]) |
* [[https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/18841973/Build+U-Boot|U-boot Bootloader]] | * [[https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/18841973/Build+U-Boot|U-boot Bootloader]] |